10.8.7. General Purpose Copy Routine¶
The cpy_tbl.h file in Copy Table Contents also contains a prototype for a general-purpose copy routine, copy_in(), which is provided as part of the run-time-support library. The copy_in() routine takes a single argument: the address of a linker-generated copy table. The routine then processes the copy table data object and performs the copy of each object component specified in the copy table.
The copy_in() function definition is provided in the cpy_tbl.c run-time-support source file shown in the following example.
/*****************************************************************************/
/* cpy_tbl.c v##### */
/* */
/* General purpose copy routine. Given the address of a linker-generated */
/* COPY_TABLE data structure, effect the copy of all object components */
/* that are designated for copy via the corresponding LCF table() operator. */
/*****************************************************************************/
#include <cpy_tbl.h>
#include <string.h>
typedef void (*handler_fptr)(const unsigned char *in, unsigned char *out)
/*****************************************************************************/
/* COPY_IN() */
/*****************************************************************************/
void copy_in(COPY_TABLE *tp)
{
unsigned short I;
for (I = 0; I < tp->num_recs; I++)
{
COPY_RECORD crp = tp->recs[i];
unsigned char *ld_addr = (unsigned char *)crp.load_addr;
unsigned char *rn_addr = (unsigned char *)crp.run_addr;
if (crp.size)
{
/*------------------------------------------------------------------*/
/* Copy record has a non-zero size so the data is not compressed. */
/* Just copy the data. */
/*------------------------------------------------------------------*/
memcpy(rn_addr, ld_addr, crp.size);
}
}
}