3.2. Specifying the Compilation Target¶
The following command-line options specify the device being used and other characteristics about the hardware environment that the compiler should assume during compilation. These options determine which instruction set is used by the compiler and whether or not the compiler can assume the availability of floating-point hardware.
armcl Option (and alias) |
commandline_name| Option |
|---|---|
--silicon_version=<processor ID> (-mv<processor ID>) |
-mcpu=<processor variant> -march=<architecture ID> |
The armcl compiler allows you to indicate which architecture and processor variant combination to assume during compilation using the -mv option. The armcl compiler assumes a default of -mv4, but you can also choose -mv5, -mv5e, -mv6M0, -mv7M3, -mv7M4, -mv7R4, or -mv7R5.
The tiarmclang compiler provides two analogous options:
Use -mcpu to direct the compiler to target a particular processor variant. The tiarmclang compiler requires that a valid -mcpu or -march option be specified (or it will assume cortex-m4 if neither an -mcpu or -march option is provided). You may select one of the following: cortex-m0, cortex-m3, cortex-m4, cortex-r4, or cortex-r5. Each of the available arguments to the -mcpu option imply a specific -march option argument.
Use -march to direct the compiler to target a particular architecture. The tiarmclang compiler assumes armv7e-m (which corresponds to the cortex-m4 processor variant) if no -mcpu or -march option is specified. You may select one of the following: armv6-m, armv7-m, armv7e-m, and armv7-r.
Please note that the tiarmclang compiler does not provide support for armv4, armv5e, armv6, armv7-a. Likewise, it does not support any of the -march variants that are not mentioned above.
armcl Option |
tiarmclang Option |
|---|---|
--code_state=<16|32> |
-mthumb -marm |
The armcl compiler uses the --code_state option to select between THUMB (16) and ARM (32) mode. For targets such as Cortex-r4 and Cortex-r5that support both the ARM and T32 (THUMB) instruction sets, the default is the Arm instruction set.
Use tiarmclang’s -mthumb option to select the T32 instruction set. If a cortex-m3 or cortex-m4 argument is specified for the -mcpu option or an armv7-m or armv7e-m argument is specified for the -march option, then the tiarmclang compiler will assume that the -mthumb option is on.
armcl Option |
tiarmclang Option |
|---|---|
--float_support=<float hardware ID> |
-mfloat-abi=<soft|hard> -mfpu=<float hardware ID> |
armcl Option (and alias) |
tiarmclang Option |
|---|---|
--endian=little (-me) --endian=big (default) |
-mlittle-endian (default) -mbig-endian |
By default, tiarmclang generates little-endian code. This is the opposite of armcl, which defaults to big-endian code.