15.6. c29strip - Object File Stripping Tool

The c29strip tool removes the symbol table and debugging information from object and executable files. To invoke the c29strip tool, use the following command line:

c29strip [options] filename [filename]

  • c29strip - is the command that invokes the object file stripping tool.

  • options - control the behavior of the c29strip tool. Options are not case sensitive and can appear before or after the files to be stripped. Precede each option with a hyphen (-).

  • filename - identify one or more object files (.obj) or executable files (.out) to be processed by c29strip. By default, the files are modified in-place.

15.6.1. Options

--buffer_diagnostics,-pdb

Line buffer diagnostic output

--diag_wrap[=on,off]

Wrap diagnostic messages (argument optional, defaults to on)

--emit_warnings_as_errors,-pdew

Treat warnings as errors

--help,-h

Display help information

--outfile,-o=file

Write the stripped output to the specified new file. When the strip utility is invoked without the -o option, the input object files are replaced with the stripped version.

Remove all information not required for execution. This option causes more information to be removed than the default behavior, but the object file is left in a state that cannot be linked. This option should be used only with static executable files.

--rom

Strip readonly sections and segments.

15.6.2. Exit Status

The c29strip utility exits with a non-zero exit code if there is an error. Otherwise, it exits with code 0.