3.11. Preprocessor Options¶
The following command-line options control the preprocessor.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--define=<name>[=<value>] (-D=<name>[=<value>]) |
-D<name>[=<value>] |
The cl2000 compiler provides the --define option to predefine a preprocessor macro. The macro symbol can be given a value if an assignment to the optional value argument is included.
The c29clang compiler’s -D option provides the same functionality. The c29clang compiler also provides the ability to append a macro parameter list in order to define function-style macros.
For both compilers, if the assignment to value argument is omitted, then the predefined symbol’s value is set to 1.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--undefine=<name> (-U=<name>) |
-U<name> |
The cl2000 compiler provides the --undefine option to undefine a preprocessor macro.
The c29clang compiler’s -U option provides the same functionality.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_dependency[=<file>] (-ppd[=<file>]) |
-M |
The cl2000 compiler provides the --preproc_dependency option, which produces a list of dependency rules for use by a make utility. This list includes both system and user header files. When this option is used, the compiler executes only the preprocessor step of the compilation. Unless a filename is specified, the preprocessed output is sent to a file with an extension of .pp.
The c29clang compiler’s -M option provides the same functionality. However, the preprocessed output is sent to stdout by default.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_includes[=<file>] (-ppi[=<file>]) |
-MM |
The cl2000 compiler provides the --preproc_includes option, which produces a list of dependency rules for use by a make utility. This list includes only user header files. When this option is used, the compiler executes only the preprocessor step of the compilation. Unless a filename is specified, the preprocessed output is sent to a file with an extension of .pp.
The c29clang compiler’s -MM option provides the same functionality. However, the preprocessed output is sent to stdout by default.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_only (-ppo) |
-E |
The cl2000 compiler provides the --preproc_only option, which causes the compiler to execute only the preprocessor step of the compilation. The preprocessed output is sent to a file with an extension of .pp.
The c29clang compiler’s -E option provides the same functionality. However, the preprocessed output is sent to stdout by default.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_macros{=<file>] (-ppm{=<file>]) |
-E -dM |
The cl2000 compiler provides the --preproc_macros option, which produces a list of predefined and user-defined macros. When this option is used, the compiler executes only the preprocessor step of the compilation. Unless a filename is specified, the preprocessed output is sent to a file with an extension of .pp.
The c29clang compiler’s -E and -dM options used together provide the same functionality. However, the preprocessed output is sent to stdout by default.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_with_comment (-ppc) |
-E -C |
The cl2000 compiler provides the --preproc_with_comment option, which causes the compiler to execute only the preprocessor step of the compilation. It keeps the comments instead of discarding them as is done with the --preproc_only option. The preprocessed output is sent to a file with an extension of .pp.
The c29clang compiler’s -E and -C options used together provide the same functionality. However, output is sent to stdout by default.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_with_compile (-ppa) |
not supported |
The cl2000 compiler provides the --preproc_with_compile option, which causes the compiler to continue after executing one of the --preproc_* options that produce preprocessor output files.
The c29clang compiler does not support continuing compilation after generating preprocessor output with the -E option.
cl2000 Option (and alias) |
c29clang Option |
---|---|
--preproc_with_line (-ppl) |
-E |
The cl2000 compiler provides the --preproc_with_line option, which causes the compiler to execute only the preprocessor step of the compilation. It adds line-control information (#line directives) to the output. Output is sent to a file with an extension of .pp.
The c29clang compiler’s -E option stops the compiler after the preprocessing stage. The preprocessed source code is emitted to stdout containing line-control information. The c29clang does not provide an option to disable the output of line-control information in the preprocessed output.