1.3.10. Diagnostic Options¶
1.3.10.1. Controlling Error, Warning, and Remark Diagnostics¶
The c29clang compiler provides the following options to assist with controlling what errors, warnings, and remarks are emitted during compilation:
- -R<remark>¶
Enable the specified remark category.
- -Wall¶
Enable most warning categories.
- -Wextra¶
Enable the diagnostics that are enabled by -Wall plus a number of additional warning types.
- -Werror¶
Treat detected warnings as errors.
- -Werror=<warning-category>¶
Treat detected warnings in the specified category as errors.
- -W<warning-category>¶
Enable the specified warning category.
- -Wno-<warning-category>¶
Disable the specified warning category.
- -w¶
Disable all warnings.
In addition to enabling and disabling diagnostics on the command line, pragmas can be used control specific diagnostics in a section of code. See clang diagnostic for details and examples.
1.3.10.2. Optimization Feedback Options¶
The following options can be used to instruct the c29clang compiler to emit information about the different optimizations and code transformations that are performed during compilation:
- -Rpass-analysis=<arg>¶
Report transformation analysis from optimization passes whose name matches the given POSIX regular expression.
- -Rpass-missed=<arg>¶
Report missed transformations by optimization passes whose name matches the given POSIX regular expression.
- -Rpass=<arg>¶
Report transformations performed by optimization passes whose name matches the given POSIX regular expression.