Overview
--------
**Serial Wire Output (SWO) Trace** is a single pin trace interface that allow users to trace the program flow and profile hardware events. These profiling capabilities are very important for debugging, validating and characterizing applications. In this workshop, you will experience using SWO Trace, via the Trace Visualization Toolkit, using basic examples.
Requirements
------------
- **CC13x2** and **CC26x2** LaunchPads.
[[+g Other LaunchPads
Please go to [Serial Wire Output (SWO) Trace workshop](https://dev.ti.com/tirex/explore/node?node=ALmaatMYmDe.acaw5f2ipw__FUz-xrs__LATEST)
+]]
2. Go to **Advanced Setup configuration**
Open the targetConfigs file under your project folder:

Double click to open the Target Configuration menu and click on the USB Debug Probe:

3. [[+g Parameters and file modification for **CC13x2** and **CC26x2** LaunchPads (expand)
{{b **Make sure of the following settings for every project imported for each lab below:** }}
Make sure that the parameters shown in the screenshot below are configured:

Additionally, you must modify the board-specific configuration file. The name of the file varies depending the device and board. For launchpads, the format will be (DEVICE)_LAUNCHXL_fxns.c. In this file, there will be a function called Board_initHook(). Add the following lines to the function:
```
// Map Serial Wire Viewer to JTAG TDO pin
IOCPortConfigureSet(IOID_16, IOC_PORT_MCU_SWV, IOC_STD_OUTPUT);
```
For example, if you are using a [CC1310 LaunchPad](https://store.ti.com/LAUNCHXL-CC1310-SimpleLink-Sub-1-GHz-wireless-microcontroller-MCU-LaunchPad-development-kit-P49907.aspx), the file is called CC1310_LAUNCHXL_fxns.c. The modifications to Board_initHook() would look as so:

[[r Note:
This is not supported on some older SDKs. Make sure you are using the latest version of the SimpleLink SDK for your LaunchPad.]]
+]]
Lab 1: Statistical Function Profile
---
**Statistical Function Profile** is a useful tool that shows the frequency of function calls within a program using statistical methods. The **Program Counter (PC)** is regularly sampled, and the function being executed is determined based on the PC value. This tool is important because it can show which functions are more crucial.
### 1.1 Example program
The basis for the example is the **empty** project which can be imported from the **SDK** using [Resource Explorer](https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_getting-started.html#resource-explorer):
{{b **Software → SimpleLink (YourDeviceFamily) SDK – v:(X.X.X.X) → Examples → Development Tools → (YourLaunchPad) → TI Drivers → empty → TI-RTOS → CCS Compiler → empty**}}
Small modifications to the project are needed to better demonstrate the capabilities of the profiler.
1. Start by adding the following dummy functions above the `mainThread()` function in empty.c.
```c
void divBy2() {
int i = 0;
for (i=0;i<50;i++) {
}
}
void divBy4() {
int i = 0;
for (i=0;i<50;i++) {
}
}
void divBy8() {
int i = 0;
for (i=0;i<50;i++) {
}
}
```
These dummy functions will be the targets that you will investigate with the function profiler.
2. Replace the while loop in the `mainThread()` function with the following for loop.
```c
int counter=0;
for (counter=0;counter<=1600;counter++) {
if (counter % 2 == 0) {
divBy2();
}
if (counter % 4 == 0) {
divBy4();
}
if (counter % 8 == 0) {
divBy8();
}
}
counter=0;
```
This loop will create an interesting function call pattern for each dummy function.
3. Setup a breakpoint at the line `counter=0;` right after exiting the loop. (You can do so by double-clicking in the editor margin of the source file.) This breakpoint will be used to stop the tool from running after the loop exits.
4. Ensure that the target configuration (and the board configuration, if applicable) are properly configured as described [above](#requirements).
Remember to modify the board-specific configuration file. Find the file in the project folder in this format: (DEVICE)_LAUNCHXL_fxns.c, then add the following lines inside the function called `Board_initHook()`.
```
// Map Serial Wire Viewer to JTAG TDO pin
IOCPortConfigureSet(IOID_16, IOC_PORT_MCU_SWV, IOC_STD_OUTPUT);
```
Your code in **empty.c** should look like this:
[[+d Expand full example code 1
```c
/*
* Copyright (c) 2015-2017, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== empty.c ========
*/
/* For usleep() */
#include
#include
#include
/* Driver Header files */
#include
// #include
// #include
// #include
// #include
// #include
/* Board Header file */
#include "Board.h"
void divBy2() {
int i = 0;
for (i=0;i<50;i++) {
}
}
void divBy4() {
int i = 0;
for (i=0;i<50;i++) {
}
}
void divBy8() {
int i = 0;
for (i=0;i<50;i++) {
}
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
/* Call driver init functions */
GPIO_init();
// I2C_init();
// SDSPI_init();
// SPI_init();
// UART_init();
// Watchdog_init();
/* Configure the LED pin */
GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
/* Turn on user LED */
GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_ON);
int counter=0;
for (counter=0;counter<=1600;counter++) {
if (counter % 2 == 0) {
divBy2();
}
if (counter % 4 == 0) {
divBy4();
}
if (counter % 8 == 0) {
divBy8();
}
}
counter=0;
}
```
+]]
### 1.2 Using the tool
1. Click **Run → Debug** (or **F11**) to launch the debugger.
2. Select **Tools → Code Analysis → Event Analysis** to launch the Configure Event Profile.
{{b If it is the first time you go to the Event Analysis menu, a section called Event Analysis will show up.}}
3. Start by choosing Statistical Function Profile and a sampling interval of **256 cycles**. Click **OK**.
{{b Shorter sampling intervals can be chosen, but high sampling rates can cause overflow and packet loss if the data cannot be drained fast enough. When the sampling rate is getting too high, warnings of overflow will appear in the **Trace Viewer**.}}

This means that the profiler will read and record the PC location every 256 cycles, creating a dense profile. Click on **Start** to accept the changes and enable the **Trace Analyzer**.
[[+y CCS cannot determine the clock frequency automatically? (expand)
You might receive an error message saying "Could not determine the System clock frequency automatically. Please set it manually in the receiver properties."
In this case, click the **Advanced Settings** button in the window shown above. Select **Receiver** on the left and then under **Hardware Configuration → Receiver Settings → Receiver → UART Options** set **Clock Frequency** to **Manual** and replace **Frequency in Hz** by the the CPU frequency for your board (120000000 for the MSP432E4, and 48000000 for the other boards used in this lab).
You will also need to set the sampling interval manually. Select **PC Trace** on the left and under **Hardware Configuration → Type → Triggers → Clock or PC Sample** set the **Clock Interval** to the desired value. +]]
4. Click **Start Capture** on the top right to capture data.
{{b You can check **Display each channel message on a separate line with timestamp** to get the messages.
}}
5. Resume the program (**Run → Resume**, or F8), and it should run and halt at the breakpoint you have set earlier. You can find the **Statistical Function Profile** view. It shows the number of times a function is encountered by the tracer. You might need to wait a few seconds for CCS to process all the data before the view shows the results.

Looking at the encounter proportion of the dummy functions, you will find that they closely match the expected calling ratio. i.e. `divBy2()` should be called twice as often as `divBy4()` and four times as often as `divBy8()`. Notice that there are a lot of small helper functions in the result list. Also, the "times encountered" field shows very large numbers. Both of these are due to the short sampling interval of 256 cycles.
6. The **Raw Data** view displays the raw data collected by the tracer. Click on the **Settings** button on the top left corner  and change the sampling interval to 4096 cycles. Click **Ok**. Restart the program (**Run → Restart**), resume execution (**Run → Resume**, or F8), and observe the result.

The list is much shorter than last time, with only a few encounters of helper functions. The calling ratio of the dummy functions also diverges from the expectation greater than before. This is because the sampling interval is very long, potentially skipping entire calls to a function.
7. That's it! When you are finished, click **Run → Terminate** (or Ctrl+F2) to terminate the debug session and close the Event Analysis window.
Lab 2: Exception Profile
---
### 2.1 Example program
For this example, the **empty** project is used as a base and the contents of empty.c are replaced with a program that behaves like the **timerled** project used for the MSP432 boards. Before importing the **empty** project again, rename the project used in Lab 1 to something else. Once again, the project can be imported from the SDK:
{{b **Software → SimpleLink (YourDeviceFamily) SDK – v:(X.X.X.X) → Examples → Development Tools → (YourLaunchPad) → TI Drivers → empty → TI-RTOS → CCS Compiler → empty**}}
Ensure that the target configuration (and the board configuration, if applicable) are properly configured as described [above](#requirements).
Remember to modify the board-specific configuration file. Find the file in the project folder in this format: (DEVICE)_LAUNCHXL_fxns.c, then add the following lines inside the function called `Board_initHook()`.
```
// Map Serial Wire Viewer to JTAG TDO pin
IOCPortConfigureSet(IOID_16, IOC_PORT_MCU_SWV, IOC_STD_OUTPUT);
```
Replace the contents of empty.c with the following:
```c
/*
* This is a modified version of an example given in the GPTimerCC26XX.h File Reference
* It will toggle the led once per second
*/
/* Driver Header files */
#include
#include
#include // For Types_FreqHz
#include // For BIOS_getCpuFreq
/* Board Header file */
#include "Board.h"
// Callback to toggle the LED
void timerCallback(GPTimerCC26XX_Handle timerHandle, GPTimerCC26XX_IntMask interruptMask)
{
GPIO_toggle(Board_GPIO_LED0);
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
/* Call driver init functions */
GPIO_init();
/* Configure the LED pin */
GPIO_setConfig(Board_GPIO_LED0, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
/* Turn off user LED */
GPIO_write(Board_GPIO_LED0, Board_GPIO_LED_OFF);
GPTimerCC26XX_Params params;
GPTimerCC26XX_Params_init(¶ms);
params.width = GPT_CONFIG_32BIT;
params.mode = GPT_MODE_PERIODIC_UP;
params.debugStallMode = GPTimerCC26XX_DEBUG_STALL_OFF;
GPTimerCC26XX_Handle hTimer = GPTimerCC26XX_open(Board_GPTIMER0A, ¶ms);
if (hTimer == NULL) {
/* Failed to initialized timer */
while (1) {}
}
// This timer will count up (from zero) to the value specified by loadVal and then call our callback.
// We set loadVal equal to our processor frequency so that the callback period is one second.
Types_FreqHz freq;
BIOS_getCpuFreq(&freq);
GPTimerCC26XX_Value loadVal = freq.lo - 1;
GPTimerCC26XX_setLoadValue(hTimer, loadVal);
GPTimerCC26XX_registerInterrupt(hTimer, timerCallback, GPT_INT_TIMEOUT);
GPTimerCC26XX_start(hTimer);
return (NULL);
}
```
These programs use a timer interrupt to toggle the on-board LED every second. You will use the the Exception profiling tool to observe these interrupts.
### 2.2 Using the tool
1. Click **Run → Debug** to launch the debugger.
2. Select **Tools → Code Analysis → Event Analysis** to launch the Configure Event Profile. Use the default options (unless you need to input the clock speed manually) and check the **Exception Profile** option. Press **Ok**.
3. Click on **Start Capture** to capture the data.
4. Resume the program, observe the on-board LED. Pause the program from the debugger (**Run → Suspend**, or Alt+F8) after seeing the LED toggle 2-3 times.
{{b A window may appear stating that "You are opening a large file." You can decline to change the scalability settings. If the file seems too large for CCS to handle, you can restart and pause the program after fewer LED toggles.}}
5. Click on the **Exception Profile** tab, you will see the graphical view of exception as well as the **Exception Statistics**. **Raw Data** shows the raw data captured by the trace.

6. Look for the row corresponding to the interrupt that was instantiated in the program.
7. Zoom out using **Left click and left/right scroll** to see more details.
For this interrupt on screen. The number of lines should be the same as the number of times the LED was toggled earlier. These straight lines mark when in the program runtime the interrupt (timer) was triggered.
8. That's it! When you are finished, terminate the debug session and close the Event Analysis window.
Lab 3: Variable Profile
---
### 3.1 Example program
The basis for the example is the **gpiointerrupt** project which can be imported from the SDK:
{{b **Software → SimpleLink (YourDeviceFamily) SDK – v:(X.X.X.X) → Examples → Development Tools → (YourLaunchPad) → TI Drivers → gpiointerrupt → TI-RTOS → CCS Compiler → gpiointerrupt**}}
Ensure that the target configuration (and the board configuration, if applicable) are properly configured as described [above](#requirements).
Remember to modify the board-specific configuration file. Find the file in the project folder in this format: (DEVICE)_LAUNCHXL_fxns.c, then add the following lines inside the function called `Board_initHook()`.
```
// Map Serial Wire Viewer to JTAG TDO pin
IOCPortConfigureSet(IOID_16, IOC_PORT_MCU_SWV, IOC_STD_OUTPUT);
```
Small modifications to the project are needed:
1. Open gpiointerrupt.c and add a global variable **click_count** right before all the functions.
```c
unsigned int click_count = 0;
```
{{b We use an unsigned integer because the **Data Variable Trace** does not distinguish between signed and unsigned data.}}
2. At the end of the `gpioButtonFxn0()` function add `click_count++;`, and at the end of the `gpioButtonFxn1()` function add
```c
if (click_count > 0)
click_count--;
```
The functions should now look like this:
```c
void gpioButtonFxn0(uint_least8_t index)
{
/* Clear the GPIO interrupt and toggle an LED */
GPIO_toggle(Board_GPIO_LED0);
click_count++;
}
void gpioButtonFxn1(uint_least8_t index)
{
/* Clear the GPIO interrupt and toggle an LED */
GPIO_toggle(Board_GPIO_LED1);
if (click_count > 0)
click_count--;
}
```
3. Ensure that the target configuration (and the board configuration, if applicable) are properly configured as described [above](#check-target-configuration).
### 3.2 Using the tool
1. Click **Run → Debug** to launch the debugger.
2. Select **Tools → Code analysis → Event Analysis**. Check **Variable Profile**. In the **Variable Address** field, enter **click_count** and press **Ok**.
3. Resume the program, press **button0** a few times and then press **button1** a few times. Pause the program afterward. As an example, **button0** is pressed 3 times and then **button1** is pressed 3 times.
4. Click on the **Variable Profile** tab, you will see the graphical view of how the watched variable changes as well as a **Tabular view of reads and writes**. You can see a graph that shows the value of the variable going up and down.

5. In the **Tabular view** chart the record of button clicks can be seen under click_count Rd and click_count Wr. The time when the buttons are clicked are also recorded.
6. That's it! When you are finished, terminate the debug session and close the Event Analysis window.
Summary
---
The **Trace Visualization Toolkit** functionalities are very helpful tools for analyzing, debugging and monitoring a program.
In this workshop, you have learned the basics of **Statistical Function Profile**, **Exception Profile** and **Variable Profile**.
These simple examples are meant to get you familiar with the capabilities of Trace Visualization Toolkit, apply them to your projects.