8.8.1.1.2.2.13. Settings

class Settings
getDetailedSettings() → list[DebugSetting]

Get a detailed list of all debugger settings.

settings = session.settings.getDetailedSettings()

# print details of settings
for setting in settings:
    print(f"{setting['id']}:")
    print(f"  type: {setting['type']}")
    print(f"  name: {setting['name']}")
    print(f"  value: {setting['value']}")
    if 'allowedValues' in setting:
        print(f"  allowedValues: {setting['allowedValues']}")
    if 'allowedRange' in setting:
        range = setting['allowedRange']
        print(f"  allowedRange: [{range['min']}, {range['max']}]")
    print("")
Returns:

A list of objects which detail each debugger setting.

Return type:

list[DebugSetting]

get(settingId) → bool | int | str

Get the value of a specific debugger setting.

# Get a boolean indicating if debugger is configured to auto run to a label on reset
autoRun = session.settings.get("AutoRunToLabelOnReset")

# print the label (a string) to which the debugger will run to on a restart or reset (if configured to do so)
print(session.settings.get("AutoRunToLabelName"))
Parameters:

settingId (str) -- The identifier for the desired setting.

Returns:

The value of the setting.

Return type:

bool | int | str

set(settingId, value) → None

Set the value of a specific debugger setting.

# Configure the debugger to auto-run to a label named SYSCFG_DL_init on reset
session.settings.set("AutoRunToLabelName", "SYSCFG_DL_init")
session.settings.set("AutoRunToLabelOnReset", True)
Parameters:
  • settingId (str) -- The identifier for the desired setting.

  • value (bool | int | str) -- The new value of the setting.

Return type:

None