8.8.1.1.2.2.7. Expressions

class Expressions
evaluate(expression) → None | int | str | float

Evaluates a GEL expression and returns the resulting value, if numerical or a string. All standard rules for GEL expressions apply. If the result of evaluating the expression is an integral value, a BigInt will be returned. If the value is a floating point value, a standard Javascript number will be returned. For any other value, like a reference to a c++ object, we return without a value.

# Adds 8 to the address of the main symbol, returns an int
result = session.expressions.evaluate("main + 8")

# Returns a floating point number
result = session.expressions.evaluate("1.0 / 2")

# Call a GEL function (assuming that this function is defined in a loaded GEL script)
session.expressions.evaluate('userDefinedGelFunction()')
Parameters:

expression (str) -- The GEL expression to evaluate.

Returns:

The value resulting from the evaluation of the expression, if numerical or a string.

Return type:

None | int | str | float