9. Frequently Asked Questions¶
This chapter answers some of the frequently asked questions (FAQs) about CCS Theia.
- 9.1. General
- 9.1.1. Is Code Composer Studio™ based on VS Code?
- 9.1.2. What are the differences between the Theia IDE and VS Code?
- 9.1.3. What happened to Code Composer Studio Theia and how is it different from Code Composer Studio 20.x?
- 9.1.4. Does Code Composer Studio come with an AI Code Assistant?
- 9.1.5. Is my device supported by the new Theia IDE based Code Composer Studio?
- 9.1.6. Which operating systems are supported by Code Composer Studio?
- 9.1.7. Why do I need to avoid non-alphanumeric (unicode) characters in my paths?
- 9.1.8. Are non-alphanumeric (unicode) characters supported?
- 9.1.9. What kind of safety certification does Code Composer Studio have?
- 9.1.10. What is the best way to look up a bug?
- 9.1.11. Where can I get more information on Code Composer Studio?
- 9.2. Installation
- 9.3. Licensing
- 9.4. Updates
- 9.5. General IDE
- 9.6. Projects
- 9.6.1. How do I create a new project from scratch?
- 9.6.2. I get a No example projects found. Please change your filter. message when looking for examples for my selected device. Does that mean that my device is not supported by Code Composer Studio?
- 9.6.3. During project build, a ccsLinker.opt file sometimes gets passed to the linker instead of the list of object files. What is this file and when is it used?
- 9.6.4. How can I resolve build error #10234-D: unresolved symbols remain?
- 9.6.5. The Eclipse WORKSPACE_LOC variable is not pointing to my workspace folder. How do I resolve this?
- 9.7. Debug
- 9.7.1. Why are my breakpoints greyed out even though they are enabled?
- 9.7.2. Why can't I source step?
- 9.7.3. How do I access the debugger/flash properties when in a debug session?
- 9.7.4. Which scripting solution (legacy or new) should I use?
- 9.7.5. I get Data Verification errors when loading my program. What does it mean?
- 9.7.6. Why isn't printf working when running code in Code Composer Studio?
- 9.7.7. Do I have to use an XDS110 debug probe to debug a secure device?
- 9.7.8. Is Pin Trace Supported?