7.7.7.1. The hotmenu KeywordΒΆ
Use the hotmenu keyword to add a GEL function to the GEL menu that is executed immediately when selected. The syntax is as follows:
hotmenu funcName()
{
statements
}
This keyword is used for GEL functions that have no Parameters to be passed.
___
Example:
menuitem "My Functions";
hotmenu InitTarget()
{
*waitState = 0x11;
}
hotmenu LoadMyProg()
{
GEL_Load("c:\\mydir\\myfile.out");
}
This example adds the following sub-selections under the Scripts menu.

When you choose the InitTarget command, it is immediately executed. To call GEL functions that require Parameters to be passed, use the dialog keyword.