8.8.1.1.1.2.10. MemMap¶
- interface MemMap()¶
- get()¶
Fetches the memory map.
// Print the memory map const { entries, enabled } = session.memory.memMap.get(); for (const entry of entries) { const attributes = entry.attributes.join(', ') console.log(`${entry.start} - ${entry.end}: ${attributes}`); } console.log(`The memory map is ${enabled ? "enabled" : "disabled"}`);
- Returns:
The memory map.
- Return type:
MemoryMapResult
- add(startLocation: DSLocation, length: Address, readable: boolean, writable: boolean)¶
Adds read or write permission for a range of target memory to the memory map.
// Add a range of memory to the memory map from 0x1000 to 0x1999 to be readable and not writable session.memory.memMap.add(0x1000, 0x1000, true, false);
- Parameters:
startLocation (
DSLocation) -- The starting address of a range in memory.length (
Address) -- The length of the range.readable (
boolean) -- Set to true to make this range readable. A memory range can be readable, writable or both.writable (
boolean) -- Set to true to make this range writable. A memory range can be readable, writable or both.
- Return type:
void
- enable(mapOn: boolean)¶
Toggles memory mapping on or off in the debugger server.
// Turn memory mapping on session.memory.memMap.enable(true); // Turn memory mapping off session.memory.memMap.enable(false);
- Parameters:
mapOn (
boolean) -- Set to true to turn memory mapping on, and false to turn memory mapping off. Default value is true.
- Return type:
void
- remove(location: DSLocation)¶
Deletes a range of memory from the memory map.
// Assume you have a range of (0x000 - 0x1007) in the current memory map, then it can be removed by session.memory.memMap.remove(0x100); // or equivalently, session.memory.memMap.remove(0x1000); // or any other address in that range.
- Parameters:
location (
DSLocation) -- Identifies an address with a memory range already defined in the memory map.
- Return type:
void
- reset()¶
Resets the memory map by making all memory non-readable and non-writeable.
session.memory.memMap.reset();
- Return type:
void