8.8.1.1.1.2.5. Clock¶
- interface Clock()¶
- disable()¶
Disable the profile clock.
session.clock.disable();
- Return type:
void
- disableAutoReset()¶
Disable Auto-Reset mode for the profile clock.
session.clock.disableAutoReset();
- Return type:
void
- enable()¶
Enable the profile clock.
session.clock.enable();
- Return type:
void
- enableAutoReset()¶
Enable Auto-Reset mode for the profile clock.
session.clock.enableAutoReset();
- Return type:
void
- getCurrentEvent()¶
Get the currently configured profile clock event.
const event = session.clock.getCurrentEvent(); if (event) { console.log(`The clock is currently profiling ${event.name}`); } else { console.log(`The clock is not currently profiling an event`); }
- Returns:
The currently configured profile clock event.
- Return type:
ClockEvent | null
- getEvents()¶
Get a list of all available profile clock events.
const events = session.clock.getEvents(); for (const event of events) { console.log(`${event.id}: ${event.name}`); }
- Returns:
A list of all available profile clock events.
- Return type:
ClockEvent[]
- read()¶
Read the current value of the profile clock counter.
const count = session.clock.read();
- Returns:
The current value of the profile clock.
- Return type:
bigint | number | string
- reset()¶
Reset the profile clock counter to zero.
session.clock.reset();
- Return type:
void
- setCurrentEvent(event: number | string)¶
Configure the profile clock to profile/count a particular event.
// by id session.clock.setCurrentEvent(1); // by name (this is just an example, events differ by target) session.clock.setCurrentEvent("CPU.discontinuity.branch");
- Parameters:
event (
number | string) -- The id or name of the event to profile.
- Return type:
void