7.7.1.21. GEL Namespace

When GEL parses a symbol name in an expression, GEL determines if the symbol is a local variable defined in the loaded symbol files first. If not, GEL checks if it is a global variable. Then, GEL matches the name against target register names. Finally, GEL looks up if any GEL variable with the same name is defined.

If you have a GEL variable named the same a variable in your code, only the variable in your code will ever be displayed. There is no way to change this lookup order.

GEL namespace is introduced to allow you to specify from where GEL should resolve a symbol.

Syntax

A GEL namespace is like a regular C++ namespace except the namespace name is a single-quoted string.

A GEL namespace is either GEL_namespace or REG_namespace or SYM_namespace.

A GEL_namespace indicates that GEL should look up the symbol in the list of GEL global variable. It is represented by either 'GEL' or 'Gel' or 'gel'. They have the same meaning and are defined for your convenience.

A REG_namespace indicates that GEL should look up the symbol in the list of target register names. It is represented by either 'REG' or 'Reg' or 'reg'. They have the same meaning and are defined for your convenience.

The syntax for a SYM_namespace is ' < SYM > [ :: [ < symbol file name > ] [ :: < source file name >] ] ' where is either 'SYM' or 'Sym' or 'sym'.

Here are some examples:

Expression Meaning
v look for v in the usual order
'GEL'::v look for a GEL variable v
'Gel'::v same as above
'gel'::v same as above
gel::v without single quotes, gel is interpreted as a C++ class name or namespace
'REG'::v look for the register v
'Reg'::v same as above
'reg'::v same as above
'SYM'::v look for a symbol v from the loaded symbol files
'Sym'::v same as above
'sym'::v same as above
'a.c'::v look for a file static variable v defined in source file a.c from all loaded symbol files
'sym::::a.c'::v same as above
'sym::a.out'::v look for a variable v defined in a symbol file matching name a.out
'sym::a.out::a.c'::v look for a file static variable v defined in source file a.c from a symbol file matching name a.out
'sym::arch/a.out::arch/a.c'::v look for a file static variable v defined in source file arch/a.c from a symbol file matching name arch/a.out