7.9.1.14. GEL Preprocessing Statements¶
GEL supports the standard #define preprocessing keyword. This is the only preprocessing keyword currently available.
A control line such as the following causes the preprocessor to replace subsequent instances of the identifier with the given sequence of tokens:
#define identifier token-sequence
Leading and trailing white spaces around the token sequence are discarded.
A control line such as the following, where there is no space between the first identifier and the open parenthesis, is a macro definition with Parameters given by the identifier list:
#define identifier( identifier-list ) token-sequence
When a macro has been defined using the #define keyword, you may use it anywhere in that file as well as in any other files that are loaded subsequently into the Code Composer Studio debugger.
___
See also: