7.9.8.74. GEL_SharedMemHaltOnWriteOn()ΒΆ
Affected cores are halted during a write to shared memory.
Syntax
GEL_SharedMemHaltOnWriteOn( void );
Parameters
None
Description
Multiple cores on a single processor can share a block of memory. While writing to memory, the breakpoints in that block have to be cleared for a short time by the driver. This function specifies that all cores with executable code on that block are halted to ensure that no breakpoints are missed and invalid code is not executed.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_SharedMemHaltOnWriteOn();
Related Topics