7.9.1.22. Defining Shared MemoryΒΆ
Multiple cores on a single processor can share a block of memory. The GEL function GEL_MapAddStr() is used to add a range of shared memory to the memory map. The attributes of shared memory are specified as parameters to the function. For example, the access to shared memory may be RAM or ROM.
Options can be used to control debugger functionality when debugging shared memory.
To Specify Shared Memory Attributes
Shared memory attributes are specified in the GEL_MapAddStr() function.
GEL_MapAddStr(address, page, length, attribute,  waitstate);
The function parameters address, page, length, and waitstate are specified as described in GEL_MapAddStr(). However, the attribute parameter accepts additional attributes that specify shared memory. For example:
RAM|SHnC|CACHE
ROM|SHnC|CACHE
| String | Description | 
| RAM | Specifies that access to memory is Read and Write. | 
| ROM | Specifies that access to memory is Read-only. | 
| SHnC | The string SH specifies shared memory. The number n identifies the block of memory being shared. The number can never be zero or negative. If a block of shared memory is specified on core A as "RAM|SH2" and then a block is specified on core B as "ROM|SH2", then that block is shared between cores A and B with Read and Write access on A and Read-only access on B. Blocks may be in different addressable regions for different cores. That is, on core A the block might start at 0x8000 and on core B the same block could start at 0x4000. The string C causes the debugger to: 
 When writing to a block of shared memory, the breakpoints in that block have to be cleared for a short time by the driver. In addition, the data in that location may be incorrect if the processor was executing. When "C" is specified, all cores with executable code on that block are halted to ensure that no breakpoints are missed and invalid code is not executed. When stepping over a software breakpoint that is set in a shared memory block, the breakpoint is first cleared, then the code is stepped, and finally the breakpoint is reset. If other cores execute code in that memory block during this time, they will miss the breakpoint. When "C" is specified, all cores with executable code on that block are halted until the breakpoint has been stepped over. C is optional, but should always be appended as the default setting. The default settings for these actions can be overridden by setting shared memory options.  | 
| CACHE | Causes the driver to invalidate the cache when any processor writes to the shared memory block. This action is necessary because core A could write to block 2 and core B could have block 2 stored in cache. The cache would need to be invalidated on core B so that core B could have the most recent data.  | 
The first attribute must identify the type of access: RAM or ROM. The rest of the attributes can be specified in any order. The vertical bar "|" character is used to separate multiple attributes. For example, RAM|SH4C|CACHE and RAM|CACHE|SH4C are both valid.
The access type (RAM vs. ROM) is from the debug probe's perspective, not the CPU.
To Debug Shared Memory
There are two basic debugger actions that you should keep in mind when debugging shared memory.
When writing to shared memory or reading from shared memory, the debugger knows what read/write access is allowed for each of the different processors and will choose a correct processor to do the write or read. For example, if core A has Read and Write access to shared memory and core B has Read-only access, you may still write to the shared memory using core B. The debugger will automatically switch to core A to do the actual write.
Any software breakpoint set in shared memory will be set on every accessible processor. Software breakpoints can even be set on processors with Read-only access provided that there is at least one processor with Read and Write access to the shared memory. For example, if a breakpoint is set in a source file, that breakpoint will be set on the other processors as well. The only known restriction is that breakpoints can only be connected to one source on one processor. If a breakpoint must also be connected to something on a second processor, a second breakpoint (at the same address) must be added. This second breakpoint can then be connected to the second processor.
___
See also: