7.9.1.3. Calling GEL FunctionsΒΆ

A GEL function can be called from anywhere in the GEL file there is a valid C expression - all functions are global.

They can also be called from any dialog box that accepts a valid C expression, as well as from the Scripting Console by using the function eval('name of GEL function').

Passing parameters to a GEL function is optional. Omitted arguments assume default values.

___

See also:

GEL Functions: Alphabetical List