7.9.1.24. Register accessΒΆ
Accessing registers from GEL can be done either via a direct definition using preprocessing statements such as #define
(details at the online CCS Help) or using any register name shown in the Registers view of CCS.
Both methods have global scope - i.e., can be used by any function of the GEL file.
Registers defined via macro:

Registers globally accessible:

Note
the global registers are defined by the CCS Module XML files. Details about this proces are shown in the section Debug Overview.
___
See also: