7.9.8.58. GEL_RefreshWindowsΒΆ
Forces a refresh of all IDE windows
Format
GEL_RefreshWindows();
Parameters
None
Description
This function causes the Disassembly window, Mixed Mode window, Register window, Memory window and the Watch window to refresh their contents with what is on the target. This can be useful if target memory is changing while the target is halted, such as due to a DMA transfer.
Synchronous
Synchronous from GEL: No
Completely synchronous: No
Example