7.9.8.73. GEL_SharedMemHaltOnWriteOff()ΒΆ
Affected cores are not halted during a write to shared memory.
Syntax
GEL_SharedMemHaltOnWriteOff( void );
Parameters
None
Description
Multiple cores on a single processor can share a block of memory. While writing to memory, the breakpoints in that block have to be cleared for a short time by the driver. This function specifies that other cores with executable code on that block are not halted.
Synchronous
Synchronous from GEL: Yes
Completely synchronous: Yes
Example
GEL_SharedMemHaltOnWriteOff();
Related Topics