7.4.4. List of importProject Options¶
Note that the available options can vary depending on the Code Composer Studio™ version used. For the list of options available for your specific Code Composer Studio version, run the command with the '-ccs.help' option:
ccs-server-cli -noSplash -workspace "<workspace_dir>" -application com.ti.ccs.apps.projectImport -ccs.help
Full list of projectImport options:
-ccs.location '<path>'
Absolute or relative path to the location containing the project.
Relative paths will be assumed to be relative to the working directory.
-ccs.device <id>
The device-variant ID. Applicable only when '-ccs.location' flag resolves to a .projectspec file.
-ccs.definePathVariable <name> <value> [@scope (global|project)]
Defines the given path-variable for resolving portable linked file paths (optional)
(also defines a global build-macro with the same name and value).
Optionally, specify the scope (defaults to 'global').
-ccs.copyIntoWorkspace
Copy project folder and contents into the workspace directory (optional).
Defaults to 'false'.
-ccs.renameTo <name>
Rename the imported project to the specified name.
-ccs.overwrite
Forces overwrite of existing file-system resources (optional).
-ccs.autoBuild
Performs an incremental build on the imported/created project (optional).
-ccs.autoImportReferencedProjects
If 'true', an attempt is made to automatically import any referenced projects found in the same parent directory as the main project.
-ccs.autoRenameReferencedProjects
If 'true', and iff the '-ccs.renameTo' flag is present, any imported referenced projects will also be renamed automatically.
-ccs.referencedProjectSearchDirectory
Directory to search for referenced projects. Applicable only when '-ccs.autoImportReferencedProjects' flag is present.
-ccs.captureCopiedFileOrigins
Capture the original locations of all resources copied into the project during the import. These will be captured into a text file named 'copiedFileOrigins.txt'.
-ccs.captureProjectspecApplicability
Capture the list of devices that the imported projectspec is applicable to. These will be captured into a text file named 'projectSpecApplicability.txt'.
-ccs.defaultImportDestination '<dir>'
Default import-destination. This is the workspace where user-projects will be created/imported by default.
-ccs.args '<file>'
File containing any extra arguments (optional).
-ccs.help
Print this help message.