# Introduction
In some development environments, a full featured ELF or COFF executable file
cannot be accepted as an input by tools such as a flash programmer or boot
loader.  These tools require a simpler form of the executable that is called a
binary file.  This article explains these binary files.
The term *binary file* is misleading.  Please do not confuse it with the
general term for any file that contains more than plain text.  As used in
this article, the term *binary file* refers to a particular variant of binary
files that are not plain text files.
# Binary Files Defined
One of the older ways to create a binary file is with the Unix utility
objcopy.  Here is the description of the format from the objcopy man page ...
> When objcopy generates a raw binary file, it will essentially produce a memory dump of the  contents of  the input object file.  All symbols and relocation information will be discarded.  The memory dump will start at the load address of the lowest section copied into the output file.
The rest of this article elaborates on this description, and discusses related
issues.
# Diagram
This diagram illustrates what happens when an executable file is used to
create a binary file.

# Diagram Explanation
The left side represents a full featured ELF or COFF file named file.out.  The
right side represents the corresponding binary file named file.bin.
Regarding file.out ...  This contrived file has three sections.  The first
two are initialized sections named secA and secB.  The last one is an
uninitialized section named .stack.  For each section, a few key properties
are shown.  This includes the name, address, and length.  For the initialized
sections, the full contents of the raw data are shown.  An uninitalized
section like .stack reserves space in system memory, but has no contents.  
Regarding file.bin ... This diagram shows the full contents of file.bin.  It
only contains the raw data from file.out.  This raw data appears in address
order.  Thus secB, which is at the lowest address 0x100, appears first.  There
is a gap between the end of secB and the start of secA.  In the simple format
of a binary file, the only way to represent such a hole is to fill it.  
Unintialized sections, which have no raw data, are ignored.
# Addresses in a Binary File
Compare the address with the file offset in the binary file.  They are related,
but they do not match.  Here is one way to represent the relationship.
    target address = lowest initialized address + file offset
The term *lowest initalized address* is the starting address of the
initialized section with the lowest address.  In this diagram, that is secB at
address 0x100.
A binary file does not record the starting address.  That detail is maintained
in some other manner.
If an initialized section has different load and run addresses, the load
address is used, and the run address is ignored.
# Holes in a Binary File
The format of a binary file is very simple.  There is no compact way to
represent a hole.  The only possible way to represent a hole is to fill it.
The value zero is usually used to fill holes.  If the binary file is created
with a variant of an objcopy utility, see if that utilty supports an option
named --gap-fill.  If so, it can be used to fill a hole with a value other
than zero.
## Avoiding Holes
The best way to avoid holes is to carefully control the placement of the
initialized sections in the executable.  Put them as close together as
possible.  In an ideal configuration, they are all adjacent to each other.
Sometimes holes cannot be avoided.  If that is the case, see if one of these
two alternatives is practical.
One alternative is to create separate bin files.  If there are two clusters of 
initialized sections, then create one bin file for each cluster.  This approach
is not always practical.  The utility that creates the bin file may not
support it.  Or, the utility that reads the bin file as input may accept only 
one file.
The second alternative relies on two presumptions.  One, all of the initialized
sections are close together accept one.  Two, there is room in memory near the
main cluster of initialized sections.  In that case, arrange for that remaining
initialized section to have different load and run addresses.  It loads at an
address near the main cluster of initialized sections.  As part of system
startup, it is copied to a different run address.
# Example
This example matches the diagram.  Therefore, it is not a realistic program.
Instead, it is much smaller and easier to understand.  It introduces several
utilities.  A good way to learn about such utilities is with small examples.
Make changes in the input files, or how the utilities are used, and observe
how the results change.
The [TI ARM Clang compiler tools](https://www.ti.com/tool/ARM-CGT) are used
to build and inspect these files.
Here is the assembly source code file.s ...
```c
@ file.s
        .section        secA,"a",%progbits
        .skip           8,0xAA
        .section        secB,"a",%progbits
        .skip           16,0xBB
        .section        .stack,"aw",%nobits
        .zero           0x800
```
Here is the linker command file file.cmd ...
```c
/* file.cmd */
/* Do NOT use this setting in a production build.  It is used in this       */
/* contrived example to prevent the linker from removing sections which are */
/* not used by the program.                                                 */
--unused_section_elimination=off
SECTIONS
{
   secB   > 0x100
   secA   > 0x120
   .stack > 0x200
}
```
These commands:
1. Build file.s to create the object file file.o
2. Link file.o to create the final executable file.out.  The linker map file file.map is also created.
```
% tiarmclang -c file.s
% tiarmclang file.o -o file.out -Wl,file.cmd -Wl,-m=file.map
warning: no suitable entry-point found; setting to 0
```
Ignore the warning.  This example is not a real program, so there isn't an
entry point.
There are few different ways to see the sections that have been created.
These are the keys lines from the linker map file file.map ...
```
secB       0    00000100    00000010
                  00000100    00000010     file.o (secB)
secA       0    00000120    00000008
                  00000120    00000008     file.o (secA)
.stack     0    00000200    00000800     UNINITIALIZED
                  00000200    00000800     file.o (.stack)
```
The object file display utility could be used.  Here is the command and a
few key lines from the output ...
```
% tiarmofd file.out
...
 Section Information
    id name                      load addr  run addr    size align alloc
    -- ----                      ---------  --------    ---- ----- -----
     0 (no name)                 0x00000000 0x00000000   0x0     0   N
     1 secB                      0x00000100 0x00000100  0x10     1   Y
     2 secA                      0x00000120 0x00000120   0x8     1   Y
     3 .stack                    0x00000200 0x00000200 0x800     8   Y
...
```
Another way to see this information is with the readelf utility ...
```
% tiarmreadelf -S file.out
...
Section Headers:
  [Nr] Name              Type            Address  Off    Size   ES Flg Lk Inf Al
  [ 0]                   NULL            00000000 000000 000000 00      0   0  0
  [ 1] secB              PROGBITS        00000100 000034 000010 00   A  0   0  1
  [ 2] secA              PROGBITS        00000120 000044 000008 00   A  0   0  1
  [ 3] .stack            NOBITS          00000200 000050 000800 00  WA  0   0  8
...
```
Use the the objcopy command to create the binary file file.bin.
```
% tiarmobjcopy -O binary file.out file.bin
```
One way to inspect a binary file is with a binary file editor.  Another way
is to use a utility to dump it out.  Here is an example that uses a utility
from Unix named od ...
```
% od -Ax -t x1 -w4 -v file.bin
000000 bb bb bb bb
000004 bb bb bb bb
000008 bb bb bb bb
00000c bb bb bb bb
000010 00 00 00 00
000014 00 00 00 00
000018 00 00 00 00
00001c 00 00 00 00
000020 aa aa aa aa
000024 aa aa aa aa
000028
```
The command line arguments to od are not standardized.  Here is what they mean
in this particular case.
* -Ax : Use hexadecimal for the file offset
* -t x1 : Format each byte as a separate 8-bit hex value
* -w4 : Show 4 bytes per line
* -v : Output all the lines, even if they are duplicates