# Overview
The Debug Server Scripting (DSS) Test Server example creates a [**Debug Server Scripting**](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html) (DSS) instance for a [target configuration](https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_debug-main.html#target-configuration-files) and starts a debug session for all debuggable cores on the target in its own Java thread. Each thread will then listen for commands on an open TCP/IP socket. Remote clients can communicate to the active debug session by connecting to the socket and sending appropriate commands.
# Dependencies and Setup
DSS and the DSS Test Server example come bundled with Code Composer Studio (CCS). Hence an installation of CCS is required.
[[+y If you are using CCSv9.0.x or earlier (expand)
The DSS Test Server example has been updated in CCSv9.1.0. To use the updated example with older CCS versions, please download the [latest example](./test_server/TestServer.zip) and use it to replace the existing obsolete example found in [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer. You can rename the existing **TestServer** folder and then extract the newly downloaded **TestServer.zip** in [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples to replace it.
+]]
The scripts that configure and start the DSS Test Server are written in [JavaScript](https://developer.mozilla.org/en-US/docs/Web/JavaScript) (the native scripting language supported by DSS). However, the remote client script example that sends commands to the DSS Test Server is written in [Perl](https://www.perl.org/). Hence an installation of Perl is needed to use the Perl script "as-is". The [JSON (JavaScript Object Notation) encoder/decoder Perl module](https://metacpan.org/pod/JSON) also needs to be installed.
[[b NOTE
While the client script for this particular example was written in Perl, any language of choice can be used communicate to the remote server and send the desired debug commands to the target. See the [Format](#format) section for more details on how the commands should be formatted.
]]
Both the client Perl script (**perl_client.pl**) and DSS server JavaScript (**test_server.js**) are configured to run the [SYS/BIOS **hello** example](https://dev.ti.com/tirex/content/simplelink_cc2640r2_sdk_2_40_00_32/examples/rtos/CC2640R2_LAUNCHXL/sysbios/hello/README.html) for the [CC2640R2 LaunchPad](https://www.ti.com/tool/LAUNCHXL-CC2640R2).
To configure the example to use a different target/example:
1. Open the **test_server.js** script (located at: [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer) in your text editor.
2. Modify **line 6** of the JavaScript by replacing **CC2640R2F.ccxml** with the name and path of the [target configuration file](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html#target-configuration) for your target.
3. Modify **line 11** of the JavaScript by replacing **Texas Instruments XDS110 USB Debug Probe/Cortex_M3_0** with the unique name for the connection/CPUName for your target configuration. For more example on unique names, please see the **openSession()** API examples mentioned in the [DSS guide](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html#multiple-debug-sessions-for-multi-core-debug).
4. Open the **perl_client.pl** script (located at: [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer) in your text editor.
5. Modify **line 84** of the perl script by replacing **hello_CC2640R2_LAUNCHXL_tirtos_ccs.out** with the name and path of the program to be used.
6. Save all files.
[[b NOTE
Nearly all the SimpleLink SDK packages come with the SYS/BIOS **hello** example. In [**Resource Explorer**](https://software-dl.ti.com/ccs/esd/documents/users_guide/ccs_getting-started.html#resource-explorer), under the tree view, expand and select **Software → SimpleLink (YourDeviceFamily) SDK - v:(X.X.X.X) → Examples → Development Tools → (YourLaunchPad) → TI-RTOS Kernel (SYS_BIOS) → hello → TI-RTOS → CCS Compiler → hello**
]]
## Start the Test Server:
Open a command window by running the **setenv.bat** file located at: [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer
Start the Test Server example by running the **test_server.js** script:
```text
> dss test_server.js
```
The Test Server will take a few moments to start up. You will know it is fully up when you are notified that the *TestServer is ready*.

[[y NOTE
Linux/MacOS users will not be able to set up the environment with the Windows specific **setenv.bat** file. Please refer to the batch file and then configure your environment accordingly.
]]
## Run the Test Server Client example:
Open a command window by running the **setenv.bat** file located at: [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer
Run the Client example by running the **perl_client.pl** script (located at: [CCS_INSTALL_DIR]/ccsv[x]/ccs_base/scripting/examples/TestServer) and passing in the host and port of the Test Server debug session you wish to connect to. For this example, use **localhost** for the host and port number **4444**.
```text
> perl perl_client.pl "localhost" 4444
```
This will run the Client example for the specified debug session. A series of messages will appear in both consoles as messages are being passed between the client and server. The client script will open a connection to specified host and port number, and then send a series of commands that the server will receive and attempt to execute on the associated debug session. The status of the command will be sent back to the client (**OK** or **FAIL**). Any failure will also have an associated message describing the cause of the failure. Note that the client script *intentionally* has some invalid commands to demonstrate how failures are handled.
[[y NOTE
The client script sends the [**stop**](#stop) command towards the end of the script. This will remotely shutdown the test server, preventing any future remote connections, and requiring a restart of the test server. Do not send the **stop** command if your wish to have the test server running and available for future connections.
]]
# Commands
## Format
The format of the data communicated between the host and client are JSON objects. [JSON (JavaScript Object Notation)](https://www.json.org) is a lightweight computer data interchange format based of JavaScript.
JSON objects are a set of name/value pairs. An object begins with "{" and ends with "}". Each name is followed by ":" and the name/value pairs are separated by ",".
Example:
```json
{"name":"timeout","timeout":10000}
```
### Using the DSSClient Perl Module
The **DSSClient** Perl module provides an **execute** function that can take a Perl data structure and encode it to JSON format. Hence one simply needs to format the command they wish to send to the Test Server in a data structure and use the execute command to encode it to the JSON format and send the command. For example, the **halt** command (to halt the target) has no parameters. The element in the data structure would be the name of the command:
```perl
# Halt the target
$cmd = {
"name" => "halt",
};
```
The first element is always the name of the command.
Let's take a look at a command with many parameters... like the **loadRawFromFile** command (load a binary file from the PC to target):
```perl
# Load binary file to memory.
$cmd = {
"name" => "loadRawFromFile",
"page" => 0,
"address" => 0x10000,
"file" => "loadRawFromFile.bin",
"wordSize" => 32,
"byteSwap" => 0,
};
```
---
All commands return a status to indicate if the command succeeded (**OK**) or failed (**FAIL**). In JSON format, it would be status":"OK" or status":"FAIL". The command can also return additional values, usually a failure message if the command failed, or data if it is a command requesting data (such as **readData**).
## List of Commands
The following commands are currently supported. Since many of the commands call an equivalent [DSS API](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html#dss-api), it is recommended to get familiar with the DSS API documentation for a better understanding of the commands.
---
### stop
Close the socket
**Format**
{"name":"stop"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### connect
Connect to the target
**Format**
{"name":"connect"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### disconnect
Disconnect from the target
**Format**
{"name":"disconnect"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### load
Loads a program on the target
**Format**
{"name":"load","program":[file name]}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### run
Synchronous run command. This command will block until the program is halted or a script timeout occurs
**Format**
{"name":"run"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### runAsynch
Asynchronous run command. This command will run the target and return
**Format**
{"name":"asynch"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### halt
Halt the target
**Format**
{"name":"halt"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### reset
Reset the target
**Format**
{"name":"reset"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### timeout
Set the DSS timout value for synchronous APIs
**Format**
{"name":"timeout","timeout":[value]}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### redirectCIO
Redirect CIO messages to a file
**Format**
{"name":"redirectCIO","file":[file name]}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### setBreakpoint
Set a breakpoint on an address or symbol
**Format**
{"name":"setBreakpoint","address":[address value (int) or symbol name (string)]}
**Returns**
status (OK or FAIL), message (breakpoint ID or failure message)
---
### removeAllBreakpoints
Remove all set breakpoints
**Format**
{"name":"removeAllBreakpoints"}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### loadRawFromFile
Load a binary file to target memory
**Format**
```text
{
"name":"loadRawFromFile",
"page":[memory page],
"address":[address value],
"file":[file name],
"wordSize":[size of word (in bits)],
"byteSwap":[byte swap enable ('0' = false, '1' = true)]
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### saveRawToFile
Save target memory contents to a binary file
**Format**
```text
{
"name":"saveRawToFile",
"page":[memory page],
"address":[address value],
"file":[file name],
"length":[number of bytes],
"wordSize":[size of word (in bits)],
"byteSwap":[byte swap enable ('0' = false, '1' = true)]
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### loadDataFromFile
Load a *.dat file to target memory
**Format**
```text
{
"name":"saveRawToFile",
"page":,
"address":,
"file":,
"length":
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### saveDataToFile
Save target memory contents to a *.dat file
**Format**
```text
{
"name":"saveRawToFile",
"page":[memory page],
"address":[address value],
"file":[file name],
"length":[number of bytes],
"ioFormat":[see DSS API documentation for ioFormat values],
"append":[enable append to file ('0' = false, '1' = true)]
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### loadGel
Load a GEL file
**Format**
{"name":"loadGel","file":[file name]}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### runGel
Run a GEL expression
**Format**
{"name":"runGel","expression":[GEL expression]}
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### readData
Read one integer value from memory
**Format**
```text
{
"name":"readData",
"page":[memory page],
"address":[address value],
"typeSize":[bit size of value to read],
"signed":[return value is signed ('0' = false, '1' = true)]
}
```
**Returns**
status (OK or FAIL), value (if status is OK), message (if status is FAIL)
---
### writeData
Write one integer value to memory
**Format**
```text
{
"name":"writeData",
"page":[memory page],
"address":[address value],
"value":[value to write],
"typeSize":[bit size of value to write]
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
### readDataArray
Read multiple values from memory
**Format**
```text
{
"name":"readDataArray",
"page":[memory page],
"address":[address value],
"typeSize":[bit size of the values to read],
"numValues":[number of values to read],
"signed":[return value is signed ('0' = false, '1' = true)]
}
```
**Returns**
status (OK or FAIL), value (if status is OK), message (if status is FAIL)
---
### writeDataArray
Write multiple values to memory. The values parameter takes a string of values delimited by a comma ("1,2,3,4")
**Format**
```text
{
"name":"writeData",
"page":[memory page],
"address":[address value],
"values":[values to write to memory],
"typeSize":[bit size of values to write]
}
```
**Returns**
status (OK or FAIL), message (if status is FAIL)
---
## Custom Commands
Additional custom commands can be created. Simply create them in your server side script and add them using the **addHandlers()** API. See **test_server.js** for an example.
# Files
The following four files are the core files that the examples depend on.
* **DSSClient.pm** - Perl module that enable customers to talk over a TCP/IP socket to a DSS TestServer as implemented in **TestServer.js**. Requires a version of Perl with JSON support. This file is only needed by Perl based client scripts.
* **json2.js** - JSON utility JavaScript file that creates a global JSON object containing two methods: **stringify** and **parse**.
* **TestServer.js** - JavaScript file where the bulk of the functionality is found, implemented in JavaScript/DSS. Starts a DSS instance for a specified target configuration, and then starts a debug sessions for all debuggable cores, each in its own Java Thread and waits for connections/commands on a TCP/IP socket per session.
* **readme.txt** - Link to this document.
The rest of the files are example files that would vary between users and is provided as an example on how to use the above (minus **readme.txt**) core scripts. The key files to be aware of are:
* **perl_client.pl** - Example client script. Demonstrates the use of **DSSClient.pm** by creating a **DSSClient** instance and sending scripting commands to an active DSS Test Server debug session.
* **test_server.js** - Example server script. Demonstrates the use of **TestServer.js**. By default, it will start a the DSS Test Server for a CC2640R2 LaunchPad. Also defines some additional custom commands that can be called from the remote client.
* **setpath.bat** - Windows batch file that configures the environment **PATH** and **PERL5LIB** variables needed to run the Test Server and examples.