Overview
---
JavaScript is the default scripting language supported by [DSS](https://software-dl.ti.com/ccs/esd/documents/users_guide/sdto_dss_handbook.html). However, DSS is implemented as a set of Java APIs, thus any language that supports importing and using Java classes can be used with DSS. [Jython](http://en.wikipedia.org/wiki/Jython) is an implementation of Python written in Java, and hence falls into this category.
Prerequisites
---
### Software
* [Code Composer Studio (CCS)](https://processors.wiki.ti.com/index.php/Download_CCS) (preferably version 8 or later)
* An installation of [Jython](http://en.wikipedia.org/wiki/Jython) (tested with Jython 2.7.0)
* Compatible Java Runtime Environment (JRE), depending on the CCS version used (see the table)
| OS |
Requires 32-bit JDK |
Requires 64-bit JDK |
| Windows |
Up to CCS v8.x |
CCS v9 and above |
| MacOS |
None |
All |
| Linux |
Up to CCS v6.1.3 |
CCS v6.2.0 and above |
{{b The CCS installation contains a compatible JRE (can be found in <CCS_INSTALL_DIR>/eclipse/jre). To use it, make sure to point Jython to its location (can be done by setting the `JAVA_HOME` environment variable).}}
### Setting Up the Environment
Before running a Jython DSS script, the following JAR files should be added to the `CLASSPATH` environment variable:
* <CCS_BASE_DIR>/DebugServer/packages/ti/dss/java/dss.jar
* <CCS_BASE_DIR>/DebugServer/packages/ti/dss/java/com.ti.ccstudio.scripting.environment_3.1.0.jar
* <CCS_BASE_DIR>/DebugServer/packages/ti/dss/java/com.ti.debug.engine_1.0.0.jar
Here <CCS_BASE_DIR> refers to the ccs_base directory in the CCS installation. For example, in CCS 8 it would be <CCS_INSTALL_DIR>/ccsv8/ccs_base.
[[b Tip:
This can be done in a batch/shell script to setup the environment before running Jython. You can even have the same batch/shell script run the Jython script afterwards to automate everything with the execution of one script.]]
Creating and Running a Jython script
---
### Importing the DSS Java Classes
The following DSS Java classes should be imported by the Jython script:
```python
from com.ti.debug.engine.scripting import *
from com.ti.ccstudio.scripting.environment import *
```
Now your Jython script can call the DSS APIs.
### Running your Jython script
You can run your DSS Jython script as you would any other Jython script. For example:
```diff
jython my_script.py
```
### Example Script
Below is an example DSS Jython script. It is a port of the **msp430f5529_breakpoints.js** example that comes with CCS (you can find the example in <CCS_BASE_DIR>/scripting/examples/DebugServerExamples/).
```python
from java.lang import *
from java.util import *
from com.ti.debug.engine.scripting import *
from com.ti.ccstudio.scripting.environment import *
# Create our scripting environment object - which is the main entry point into any script and
# the factory for creating other Scriptable Servers and Sessions
script = ScriptingEnvironment.instance()
# Create a log file in the current directory to log script execution
script.traceBegin("BreakpointsTestLog_python.xml", "DefaultStylesheet.xsl")
# Set our TimeOut
script.setScriptTimeout(15000)
# Log everything
script.traceSetConsoleLevel(TraceLevel.ALL)
script.traceSetFileLevel(TraceLevel.ALL)
# Get the Debug Server and start a Debug Session
debugServer = script.getServer("DebugServer.1")
debugServer.setConfig("../msp430f5529/msp430f5529.ccxml");
debugSession = debugServer.openSession(".*")
debugSession.target.connect()
# Load a program
# (ScriptingEnvironment has a concept of a working folder and for all of the APIs which take
# path names as arguments you can either pass a relative path or an absolute path)
debugSession.memory.loadProgram("../msp430f5529/programs/modem.out")
# Set a breakpoint
address = debugSession.symbol.getAddress("ReadNextData")
bp = debugSession.breakpoint.add(address)
# Using an expression - get the current value of the PC
nPC = debugSession.expression.evaluate("PC")
scriptEnv.traceWrite("Current halted at {}. This should be at the start of main().".format(hex(nPC)))
# Run the target. Should halt at our breakpoint.
debugSession.target.run()
nPC = debugSession.expression.evaluate("PC")
# Verify we halted at the correct address.
if (nPC == address):
script.traceWrite("SUCCESS: Halted at correct location")
else:
script.traceWrite("FAIL: Expected halt at " + hex(address) + ", actually halted at " + hex(nPC))
script.traceSetConsoleLevel(TraceLevel.INFO)
script.traceWrite("TEST FAILED!")
script.traceEnd()
System.exit(1);
# All done
debugSession.terminate()
debugServer.stop()
```