C function parameters can be passed by value (e.g. int value) or by reference (e.g. int *value). When passing by value, the compiler needs to generate code to copy the variables' values into the general-purpose registers and the stack. The registers have faster access time but are limited in number hence they are used for the first small variables. For larger variables such as structures or unions, the stack located in RAM is required to store the additional data. Copying of the data structures requires additional code execution. When passing by reference, the function only needs to copy the addresses of the variables, limiting the overall data-copying instructions to the number of the parameters of the function. This greatly reduces the number of instructions being executed each time the function is invoked.
Notice that in C, arrays are by default pointers and hence technically are already passed by reference.
Passing large variables such as structures & unions can generate additional code executions for the function, depending on the size of the data being passed. The impact increases significantly if the function is frequently invoked.
At least one function in the project passes a structure or union
by value.
If the size of the structure or union is significant, change the function parameter passing method to pass by reference.
/*-------------ULP 9.1-------------------------------------------------
*
* Detect structures or unions being used as function parameter
*
* NOTICE that arrays are automatically treated as pointers so this rule
* should not raise the flag for passing array parameters
*
*-------------ULP9.1-------------------------------------------------*/
#include "msp430.h"
typedef struct
{
unsigned char variable1;
int variable2;
char variable3[3];
} structOne;
structOne structVariable, *structPointer;
typedef union
{
int variable1;
char variable2;
char variable5[5];
} unionOne;
unionOne unionVariable, *unionPointer;
char array[30];
//----------------------------------------------------------
//--------- STRUCTURE EXAMPLE -------------------------
//----------------------------------------------------------
void ULP9_1_BadExample1(structOne structVariableParam)
{
if (structVariableParam.variable2 > 0)
P1DIR |= BIT0;
}
void ULP9_1_GoodExample1(structOne* structVariablePointer)
{
structVariablePointer->variable2 = 0xBEEF;
if (structVariablePointer->variable2 > structVariablePointer->variable1)
P1DIR ^= BIT0;
}
//----------------------------------------------------------
//--------- UNION EXAMPLE -----------------------------
//----------------------------------------------------------
void ULP9_1_BadExample2(unionOne unionVariableParam)
{
unionVariableParam.variable1 = 0xBEEF;
}
void ULP9_1_GoodExample2(unionOne* unionVariablePointer)
{
unionVariablePointer->variable1 = 0xBEEF;
}
//----------------------------------------------------------
//--------- ARRAY EXAMPLE -----------------------------
//----------------------------------------------------------
void ULP9_1_GoodExample3(char array[30])
{
array[0] = 1;
}
void ULP9_1_Examples(void)
{
ULP9_1_BadExample1(structVariable);
ULP9_1_BadExample2(unionVariable);
//-------Good examples-----------------
ULP9_1_GoodExample1(&structVariable);
structPointer = &structVariable;
ULP9_1_GoodExample1(structPointer);
ULP9_1_GoodExample2(&unionVariable);
unionPointer = &unionVariable;
ULP9_1_GoodExample2(unionPointer);
ULP9_1_GoodExample3(array);
}
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Hold watchdog timer
ULP9_1_Examples();
}
See the
rest of the code examples for all MSP430 devices here!
Want to squeeze a few more nanoAmps out of your application? Leverage the e2e (Engineer-to-Engineer) online community to get all of your ULP questions answered! Or, if you are an Ultra-Low Power pro, give back to the community with your expertise.
Go to MSP430's e2e online forum!
If you are posting on the forums in relation to this rule, try using the tag "ULP_9.1"
|
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Compiler/diagnostic messages/MSP430/1537 here. |