"For FRAM devices, at start up, the GPIO power-on default high-impedance mode needs to be disabled to activate previously configured port settings. This can be done by clearing the LOCKLPM5 bit in PM5CTL0 register."
Upon exit from LPMx.5, all peripheral registers are set to their default conditions but the I/O pins remain locked while LOCKLPM5 remains set. Keeping the I/O pins locked ensures that all pin conditions remain stable when entering the active mode, regardless of the default I/O register settings.
If the LOCKLPM5 bit is not cleared, all GPIO pins remain in
default high-impedance mode and cannot be reverted back to
previously configured settings.
The PM5CTL0.LOCKPM5 bit clearing code instruction cannot be
detected in the project.
Insert the following line of code at the beginning of the project:
// Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5;
Refer to FRAM device code examples from CCS - TI Resource Explorer or as downloadable packages at https://www.ti.com/lsds/ti/microcontroller/16-bit_msp430/tools_software.page#code
Refer to the MSP430 Family User's Guides for FRAM devices for more details.
For more questions/answers,Go to
MSP430's e2e online forum!
If you are posting on the forums in relation to this rule, try using the tags "DiagMessage_10420" and "FRAM_GPIO_Usage"
|
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Compiler/diagnostic messages/MSP430/10420 here. |