This error occurs when the linker is parsing a linker command file and finds an invalid section type following a section definition. If you see below error then you might have MSP CGT 4.1.x device linker command files being used with the 4.0.x version of MSP compiler.
"lnk_msp430f5438a.cmd", line 177: error #10030-D: expecting section type (COPY, DSECT, or NOLOAD) instead of "VECT_INIT"
MSP430 compiler revision 4.1.x has a new feature for section type=VECT_INIT. For details see: [1]
This error can be avoided using below remedy. Once doing below if
you instead get a warning for “no matching section” then you may
need to generate an interrupt ISR. However, uninitialized ISR
vectors when triggered could lead to jumping to unknown addresses,
execution of erroneous code which at the very least could lead to
application crashing, unexpected application behavior, or more
severely memory erasure or electrical damage.
The most likely scenario to generate this error is if a CCS 5.2.0
project was created and then later the compiler version choice was
changed from 4.1.x back to 4.0.x. CCS 5.2.0 includes new MSP CGT
4.1.0 and the associated linker command files containing section
type=VECT_INIT.
Either replace the lnk_msp430xxxx.cmd file with an older version or edit your project’s lnk_msp430xxxx.cmd file to remove “type=VECT_INIT”. You will still get below warnings about “no matching section” due to having explicit section specifiers eg: { * ( .int14 ) }:
"lnk_msp430f5438a.cmd", line 165: warning #10068-D: no matching section
Section entries for lnk_msp430f5438a.cmd as included with MSP CGT 4.1.x:
.int38 : {} > INT38
.int39 : {} > INT39
.int40 : {} > INT40
RTC : { * ( .int41 ) } > INT41 type = VECT_INIT
PORT2 : { * ( .int42 ) } > INT42 type = VECT_INIT
USCI_B3 : { * ( .int43 ) } > INT43 type = VECT_INIT
USCI_A3 : { * ( .int44 ) } > INT44 type = VECT_INIT
Version of above included in MSP CGT 4.0.x:
.int38 : {} > INT38
.int39 : {} > INT39
.int40 : {} > INT40
.int41 : {} > INT41
.int42 : {} > INT42
.int43 : {} > INT43
.int44 : {} > INT44
Refer to our following code example for guidance on using and initializing interrupt vectors.
processors.wiki.ti.com/index.php/File:Msp430_initialize_unused_interrrupt_vectors.zip
See the rest of the code examples for all MSP430 devices here!
Leverage the e2e (Engineer-to-Engineer) online community to get all of your MSP430 questions answered! Or, if you are an MSP430 pro user, give back to the community with your expertise.
Go to MSP430's e2e online forum!
|
For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article Compiler/diagnostic messages/MSP430/10030 here. |