Relocation is one of the jobs performed by the linker. When a function is called or a variable is accessed, the assembly language source code refers to the function or variable by its name (in object file terminology, this is the symbol). The assembler does not know the machine address of the symbol, so it leaves a blank hole (the relocation field) in the object file where the address needs to go, and creates a relocation, which tells the linker that it needs to fill in the field. For each relocation, the linker fills in the relocation field with the machine address of the referred-to function or variable.
However, sometimes the address does not fit in the field. This is called a relocation overflow.
A complete explanation of every possible way you can get relocation overflow would make this page too long. What follows is a quick overview to help you understand what relocation overflow is, and how to look for more help fixing it.
When deciphering a relocation overflow error message, it is important to know whether the referred-to symbol is a function or variable, whether the relocation field itself is in a code section or data section, and what type of relocation it is. There are many relocation types, which fall into these broad categories:
An absolute relocation requires the entire machine address to be placed in the relocation field. An absolute relocation is usually the result of the C address-of operator. For example:
int *pointer = &object;
int *function(void) { return &object; }
It is unusual for an absolute relocation to overflow.
A PC-relative relocation is usually found in a branch or call. Some targets (ARM, MSP430) support PC-relative addressing of data. In a PC-relative relocation, the value that needs to be placed in the relocation field is the offset from the current PC of the referred-to function or variable. The offset is the difference between the address of the instruction containing the relocation field (for some architectures, a nearby address such as the fetch packet start) and the address of the referred-to function or variable. PC-relative addressing is usually used because the absolute address would be too large to encode in a single instruction, so a field smaller than the size of an address is used. However, because the field is smaller than the address width, it has a limited reach. That is, it can only refer to addresses that are within a certain limit.
A typical scenario for PC-relative relocation overflow is on C6200 when "near" code memory model is used. The C6200 has a call instruction which has only a 21-bit offset, but the width of an absolute address is 32 bits. If the call destination is more than pow(2,23) bits away (21 bits, plus 2 bits for scaling), the call instruction cannot reach the target function.
For extremely large functions, it is possible to have a branch within the function that cannot reach the destination. This is very rare.
Static-base-relative (also known as .bss-relative, DP-relative and data-page-relative) relocations are similar to PC-relative relocations, but they are instead relative to a known fixed location (such as the starting address of the .bss section).
Until the relocation overflow is fixed, the program will not link.