fatal error #16000: object files have incompatible formats
("/db/lang/msp/exec/rts430_eabi.lib" = ELF, "example.obj" =
TI-COFF)
The linker has been supplied with object files or libraries that were compiled with different, incompatible object file formats.
The linker can only combine object files and libraries of a single object file format, but files of multiple object file formats were specified. The object file format is controlled by the application-binary interface (ABI), so ultimately files were compiled with a different --abi option. Since the object files for your project are compiled according to the build options this is usually an issue with using a library file built for a different ABI.
Make sure all of the pre-built object and library files are built for the ABI that you are using. You can verify the ABI being used by looking at the --abi option in the build options dialog. If you are explicitly specifying the RTS library to be used through the --library option you can remove it -- the linker will automatically include the correct RTS library. If you are using additional libraries provided by TI or 3rd parties please confirm that they are for the correct ABI.
An executable cannot be created until this error is resolved.