#Introduction
Projects that are shared among multiple users should be made portable. Portable projects should essentially avoid absolute paths.
There are two main areas where absolute paths should be avoided:
- When [linking source files](./users_guide/ccs_project-management.html#adding-or-linking-source-files-to-project).
- When specifying compiler include paths and linker search paths.
#Variables
To facilitate the creation of portable projects, there are two kinds of variables supported by CCS - **Path Variables** and **Build Variables**.
**Path Variables** specify locations in the file system. The path to linked source files/resources can be set relative to these variables. This allows you to avoid references to a fixed location on your file system.
**Build Variables** specify locations, strings etc. They can be used in the project build options, for example, when specifying paths for header files or libraries.
You can set paths to be relative to either [predefined variables](#predefined-variables) or [user-defined variables](#user-defined-variables).
To see the complete list of Path variables go to **Project Properties → Resource → Linked Resources → Path Variables** tab.
To see the complete list of Build variables, go to **Project Properties → Build → Variables** tab, and check the box **Show system variables**.
[[b Note:
There are also [Dynamic Variables](#dynamic-variables). These are all predefined, and are only used within Debug Configurations.
]]
##Predefined Variables
Each CCS project contains a predefined set of Path and Build variables. Some of these are defined by Eclipse (such as PARENT_LOC, PROJECT_LOC and WORKSPACE_LOC) and some are defined by CCS (such as CG_TOOL_ROOT, CCS_INSTALL_ROOT).
For example, CG_TOOL_ROOT is set to the root installation directory of the version of compiler tools chosen to build the project. When you change the compiler version used by the project, this variable is automatically updated to the appropriate path for the selected version.
CCS also defines some variables when a TI software product (such as Simplelink SDK, C2000Ware, etc.) is installed into CCS and selected for the project.
An example is COM_TI_SIMPLELINK_XXXX_SDK_INSTALL_DIR (where XXXX is the device name). This variable is automatically set to the root installation directory of the version of Simplelink SDK product selected in the **Project Properties → General → Products** tab. If you have multiple versions of the SDK installed and change the version of SDK used by the project in the **Project Properties → General → Products** tab, this variable is automatically updated to the appropriate path for the selected version.
##User-defined Variables
Custom Build and Path variables can be created at the workspace level or project level.
When you create a new variable at the workspace level it will automatically propagate as both Path variable and Build variable for all projects in the workspace. This is advantageous for projects checked into source control as the project does not have to be modifed with each checkout.
When you create a new variable at the project level it will apply only to that specific project. This allows the project to be portable across different workspaces and computers.
###Creating Variable at Workspace Level
To create a workspace level Build or Path variable:
- Go to menu **Window → Preferences → Code Composer Studio → Build → Variables**.
- Click the **Add** button to define a new variable.
- Specify the **Variable name**, **Type** and **Value**.
- Click **Apply and Close**.
This screenshot shows an example of setting a new variable called MYROOT.

If the **Type** selected is **File**, **Directory** or **Path**, then the variable gets defined as both a Build variable and a Path variable for all projects in the workspace. If the **Type** selected is not one of the above then the variable gets defined as just a Build variable.
Note that for it to be accepted as a Path variable the path should be absolute.
In this example, the **Type** selected is **Directory** so the variable is defined as both a Build variable and Path variable.
To confirm the variable is defined:
- Select any project in the workspace.
- From the context menu, go to **Properties → Resource → Linked Resources → Path Variables** tab.
- Observe that the variable set earlier is shown here.

- Go to **Build → Variables** tab, and check the box to **Show system variables**.
- Observe that the variable set earlier is shown here as well.

This variable can now be used both as a Path variable and as a Build variable.
###Creating Variable at Project Level
To create a project level Build variable:
- Go to **Project Properties → Build → Variables** tab.
- Click the **Add** button to define a new variable.
- Specify the **Variable name**, **Type** and **Value**.
This will define the variable as a Build variable. It will also define it as a Path variable if the **Type** selected is **File**, **Directory** or **Path**.
To create a project level Path variable:
- Go to **Project Properties → Resource → Linked Resources → Path Variables** tab.
- Click the **New** button to define a new variable.
- Specify the **Variable name**, **Type** and **Value**.
This will define the variable as a Path variable and also as a Build variable.
#Linking Source Files
To make a project portable, use Path variables when linking source files to the project. You can use predefined Path variables or custom variables that you created.
To link files relative to the Path variable:
- Select **Add Files** from project context menu, browse and select the file(s) you wish to link.
- In the dialog that comes up, select **Link to files** and choose whether to create a link relative to PROJECT_LOC (selected by default, and resolves to the root folder of the current project) or to one of the other available path variables.

#Specifying Compiler/Linker Options
To make a project portable, use Build variables in the project build options, such as when specifying compiler include paths and linker search paths. You can use the predefined system variables or variables that you created.
Refer to the value of a variable using the syntax ${VAR}. For paths relative to the variable use ${VAR}/dir_name/.
The screenshot below shows an example of using the user-defined variable MYROOT and several predefined variables in the project's compiler include options.

#Sharing Variables File
You can share variables among multiple users by defining the needed variables to an *.ini file that the user can import.
- The file can be automatically read during a project import if:
- the file is named **macros.ini** and
- the file is at the project root location
- Otherwise the file can be manually imported via menu **File → Import → Build Variables**.
- After import, the variables are set both as Path variables and Build variables.
- The variables are set at the workspace level.
The syntax for defining variables in the *.ini file is
VAR = VALUE
By default, variable definitions are assumed to be paths. However, there is support for specifying a string type for the variable. To specify a variable as a string type, prepend the variable definition with [string].
[string] VAR = VALUE
#Portable Target and Debug Configurations
Target configuration files and debug configurations can be made portable by specifying their locations using a relative path instead of absolute path.
##Target Configurations
When a [Target Configuration file](./users_guide/ccs_debug-main.html#target-configuration-files) is linked to a project it defaults to an absolute path. The steps below show how to link a target configuration file and then convert the absolute path to variable relative path:
- Open the **Target Configurations** view (menu **View → Target Configurations**).
- Right-click on the desired target configuration, go to **Link File to Project** and select the project that will use this specific target configuration.
- Go to the **Project Explorer** view, highlight the project selected in the previous step.
- From the project's context menu, go to **Properties → Resource → Linked Resources**. The target configuration file should be shown there.
- Highlight the target configuration and click on **Convert...**. After a few confirmation screens, the path to the target configuration will be automatically changed to a path relative to a variable.
- Click **OK** to accept all changes.
##Debug Configurations
[Debug Configurations](./users_guide/ccs_debug-main.html#debug-configurations) can also be made portable by ensuring that there are no absolute paths used in their fields.
When launching a [project-based debug session](./users_guide/ccs_debug-main.html#automatic-launch) for the first time, the debug configuration generated for that project is portable by default. This is because it uses **Dynamic Variables**.
### Dynamic Variables
In Eclipse (and by extension, CCS) [Build and Path Variables](#variables) can not be used directly in the fields of Debug Configurations. However there are variables that can be used specifically within Debug Configurations, called Dynamic Variables. In CCS Debug Configurations, Dynamic variables can be used in the *Target Configuration*, *Initialization Script* (since CCSv9.2), and *Program* fields.
Some common Dynamic variables include (where myProjectName is the name of the project that you wish to reference):
- `${build_artifact:myProjectName}` - resolves to the output file built by the project, in the build directory of the project's active build configuration.
- Automatically used in the *Program* field, in the Debug Configuration generated by launching a project-based debug session.
- `${target_config_active_default:myProjectName}` - resolves to the active target configuration file of the project's active build configuration.
- Automatically used in the *Target Configuration* field, in the Debug Configuration generated by launching a project-based debug session.
- `${workspace_loc:/myProjectName/directoryName/fileName.ext}` - resolves to an arbitrary file or directory of an open project; this works even if the project's folder is outside of your workspace.
- In CCSv9.2 and higher, this is automatically used whenever you specify a file using the **Workspace...** button, in the Debug Configurations dialog.
#### Using Build/Path Variables in Debug Configurations
While Build and Path variables like ${PROJECT_BUILD_DIR} can not be used *directly* in the fields of Debug Configurations, there is a Dynamic variable (build_var) that can be used as a *wrapper* to evaluate any Build or Path variable in the context of a given project and [build configuration](./users_guide/ccs_project-management.html#build-configurations). Usage is as follows:
- `${build_var:/myProjectName/buildConfigurationName/BUILD_VARIABLE}` - evaluates BUILD_VARIABLE in the context of myProjectName's buildConfigurationName build configuration.
- `${build_var:/myProjectName/BUILD_VARIABLE}` - evaluates BUILD_VARIABLE in the context of myProjectName's active build configuration.
- `${build_var:BUILD_VARIABLE}` - evaluates BUILD_VARIABLE in the context of the currently selected resource's project's active build configuration.
- **NOTE:** this usage is **not recommended**, because the currently selected resource comes from the Project Explorer or the active editor, and the behaviour may be difficult to predict.
[[d Example
Assume there is an open workspace project called "myProjectName", and in that project's active build directory there is an executable file called "file1.out". To load that file to the target when launching a debug session on the project, you may set the project's Debug Configuration's *Program* field to:
```
${build_var:/myProjectName/PROJECT_BUILD_DIR}/file1.out
```
- The build_var Dynamic variable will evaluate the PROJECT_BUILD_DIR Build variable for myProjectName's active build configuration; this resolves to myProjectName's active build directory.
- Then, "/file1.out" is appended to that directory, and you have the full path to the desired file.
]]