README
portable
Example Summary
This example is a multi-threaded application that uses multiple drivers. It demonstrates how SimpleLink SDK examples can be portable across devices, kernels, and compilers. This is accomplished by using TI Drivers and POSIX APIs. This example is described in more detail in the SDK User’s Guide at <SDK_INSTALL_DIR>/docs/simplelink_mcu_sdk/Users_Guide.html.
Peripherals Exercised
Board_GPIO_LED0
- Indicates that temperature has exceeded the alert thresholdBoard_GPIO_BUTTON1
- Used to restart the UART consoleBoard_UART0
- Used for a simple consoleBoard_I2C_TMP
- Used to read temperature- For boards with an on-board TMP sensor (e.g. CC3220 Launchpads), that sensor is used.
- For boards without an on-board TMP sensor, the Sensors Boosterpack (http://www.ti.com/tool/boostxl-sensors) is needed. It has the TMP007 sensor along with several other nifty sensors.
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
- Open a serial session (e.g.
PuTTY
, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*
in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
The target displays a simple console on the serial session.
Valid Commands -------------- h: help q: quit and shutdown UART c: clear the screen t: display current temperature
If you are using TMP006, the DIE temperature is displayed. You’ll need to change the temperature of the actual TMP006 sensor to see a change. If you have a TMP007, the OBJECT temperature is displayed. To change this value, simply have the sensor pointed at something with a different temperature (e.g. the palm of your hand). Please note to keep the example short and sweet, the TMP sensor was not calibrated.
If you quit the console, the device will go into a lower power mode. To start the console back up, hit
Board_GPIO_BUTTON1
.
Application Design Details
This example shows how to initialize the UART driver in blocking read and write mode.
A thread,
consoleThread
, is a simple console. When the UART is closed the device can go into a lower power mode.A thread,
temperatureThread
, reads the temperature via I2C. The thread reads the sensor every second. The timing is controlled by a POSIX timer and semaphore. This approach was used to eliminate time drift (which would have occurred with simply using sleep(1)).The temperatureMutex mutex is used to protect the reading/writing of the temperature variables. The reading/writing of these two variables must be done atomically. For example without the mutex, the temperature thread (which is higher priority) could interrupt the reading of the variables by the console thread. This could result with the console thread printing a Celsius value that did not match up with the Fahrenheit value.
TI-RTOS:
- When building in Code Composer Studio, the kernel configuration project will be imported along with the example. The kernel configuration project is referenced by the example, so it will be built first. The “release” kernel configuration is the default project used. It has many debug features disabled. These feature include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” kernel configurations and how to switch between them, please refer to the SimpleLink MCU SDK User’s Guide. The “release” and “debug” kernel configuration projects can be found under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).
FreeRTOS:
- Please view the
FreeRTOSConfig.h
header file for example configuration information.
Code Composer Studio:
- When using in CCS for the CC3220 devices, it’s recommended you do a “Free Run” instead of “Run”. This is because when the CC3220 device goes into low power mode, emulation is lost.
SimpleLink Sensor and Actuator Plugin:
- This example uses a TMP007 (or TMP006) sensor. It interfaces via the I2C Driver. For a richer API set for the TMP sensors, please refer the SimpleLink Sensor and Actuator Plugin. This plugin also offers a Button module to handle debounce also.