|
Id |
Component |
Headline |
Additional Details |
Workaround (if applicable) |
Planned Resolution |
|
SDSCM00040469 |
DVT |
Use profile data to compute CPU loading |
|
|
|
|
SDSCM00040470 |
DVT |
Call graph with link back to raw data view |
|
|
|
|
SDSCM00040471 |
DVT |
Show profile data in call graph |
|
|
|
|
SDSCM00040472 |
DVT |
Would like to pick out a range of data to display |
|
|
|
|
SDSCM00041366 |
DVT |
Code Coverage coloring does not work for files that do not have
a CCS Project |
Line coloring works if coverage is done for an executable from a
CCS Project. Does not work E.g. if a .out file is directly loa... |
|
|
|
SDSCM00041756 |
DVT |
Add ability in image analyzer to flip the image on either axis:
up/down or left/right |
Request to add the ability in image analyzer to flip the image
on either axis: up/down or left/right |
|
|
|
SDSCM00045827 |
DVT |
Using JTAGRunMode with stairstep example on LM4F232 results in
"trouble reading memory block" error |
RTA does not work reliably when using JTAGRunMode on LM4F232 and
results in "trouble reading memory block" errors. |
|
CCS 6.2.0 |
|
SDSCM00046280 |
DVT |
Image Analyzer does not process 8bit data read in big endian for
RGB correctly |
Ther is a problem with viewing RGB data with 8bit Data Read. See
forum post for details.
http://e2e.ti.com/support/development_... |
Customer was able to workaround this using 32bit Data Read. See
Forum Post for details: http://e2e.ti.com/support/development_t... |
CCS 6.2.0 |
|
SDSCM00050047 |
DVT |
System Analyzer/UIA data transfer via JTAG should have a
progress bar |
When using UIA in JTAG stop mode, this stage is preceded by the
time when the JTAG reads data from the target. If the logger buf... |
N/A. |
|
|
SDSCM00050087 |
DVT |
Ability to show user events in Execution Graph |
|
|
CCS 6.2.0 |
|
SDSCM00050408 |
DVT |
Request for a way to clear the printf log data without having to
close the view |
Request for a way to clear the printf log data without having to
close the view |
|
|
|
SDSCM00050409 |
DVT |
Request for a way to be able to adjust and save column settings
in system analyzer data views |
Request for a way to be able to customize and save column
settings in system analyzer data views so they are preserved for
futur... |
|
|
|
SDSCM00050410 |
DVT |
Request to add commas to timestamps in RTOS Analyzer views to
make it easier to analyze the numbers |
Request to add commas to timestamps in RTOS Analyzer views to
make it easier to analyze the numbers |
|
|
|
SDSCM00050680 |
DVT |
Bookmarks in any DVT view (Trace/RTOS/System Analyzer) does not
work with filtering and sorting. |
Bookmarks in DVT views (RTOS/System/Trace Analyzer) are
associated with the index into the buffer. When the buffer is
filtered/s... |
None. |
|
|
SDSCM00051495 |
DVT |
Graph Q_Value parameter should allow values larger than 30 |
When trying to set a Q_Value larger than 30, the graph tool
refuses to accept this entry and limits the range from 0 to
30. Th... |
N/A. |
CCS 6.2.0 |
|
SDSCM00042934 |
Emulation |
Improve the error message when attempting to connect to the
ethernet interface of XDS560v2 STM from multiple hosts |
Whenever two users attempt to connect to the ethernet interface
of a single XDS560v2 STM emulator, the error message thrown
show... |
N/A. |
|
|
SDSCM00043910 |
Emulation |
MSP430 REGISTER view descriptions for SR.SCG0 and SR.SCG1
incorrect in CCSv5.1 |
|
|
|
|
SDSCM00047337 |
Emulation |
Request to separate out FPU registers into their own group |
Request to separate out FPU registers for Stellaris into their
own group so they are visible in the CCS registers view under
the... |
|
|
|
SDSCM00047580 |
Emulation |
Linking MSP FETS and sessions |
|
|
|
|
SDSCM00049637 |
Emulation |
Remove/improve error messages displayed in CCS console when
accessing uninitialized peripherals |
Request to remove/improve error messages displayed in CCS
console when accessing uninitialized peripherals. |
|
|
|
SDSCM00050949 |
Emulation |
Debug view does not display correct target state on disconnect |
On C2000 devices with a majority of emulators (excluding
XDS100), the default behavior is to resume execution of a halted
target... |
|
|
|
SDSCM00051311 |
Emulation |
Blackhawk XDS200 debuggers do not install firmware update
utilities |
When installing XDS200 debugger support, one of the critical
update directories for updating the firmware is located under a
Spe... |
Install the Spectrum Digital support |
CCS 6.1.1 |
|
SDSCM00051476 |
Emulation |
Add ability to view D0 - D31 and S0 - S31 floating point
registers on Cortex A15 |
Add the ability to view Neon floating point registers in the
registers view. |
|
|
|
SDSCM00034673 |
IDE |
CCS v4 allows usage of 1 hardware breakpoint less than CCS 3.3
for BIOS programs |
CCS v4.0x allows user to set only 1 hardware breakpoint when
debugging BIOS programs in Flash |
|
|
|
SDSCM00038571 |
IDE |
Need excluded files filter for the Project Explorer |
In the Project Explorer, which will be the default project view
in CCSv5 instead of the C/C++ Projects View, there is a list of
... |
|
|
|
SDSCM00038857 |
IDE |
EASY: Simplified Build Options Dialog |
Today the build options dialog is quite cluttered and it can be
overwhelming to use. Creating the Basic options helped a bit bu... |
|
|
|
SDSCM00039559 |
IDE |
Would like ability to adjust file specific options on multiple
selected files. |
Would like ability to be able to apply file specific options on
multiple files. |
|
|
|
SDSCM00040028 |
IDE |
Import wizard should prompt user to change compiler version if
needed |
If I am importing a project that uses a different version of the
compiler than what I have installed the wizard should inform
me... |
|
|
|
SDSCM00040045 |
IDE |
NullPointerException when renaming project |
Sometimes when renaming an imported project you will get a
dialog complaining of a null pointer exception. |
|
|
|
SDSCM00040259 |
IDE |
Merge the two CCS project import wizards |
Today we have separate wizards for importing eclipse based CCS
projects and legacy CCSv3.x projects. We could have them be a
si... |
|
|
|
SDSCM00040262 |
IDE |
MMU Page table view should be listed on the view menu |
The MMU Page Table View should be listed on the view menu. |
|
|
|
SDSCM00040708 |
IDE |
For header files outside the project folder double clicking on
compile errors in the Problems view does not jump to error |
When a compilation error occurs in a header file that is outside
the project (e.g. system header file or even user header file
l... |
|
|
|
SDSCM00041325 |
IDE |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension |
Library projects for non-default build configurations must have
'lib' for the Artifact Extension. The default 'Debug' and
'Relea... |
|
|
|
SDSCM00045764 |
IDE |
Renaming linked files causes invalid duplicate links in another
workspace that is sharing the same file |
When the file is renamed in CCS (hence updating the .project
file), the rename is not getting handled properly by other
workspac... |
Remove the project from the workspaces that exhibit the issue
and re-import it. This will correctly update the Project
Explorer ... |
|
|
SDSCM00046736 |
IDE |
Eclipse won't start when there are unusual characters in the
platform path |
Eclipse and hence CCS will not start if a folder contains #!$
characters in the path. As a workaround CCS installer is
detecting... |
Don't use a User or Install path that includes characters like #
or $. |
|
|
SDSCM00047055 |
IDE |
Support for debugging RealView Compiler output including
Semi-hosting |
Would like to be able to use CIO functions like printf when
debugging code generated by the RealView compiler in CCS. |
|
CCS 7.0.0 |
|
SDSCM00047285 |
IDE |
Support Linux OS Aware Debug |
This feature existed with CCSv4 but was not ported to CCSv5 for
a variety of reasons (compatibility issues with stock Eclipse,
l... |
|
|
|
SDSCM00047442 |
IDE |
New project wizard should only create one default build
configuration |
When a new project is created in CCS, two build configurations
are created by default - 'Debug' and 'Release'. This has been
the... |
|
|
|
SDSCM00047490 |
IDE |
Rebuild of index for updating macro expansions does not permeate
through multiple levels of include files |
Rebuild of index for updating macro expansions does not permeate
through multiple levels of include files |
|
|
|
SDSCM00047723 |
IDE |
In the Target Configuration Editor, changing the "Device" or the
"Connection" should not reset to all defaults |
Whenever creating a Target Configuration using the Editor, any
changes to either the Connection or the Device reset all
settings... |
N/A. |
CCS 6.2.0 |
|
SDSCM00048600 |
IDE |
CCS needs to interpret .debug_macinfo ( was: Symbol not found
when adding expression ) |
In some cases, adding a symbol found in the source window to the
watch window results in an error: identifier not found. This
ha... |
Inspect the generated map file for the program. Look for the
symbol name and note its fully qualified name. Use the long name
in... |
CCS 6.2.0 |
|
SDSCM00049478 |
IDE |
CCSv6 should be integrated in Ubuntu's Dash menu |
Historically CCS and Blackhawk/Spectrum Digital always created
desktop icons in Ubuntu. This is fine for Ubuntu releases 10.10
... |
N/A. |
CCS 6.2.0 |
|
SDSCM00049589 |
IDE |
variables decalred in annoymous namspace cannot be accessed
(GCC compiler ) |
|
|
CCS 6.2.0 |
|
SDSCM00049607 |
IDE |
[CDT] Enhance Codan plug-in with the ability to create custom
rules |
Enhance Codan plug-in with the ability to define and create
custom rules. Codan is an Eclipse plug-in and any
modifications wo... |
Use other 3rd party Code Analysis plug-ins that support this
feature |
CCS 6.2.0 |
|
SDSCM00049786 |
IDE |
GC: support bi-directional char array binding |
|
|
CCS 6.2.0 |
|
SDSCM00049856 |
IDE |
CCSv6 experiences high CPU usage when chromium based tool is
opened |
If GUI Composer feature is installed in Linux, then CCS will
experience high CPU usage for the rest of CCS session. There is
no ... |
|
CCS 6.2.0 |
|
SDSCM00049901 |
IDE |
Blank line shown above editor area when editors are open side by
side |
When viewing source files side by side you get a blank line
above the editor area. |
|
|
|
SDSCM00049917 |
IDE |
Error when using editor feature 'Open Declaration' to jump to
declaration of an array |
Error when using editor feature 'Open Declaration' to jump to
declaration of an array. An internal error occurred during: "Ope... |
|
|
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
CCS 6.2.0 |
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
CCS 6.2.0 |
|
SDSCM00049946 |
IDE |
EVE CCS/Load Program/Browse Project not working |
|
|
CCS 6.2.0 |
|
SDSCM00050201 |
IDE |
Removing file should remove all associated settings |
|
|
CCS 6.2.0 |
|
SDSCM00050229 |
IDE |
The ability to set file specific linker options should not be
exposed |
If you have a .lib in your project you can right click on it and
CCS will let you set file specific options for the linker.
How... |
|
CCS 6.2.0 |
|
SDSCM00050293 |
IDE |
Spell-checker in the editor does not work |
Spell-checker in the editor does not work despite the feature
being enabled. |
|
CCS 6.2.0 |
|
SDSCM00050372 |
IDE |
CCS needs to interpret .debug_macinfo (GCC support) |
In some cases, adding a symbol found in the source window to the
watch window results in an error: identifier not found. This
ha... |
Inspect the generated map file for the program. Look for the
symbol name and note its fully qualified name. Use the long name
in... |
CCS 6.2.0 |
|
SDSCM00050489 |
IDE |
Once launch configuration has been created, can't switch from
load symbols back to load program |
|
Simplest way of making the change without deleting launch
configuration is to use "Debug Configurations..." dialog (Run->
Debug... |
CCS 6.2.0 |
|
SDSCM00050510 |
IDE |
Hide the 'RemoteSystemsTempFile' project as an option when
browsing projects in the workspace |
The RSE plugin comes with CCSv6 by default. Because of that, a
folder called 'RemoteSystemsTempFile' appears in the workspace
w... |
|
CCS 6.2.0 |
|
SDSCM00050521 |
IDE |
Autoformat (ctrl + shift + F) can alter formatting of source
files which can cause compiler errors. |
Autoformat (ctrl + shift + F) can alter formatting of source
files which can cause compiler errors. Related to combination
of #... |
|
|
|
SDSCM00050556 |
IDE |
Memory Usage View should support GCC |
The Memory Usage View is currently only supported for TI build
tools. It is important to support GCC due the growing popularity
... |
|
CCS 6.2.0 |
|
SDSCM00050620 |
IDE |
Request command line utility to dump out the type information
for every symbol |
|
|
|
|
SDSCM00050650 |
IDE |
CCS for Linux shows GTK and DVT errors errors when launched from
the command line (DVT Text) |
Calling CCSv6 from a Linux terminal shows several error messages
related to GTK at startup, the already common "client has not
b... |
|
CCS 6.2.0 |
|
SDSCM00050833 |
IDE |
Callstack line numbers are off by 1 when using imported Energia
project |
When I look at the call stack (and PC in the editor) the source
line number is off by +1. If the call is on line 239 it
instead... |
|
CCS 6.2.0 |
|
SDSCM00050940 |
IDE |
Trying to set the optimization level via C/C++ Build settings
results in an error message |
Create a project Right click on it and select properties Click
at the bottom to show advanced options Under C/C++ Build select
s... |
Compiler options should be set via CCS Build -> Compiler |
CCS 6.2.0 |
|
SDSCM00050964 |
IDE |
Hex Utility (and GNU Objcopy in the case of GNU tools) should
run before post build steps in CCS |
Request for the Hex Utility (and GNU Objcopy in the case of GNU
tools) to run before post build steps in CCS during project buil... |
|
CCS 6.1.1 |
|
SDSCM00051026 |
IDE |
CCS hex utility build dialog has no method for supplying a
command file |
|
|
CCS 6.2.0 |
|
SDSCM00051052 |
IDE |
When using SW breakpoints in source file, the LDR instruction
does not work correctly on a Cortex-A8 (AM335x) |
|
|
CCS 6.1.1 |
|
SDSCM00051072 |
IDE |
Launching a debug session when a previous one is still active
leaves its header lingering in the Debug view |
When launching one debug session with another one still running,
CCS politely asks to terminate it before completing the new lau... |
N/A. |
CCS 6.2.0 |
|
SDSCM00051082 |
IDE |
Remember that clock was visible from previous debug session and
show it again |
The issue is that if you enable and show the clock in a debug
session it does not remember that the next time you launch so
you ... |
Manually open the clock after each debug launch. |
CCS 6.2.0 |
|
SDSCM00051224 |
IDE |
C Code Formatter Results in Build Errors |
This has only been seen with one project but using the code
formatter did introduce a build error with it. |
Use the local history tool in CCS to revert to the previous
version of the file. |
|
|
SDSCM00051272 |
IDE |
The CCS Online Help content for "Data File Formats" is outdated |
The CCS Online Help content for "Data File Formats" is outdated
since the fomat changed for CCSv6. |
|
CCS 6.1.1 |
|
SDSCM00051434 |
IDE |
Multiple copies of the same header file are opened when clicking
on a error/warning in the Problems view |
For errors/warning listed in the Problems view, clicking on one
for an entry found in a header file not part of the project
will... |
|
CCS 6.1.1 |
|
SDSCM00048795 |
Trace |
Trace: "End at address" of the "Trace Range" parameter fails to
stop and display trace data |
Setting an end address to the "Trace Range" parameter fails to
stop the Trace data collection at the specified address and
cause... |
Use "Range" or "Start and stop at address" instead. |
|
|
SDSCM00048813 |
Trace |
When simultaneously running two separate CCS debug session, one
instance may hang and crash |
When simultaneously running two separate CCS debug session, one
instance may hang and crash when trying to run both targets. Th... |
Use a single target configuration that defines both emulators. |
|
|
SDSCM00050024 |
Trace |
Cache analysis trace job collapses CCS |
When trying to gather the data for cache analysis trace job, CCS
collapses without a trace. This is probably related to the
am... |
N/A |
|
|
SDSCM00050619 |
Trace |
Trace viewer should not reset its display arrangement when a
column is added/restored |
If the trace display is changed by order, size, etc., whenever a
column is added/removed the display is restored to defaults.
T... |
N/A. |
|
|
SDSCM00050622 |
Trace |
Trace display should allow cumulative storing of data between
start/stop jobs |
Whenever a trace job is started, the trace display (and its
data) is cleared from the view before the new incoming data is
captu... |
Save to .csv/.tdf every step on the way. |
|