Release Notes for Code Composer Studio™ v12.5.0
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™.The release notes are divided into six sections:
Contents
CCSv12.5.0 uses an unmodified
Eclipse and CDT version 22.03LTS.
They are packaged together under “Eclipse IDE for C/C++ Developers” package
available from www.eclipse.org.
Additional plug-ins or 3rd party tools may be installed that are compatible
with Indigo release.
For additional information and support, please go to: http://dev.ti.com/tirex/#/?link=Development%20Tools%2FIntegrated%20Development%20Environments%2FCode%20Composer%20Studio%2FUser's%20Guide
|
Memory |
Disk space |
Processor |
|
|
Minimum |
4GB |
2.5GB |
2.0GHz single core |
|
Recommended |
8GB |
5.0GB |
2.0GHz dual core |
Please note that Code Composer Studio is a 64bit application and thus will not run on 32bit operating systems.
XDS510 class debug probes are no longer supported
Supported distributions include:
Code Composer Studio will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Code Composer Studio device support on macOS is limited to microcontrollers (MSP, C2000, SimpleLink, Tiva and Hercules) and does not include processors (Sitara, DSP, KeyStone).
Versions Supported
Each Code Composer Studio release is validated against a set of macOS releases. This release was validated with:
Debug Probe Support
Debug Probes Not Supported
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCS_12.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio:1. Run ccs_setup_12.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The online web installer and the offline installer are now distributed as disk images (.dmg files)
1. Right-click on CCS_12.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio:1. Run ccs_setup_12.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
Please visit https://software-dl.ti.com/ccs/esd/documents/users_guide_12.1.0/index.html
before installing CCS on Linux. It contains important information on
installing CCS on different Linux distributions, including CCS dependencies that may need to be installed first.
Before installing CCS, the tarball file in which the CCS Installer is distributed must first be extracted:untar CCS_12.x.x.xxxxx_linux-x64.tar.gz or CCS_12.x.x.xxxxx_web_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCS_12.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS as root. However, it is preferred that you first install CCS as a normal user and then install the drivers as root.
To install Code Composer Studio as a normal user and emulation drivers as root:1. Run ccs_setup_12.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio as root:
1. Run ccs_setup_12.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
General Enhancements
· Compilers
o TI ARM Clang compiler 3.2.0 LTS bundled
o C28 Compiler tools 22.6.1 LTS bundled
· IDE
o General bug fixes and enhancements
· Debugger
o General bug fixes and enhancements
· Device Support
o MSPM0 – updated device support and bug fix
o Sitara MCU – AM263Px device support
o C2000 – TMS320F28P65x device support added for Linux and MacOS
§ users should review the TMS320F28P65x Flash plugin usage notes provided at https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/951697/faq-flash-frequently-asked-questions
· SysConfig
o v1.18.0 bundled
Bug Fixes
· For up-to-date status information, go to this Link
General Enhancements
· IDE
o General bug fixes and enhancements
· Debugger
o General bug fixes and enhancements
· Device Support
o C2000 – TMS320F28P65x device support (Windows only)
§ users should review the TMS320F28P65x Flash plugin usage notes provided at https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/951697/faq-flash-frequently-asked-questions
o CC26xx – updated device support and bug fix
o mmWave – added support for AWRL6432 and IWRL1432
o MSPM0 – updated device support and bug fix
· Debug Probe
o Segger J-Link – updated support (v7.88.0c)
Bug Fixes
· For up-to-date status information, go to this Link
General Enhancements
· Compilers
o TI CLANG 2.1.3 LTS compiler bundled
· IDE
o General bug fixes and enhancements
· Debugger
o General bug fixes and enhancements
· Device Support
o CC1xxx/2xxx – CC1314/CC1354, CC234x device support updates
o Sitara AM62A device support updates.
o Automotive device support: J721S2_TDA4VL (J7_AEP) , J721S2_TDA4VH (J7_AHP) device support updates
Bug Fixes
· For up-to-date status information, go to this Link
General Enhancements
· Compilers
o TI CLANG 2.1.2 LTS compiler bundled
o ARM MCU v20.2.7 LTS compiler update
· IDE
o General bug fixes and enhancements
· Debugger
o General bug fixes and enhancements
· Device Support
o CC1xxx/2xxx – CC1314/CC1354, CC234x device support updates
o AM263x device support updates: AM2631/2/4 devices added.
§ Created device xmls for each version of the device with different number of cores
§ Added PG detection script to diagnostics folder
§ Addressing bug Created OnPreFileLoaded() function that issues GEL_Reset()
o AM243x device support updates
§ Multiple device XML GPNs now supported for AM243x
§ Modules now supported for AM243x
§ Directory structure for the package fixed
o Automotive device support: J721S2_TDA4VL (J7_AEP) , J721S2_TDA4VH (J7_AHP) device support added
o Sitara AM62x: adding peripheral xmls. optimized PLL config gels, added more info to DDR Regdump GELs, updated DDR configs, fixed bug in DDR size function
Bug Fixes
· For up-to-date status information, go to this Link
General Enhancements
· Compilers
o TI CLANG 2.1.2 LTS compiler bundled
o ARM MCU v20.2.7 LTS compiler update
· IDE
o General bug fixes and enhancements
· Debugger
o General bug fixes and enhancements
· Device Support
o C2000 Device Support (linux64/osx/win64) v6.8.0.0
o CC26xx Device Support (linux64/osx/win64) v3.16.11.152
o Sitara Device Support (linux64/win64) v1.6.2
Bug Fixes
· For up-to-date status information, go to this: Link
General Enhancements
· Compilers
o TI CLANG 2.1.0 LTS compiler bundled
o ARM MCU v20.2.6 LTS compiler update
o C6000 v8.3.15 compiler update
o C2000 MCU LTS v22.6.0 compiler update
· IDE
o Eclipse and CDT 22.03LTS
o Various bug fixes and enhancements
· Debugger
o Improved CLANG debug experience
o Various bug fixes and enhancements
Bug Fixes
· For up-to-date status information, go to this Link
This dynamic query lists all issues that are currently open.
https://sir.ext.ti.com/jira/browse/EXT_EP-9781?filter=10387
name
version
ARM Clang Compiler Tools (linux64/osx/win64)
v3.2.0.LTS
ARM Compiler Help (linux64/osx/win64)
v18.1.0.20181119
ARM Compiler Tools (linux64/osx/win64)
v20.2.7.LTS
Automotive Processor Device Support (linux64/win64)
v1.1.13
BeagleBone FTDI Drivers (win64)
v2.8.30.20140130
Blackhawk Emulators (linux64/win64)
v9.0.0.002
C2000 Compiler Help (linux64/osx/win64)
v18.1.0.20180221
C2000 Device Support (linux64/osx/win64)
v6.17.0.0
C2000 Emulation Flash (linux64/osx/win64)
v1.0.0.5
C2800 Compiler Tools (linux64/osx/win64)
v22.6.1.LTS
C55xx Device Support (linux64/win64)
v1.2.1
C6000 Compiler Help (linux64/win64)
v7.4.0.20150713
C6000 Device Support (linux64/win64)
v1.1.7
C6000 v8 Compiler Tools (linux64/win64)
v8.3.12
CC2538 Device Support (linux64/osx/win64)
v2.0.4.11
CC26xx Device Support (linux64/osx/win64)
v3.17.10.24
CC3220 Device Support (linux64/osx/win64)
v1.0.5
CC323X Device Support (linux64/osx/win64)
v1.0.5
CC32xx Device Support (linux64/osx/win64)
v1.0.8
CC32xx Driver Support (linux64/osx/win64)
v1.0.8
CCS Certificate (win64)
vmaster
CCS Documentation (linux64/osx/win64)
vCCS_12.x.0_release_notes
CCS Installer (linux64/osx/win64)
v12.5.0.20230818103534
CCS Installer Dependencies (win64)
v1.0.0.20170130000000
CCS Installer Dependencies (linux64/osx)
v1.0.0.20180710000000
CCS Launcher (osx)
v12.0.0.20220615
CCS Launcher (linux64)
v12.4.0.20230414
CCS Launcher (win64)
v12.0.0.20220603
CCS P2 Templates (linux64/osx/win64)
v11.1.0.20211206
CCS User's Guide (linux64/osx/win64)
v12.5.0.202309221403
CCS Utilities (linux64/osx/win64)
v1.0.0.20230823
Code Composer Plugins (linux64/osx/win64)
v12.5.0.N202309161830
Compiler Tools On-line Documentation (linux64/osx/win64)
v1.1.6
DVT (linux64/osx/win64)
v4.1.0.202307061549
DaVinci Device Support (linux64/win64)
v1.1.6
Debug Server (linux64/osx/win64)
v12.5.0.3202
Debug Server Flash (linux64/osx/win64)
v12.5.0.3202
Eclipse (linux64/osx/win64)
v4.8.0.0
Eclipse P2 Extensions (linux64/osx/win64)
v7.0.0.202001271514
Hercules Emulation (linux64/osx/win64)
v6.0.9
IDE Chrome (linux64/osx/win64)
v12.5.0.N202309161830
IDE GUI Composer (linux64/osx/win64)
v12.5.0.N202309161830
IDE Tools Common (linux64/osx/win64)
v12.5.0.N202309161830
InstallBuilder (linux64/osx/win64)
v21.9.0
JRE (linux64/osx/win64)
v11.0.13.8
Keystone2 (linux64/win64)
v1.2.4
MSP430 Compiler Help (linux64/osx/win64)
v18.1.0.20181119
MSP430 Compiler Tools (linux64/osx/win64)
v21.6.1.LTS
MSP430 and MSP432 Support (linux64/osx/win64)
v11.1.0.20211104
MSPM0 Support (linux64/osx/win64)
v1.02.00.05
MSVC 2017 Redistributable (x64) (win64)
v14.34.31938
Mmwave Radar Device Support (linux64/win64)
v1.7.7
Node.js (linux64/osx/win64)
v18.16.0
OMAP Device Support (linux64/win64)
v1.1.0
OMAPL Device Support (linux64/win64)
v1.1.2
P2 App (linux64/osx/win64)
v12.5.0.N202309161830
PGA Device Support (linux64/osx/win64)
v1.0.2
SEGGER J-Link (linux64/osx/win64)
v7.88.0.c
SEGGER J-Link USB Driver (win64)
v1.0.1.0
Shared Device Support (linux64/win64)
v1.1.7
Sitara Device Support (linux64/win64)
v1.6.4
Sitara MCU Device Support (linux64/win64)
v1.2.5
Sys Config (linux64/osx/win64)
v1.18.0.3266
TI Cloud Agent (linux64/osx/win64)
v0.5.4507
TI Emulators (linux64/osx/win64)
v9.13.0.00201
TIREX Desktop (linux64/osx/win64)
v3.8.0.201911142334
TIREX4 Desktop (linux64/osx/win64)
v4.15.0.202309151451
Target Content (linux64/osx/win64)
v3.62.1.16
TargetDB Default Props (linux64/osx/win64)
v12.5.0.N202309161830
Tiva C Series ARM MCUs (linux64/osx/win64)
v2.1.1.15071
Tiva E Series ARM MCUs (linux64/win64)
v2.1.1.15071
Tiva/Stellaris ICDI Debug Probe (linux64/osx/win64)
v2.1.3.15
UCD Digital Power Controllers (linux64/win64)
v1.1.5
core (linux64/osx/win64)
v12.0.0.20220405
Windows XP, Windows Vista, Windows
7, Windows 8, Windows 8.1,Windows 10, Visual SourceSafe, Visual Basic, and
Visual C++ are all trademarks and/or registered trademarks of Microsoft
Corporation.
C2000, C5000, C54x, C55x, C6000, C6x, CC2538, CC26xx, CC32xx, OMAP, TMS320,
TMS570, MSP430, Stellaris, Tiva-C, Hercules, GUI Composer, Grace, Code Composer
Studio, Code Composer Studio App Center, TI-RTOS, SYS/BIOS, XDS560, XDS510,
XDS200, XDS100 and XDS110 are trademarks of Texas Instruments.
© Copyright 2022