Release Notes for Code Composer Studio™ v10.x.0
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™.The release notes are divided into six sections:
Contents
CCSv10.x.0 uses an
unmodified Eclipse and CDT version 19.12LTS.
They are packaged together under “Eclipse IDE for C/C++ Developers” package
available from www.eclipse.org. Additional plug-ins or 3rd party tools may be installed that are
compatible with Indigo release.
For additional information and support, please go to: http://dev.ti.com/tirex/#/?link=Development%20Tools%2FIntegrated%20Development%20Environments%2FCode%20Composer%20Studio%2FUser's%20Guide
|
Memory |
Disk space |
Processor |
|
|
Minimum |
4GB |
2.5GB |
2.0GHz single core |
|
Recommended |
8GB |
5.0GB |
2.0GHz dual core |
|
|
|
|
|
Please note that Code Composer Studio is a 64bit application and thus will not run on 32bit operating systems.
XDS510 class debug probes are no longer supported
Supported distributions include:
Code Composer Studio will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Code Composer Studio device support on macOS is limited to microcontrollers (MSP, C2000, SimpleLink, Tiva and Hercules) and does not include processors (Sitara, DSP, KeyStone).
Versions Supported
Each Code Composer Studio release is validated against a set of macOS releases. This release was validated with:
Debug Probe Support
Debug Probes Not Supported
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCS_10.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio:1. Run ccs_setup_10.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The online web installer and the offline installer are now distributed as disk images (.dmg files)
1. Right-click on CCS_10.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio:1. Run ccs_setup_10.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
before installing CCS on Linux. It contains important information on
installing CCS on different Linux distributions, including CCS dependencies that may need to be installed first.
Before installing CCS, the tarball file in which the CCS Installer is distributed must first be extracted:untar CCS_10.x.x.xxxxx_linux-x64.tar.gz or CCS_10.x.x.xxxxx_web_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCS_10.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS as root. However, it is preferred that you first install CCS as a normal user and then install the drivers as root.
To install Code Composer Studio as a normal user and emulation drivers as root:1. Run ccs_setup_10.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio as root:
1. Run ccs_setup_10.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
· General Enhancements
· Compilers
o TI CLANG 1.3.0 LTS compiler bundled
o MCU v20.2.5 LTS compiler update
o C6000 v8.3.10 compiler update
· New device support
o AM243X device pin-trace
o CC13x1 support
· Installer
o Fixes for visual artefacts in Installer dialogs on M1-based mac machines.
Bug Fixes
· For up-to-date status information, go to:
· General Enhancements
· New device support
o AM243X devices
Bug Fixes
· For up-to-date status information, go to:
· General Enhancements
· Bugfixes for IDE, sysconfig and MSP install
· Security issue resolved: Getting Started View updated to protect against a potential man-in-the-middle attack vulnerability.
· New device support
o AM64x, J7ES PG 1.1
o CC1312R7, CC1352P7, CC2652R7, CC2652P7, CC1311R3, CC1311P3, CC2651R3, CC2651P3
o CC2672x
Bug Fixes
· For up-to-date status information, go to:
· General Enhancements
· Mac OS installers are now distributed as signed and notarized disk image (DMG) files.
· Bugfixes for IDE, sysconfig and MSP install
· Security issue resolved: Getting Started View updated to protect against a potential man-in-the-middle attack vulnerability.
· New device support
o J7VCL
o TPR12
o CC1312R7, CC1352P7, CC2652R7, CC2652P7
o CC1311R3, CC1311P3, CC2651R3, CC2651P3
Bug Fixes
· For up-to-date status information, go to:
· General Enhancements
· Mac OS installers are now distributed as signed and notarized disk image (DMG) files.
· Bugfixes for IDE, sysconfig and MSP install
· Security issue resolved: Getting Started View updated to protect against a potential man-in-the-middle attack vulnerability.
Bug Fixes
· For up-to-date status information, go to:
Known Issues
· For up-to-date CCS status information, go to:
o https://sir.ext.ti.com/jira/browse/EXT_EP-10173?jql=(Product%20~%20%22Code%20Composer%20Studio%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20Debugger%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20IDE%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20Graphs%22%20OR%20product%20~%20%22Resource%20Explorer%22%20OR%20product%20~%20%22Pin%20Mux%20Tool%22%20OR%20product%20~%20SysConfig)%20AND%20resolution%20%3D%20Unresolved%20AND%20type%20%3D%20Bug%20OR%20(%22Found%20In%20Release%22%20~%20CCS_7.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.1.1%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.2.0)%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.4.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.3.1%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.0.1%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.1.1%20%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.2.0%20%20ORDER%20BY%20updated%20DESC
o
· For up-to-date TI Debug Probe status information, go to:
· General Enhancements
· Mac OS installers are now distributed as signed and notarized disk image (DMG) files.
· Bugfixes for IDE, DVT, Debugger
· MCU Compilers LTS 20.02.1
· C6000 Compiler 8.3.6
· MSP430 GCC v9.2.0.50
· XDCTools v3.61
Bug Fixes
· For up-to-date status information, go to:
Known Issues
· For up-to-date CCS status information, go to:
o https://sir.ext.ti.com/jira/browse/EXT_EP-10173?jql=(Product%20~%20%22Code%20Composer%20Studio%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20Debugger%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20IDE%22%20OR%20Product%20~%20%22Code%20Composer%20Studio%20Graphs%22%20OR%20product%20~%20%22Resource%20Explorer%22%20OR%20product%20~%20%22Pin%20Mux%20Tool%22%20OR%20product%20~%20SysConfig)%20AND%20resolution%20%3D%20Unresolved%20AND%20type%20%3D%20Bug%20OR%20(%22Found%20In%20Release%22%20~%20CCS_7.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_7.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_8.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.2.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_9.3.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.0.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.1.0%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.1.1%20OR%20%22Found%20In%20Release%22%20~%20CCS_10.2.0)%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_7.4.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_8.3.1%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.0.1%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.2.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_9.3.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.0.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.1.0%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.1.1%20%20AND%20%22Fix%20In%20Release%22%20!~%20CCS_10.2.0%20%20ORDER%20BY%20updated%20DESC
· For up-to-date TI Debug Probe status information, go to:
General Enhancements
· Mac OS installers are now distributed as signed and notarized disk image (DMG) files.
· Bugfixes for IDE, DVT, Debugger
· MCU Compilers LTS 20.02.0
· C6000 Compiler 8.3.6
· MSP430 GCC v8.3.1.25
· XDCTools v3.61
Bug Fixes
· For up-to-date status information, go to:
o https://sir.ext.ti.com/jira/issues/?jql=(resolution%20%3D%20Fixed%20OR%20resolution%20%3D%20Implemented%20)%20AND%20%20((%22Fix%20In%20Release%22%20~%20CCS_10.0.0%20)%20OR%20%20(%22Fix%20In%20Release%22%20~%20EMU20_M02))%20ORDER%20BY%20updated
Known Issues
· For up-to-date CCS status information, go to:
· For up-to-date TI Debug Probe status information, go to:
This dynamic query lists all issues that are currently open.
https://sir.ext.ti.com/jira/browse/EXT_EP-9781?filter=10387
name
version
ARM Clang Compiler Tools (linux64/osx/win64)
v1.3.0.LTS
ARM Compiler Help (linux64/osx/win64)
v18.1.0.20181119
ARM Compiler Tools (linux64/osx/win64)
v20.2.5.LTS
Automotive Processor Device Support (linux64/win64)
v1.1.9
BeagleBone FTDI Drivers (win64)
v2.8.30.20140130
Blackhawk Emulators (linux64/win64)
v9.0.0.002
C2000 Compiler Help (linux64/osx/win64)
v18.1.0.20180221
C2000 Device Support (linux64/osx/win64)
v6.2.0.0
C2000 Emulation Flash (linux64/osx/win64)
v1.0.0.5
C2800 Compiler Tools (linux64/osx/win64)
v20.2.5.LTS
C55xx Device Support (linux64/win64)
v1.2.1
C6000 Compiler Help (linux64/win64)
v7.4.0.20150713
C6000 Device Support (linux64/win64)
v1.1.7
C6000 v8 Compiler Tools (linux64/win64)
v8.3.10
CC2538 Device Support (linux64/osx/win64)
v2.0.4.11
CC26xx Device Support (linux64/osx/win64)
v3.15.03.123
CC3220 Device Support (linux64/osx/win64)
v1.0.5
CC323X Device Support (linux64/osx/win64)
v1.0.5
CC32xx Device Support (linux64/osx/win64)
v1.0.8
CC32xx Driver Support (linux64/osx/win64)
v1.0.8
CCS Certificate (win64)
vmaster
CCS Documentation (linux64/osx/win64)
vrelease/CCS_10.4.0-release-notes
CCS Installer (linux64/osx/win64)
v10.4.0.20210611090741
CCS Installer Dependencies (win64)
v1.0.0.20170130000000
CCS Installer Dependencies (linux64/osx)
v1.0.0.20180710000000
CCS Launcher (osx)
v10.1.0.20200320
CCS Launcher (linux64)
v10.0.0.20200219
CCS Launcher (win64)
v10.0.0.20200131
CCS P2 Templates (linux64/osx/win64)
v10.3.0.20210316
CCS User's Guide (linux64/osx/win64)
v10.4.0.202106241026
CCS Utilities (win64)
v9.1.0.20190321
CCS Utilities (linux64/osx)
v1.0.0.20190716
Code Composer Plugins (linux64/osx/win64)
v10.4.0.N202105291800
Compiler Tools On-line Documentation (linux64/osx/win64)
v1.1.6
DVT (linux64/osx/win64)
v4.1.0.202105121547
DaVinci Device Support (linux64/win64)
v1.1.6
Debug Server (linux64/osx/win64)
v10.4.0.2437
Debug Server Flash (linux64/osx/win64)
v10.4.0.2437
Eclipse (linux64/osx/win64)
v4.8.0.0
Eclipse P2 Extensions (linux64/osx/win64)
v7.0.0.202001271514
GCC ARM Compiler Tools (linux64/osx/win64)
v7.2.1.2017-q4-major
GCC MSP430 Compiler Tools (linux64/osx/win64)
v9.3.1.11
Hercules Emulation (linux64/osx/win64)
v6.0.8
IDE Chrome (linux64/osx/win64)
v10.4.0.N202105291800
IDE GUI Composer (linux64/osx/win64)
v10.4.0.N202105291800
IDE Tools Common (linux64/osx/win64)
v10.4.0.N202105291800
InstallBuilder (linux64/osx/win64)
v21.3.0
JRE (win64)
v1.8.0.144
JRE (linux64/osx)
v1.8.0.122
JRE32 (win64)
v1.8.0.112
Keystone2 (linux64/win64)
v1.2.4
MSP430 Compiler Help (linux64/osx/win64)
v18.1.0.20181119
MSP430 Compiler Tools (linux64/osx/win64)
v20.2.5.LTS
MSP430 and MSP432 Support (linux64/osx/win64)
v10.3.0.20210408
MSVC 2017 Redistributable (x64) (win64)
v14.28.29913
MSVC 2017 Redistributable (x86) (win64)
v14.11.25325
Mmwave Radar Device Support (linux64/win64)
v1.6.9
Node.js (linux64/osx/win64)
v8.11.4
OMAP Device Support (linux64/win64)
v1.1.0
OMAPL Device Support (linux64/win64)
v1.1.2
P2 App (linux64/osx/win64)
v10.4.0.N202105291800
PGA Device Support (linux64/osx/win64)
v1.0.2
SEGGER J-Link (linux64/osx/win64)
v6.44.0.b
SEGGER J-Link USB Driver (win64)
v1.0.1.0
Shared Device Support (linux64/win64)
v1.1.7
Sitara Device Support (linux64/win64)
v1.5.4
Sitara MCU Device Support (linux64/win64)
v1.0.1
Sys Config (linux64/osx/win64)
v1.9.0.2015
TI Cloud Agent (linux64/osx/win64)
v0.5.3125
TI Emulators (linux64/osx/win64)
v9.4.0.00129
TIREX Desktop (linux64/osx/win64)
v3.8.0.201911142334
TIREX4 Desktop (linux64/osx/win64)
v4.8.0.202106161344
Target Content (linux64/osx/win64)
v3.62.1.15
TargetDB Default Props (linux64/osx/win64)
v10.4.0.N202105291800
Tiva C Series ARM MCUs (linux64/osx/win64)
v2.1.1.15071
Tiva E Series ARM MCUs (linux64/win64)
v2.1.1.15071
Tiva/Stellaris ICDI Debug Probe (linux64/osx/win64)
v2.1.3.15
UCD Digital Power Controllers (linux64/win64)
v1.1.5
core (linux64/osx/win64)
v10.0.0.20200106
Windows
XP, Windows Vista, Windows 7, Windows 8, Windows 8.1,Windows 10, Visual
SourceSafe, Visual Basic, and Visual C++ are all trademarks and/or registered
trademarks of Microsoft Corporation.
C2000, C5000, C54x, C55x, C6000, C6x, CC2538, CC26xx, CC32xx, OMAP, TMS320,
TMS570, MSP430, Stellaris, Tiva-C, Hercules, GUI Composer, Grace, Code Composer
Studio, Code Composer Studio App Center, TI-RTOS, SYS/BIOS, XDS560, XDS510,
XDS200, XDS100 and XDS110 are trademarks of Texas Instruments.
© Copyright 2021