Release Notes for Code Composer Studio™ Theia v1.2.0
These release notes contain valuable information which may not be included in other product documentation. This information will assist you in the use of Code Composer Studio™ Theia.The release notes are divided into six sections:
Contents
CCS Theia v1.1.0 uses a modified version of Theia-IDE ( https://theia-ide.org/ )
For additional information and support, please go to:
https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs_theia/index.html
|
Memory |
Disk space |
Processor |
|
|
Minimum |
4GB |
2.5GB |
2.0GHz single core |
|
Recommended |
8GB |
5.0GB |
2.0GHz dual core |
|
|
|
|
|
Please note that Code Composer Studio Theia v1.1.0 only supports MSPM0 devices.
Please note that Code Composer Studio Theia is a 64bit application and thus will not run on 32bit operating systems.
Supported distributions include:
Code Composer Studio Theia will run on other distributions but those are the officially supported and tested distributions. For more details on installation instructions as well as debug probe and device support please see this article on Linux Host Support.
Versions Supported
Each Code Composer Studio Theia release is validated against a set of macOS releases. This release was validated with:
Debug Probe Support
Details of the macOS releases, debug probes and devices supported is available here.
Please note that use of anti-virus software or a firewall may cause issues during installation.
McAfee software in particular has been especially troublesome.
If possible, disable anti-virus and firewall software during installation.
If not, use of the Offline Installer is strongly recommended.On Windows:
If you are using an Offline CCS Theia Installer, the zip file in which it is
distributed must first be extracted:1. Right-click on CCSTheia1.x.x.xxxxx_win64.zip and select "Extract All...".
2. Enter the directory where you wish to extract the files.
3. Click on Extract.Once extraction has successfully completed, proceed with the installation steps below.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx.exe.
2. Choose where you want to install.
3. Select the components you wish to install.On OS X:
Please visit https://software-dl.ti.com/ccs/esd/documents/ccs_macos_host_support.html
The offline installer is now distributed as disk images (.dmg files)
1. Right-click on CCSTheia1.x.x.xxxxx_osx.dmg and select "Open”. This will open the disk image and mount it.
To install Code Composer Studio Theia:1. Run ccs_theia_setup_1.x.x.xxxxx by clicking on the application in the Finder
2. Choose where you want to install.
3. Select the components you wish to install.On Linux:
Please visit https://software-dl.ti.com/ccs/esd/documents/users_guide_11.1.0/index.html
before installing CCS Theia on Linux. It contains important information on
installing CCS Theia on different Linux distributions, including CCS Theia dependencies that may need to be installed first.
Before installing CCS Theia, the tarball file in which the CCS Theia Installer is distributed must first be extracted:untar CCSTheia1.x.x.xxxxx_linux-x64.tar.gz and extract all files.
e.g. tar xfz CCSTheia1.x.x.xxxxx_linux-x64.tar.gz
Once extraction has successfully completed, proceed with the installation steps below.
Note: To facilitate the installation of emulation drivers, it is necessary to run part of the installation process as root.
You may if you wish install all of CCS Theia as root. However, it is preferred that you first install CCS Theia as a normal user and then install the drivers as root.
To install Code Composer Studio Theia as a normal user and emulation drivers as root:1. Run ccs_theia_setup_1.x.x.xxxxx.run as a normal user.
2. Choose where you want to install.
3. Select the components you wish to install.
4. Navigate to directory <Install-Folder>/ccs/install_scripts.
5. As root, execute script "install_drivers.sh".To install all of Code Composer Studio Theia as root:
1. Run ccs_theia_setup_1.x.x.xxxxx.run as root.
2. Choose where you want to install.
3. Select the components you wish to install.
· Theia IDE update to v1.40
· Energy Trace for MSPM0 (Windows only)
· Core trace for MSPM0 (Windows and Linux)
· Project system: File specific build options support
· Improvements to source lookup path configuration
· Real-time mode and continuous memory accesses (where supported by device)
· Watchpoint support
· Multi-instance of RTOS objects
· Memory allocation view
· Register view may appear blank the first time it is opened, please close and re-open the view. This only happens first time register view is opened.
· PC Hibernation affects CCS Theia inter-process communication. You may see a message “An unexpected error occurred in TI Cloud Agent! Please click one of the buttons below.“ with buttons to Save And Reload, Reload or Exit. Please choose Save and Reload option to restart CCS Theia and re-establish IPC communication.
· New Theia-IDE based IDE:
· Compilers
o TI CLANG 3.2.0 LTS compiler is bundled
· Device Support
o MSPM0
name
version
ARM Clang Compiler Tools (linux64/osx/win64)
V3.2.0.LTS
CCS Certificate (win64)
vmaster
CCS Installer (linux64/osx/win64)
v1.2.0.20231012131617
CCS Installer Dependencies (win64)
v1.2.0.20231012131617
CCS Installer Dependencies (linux64/osx)
v1.2.0.20231012131617
CCS Utilities (win64)
1.0.0.20230823
CCS Utilities (linux64/osx)
1.0.0.20230823
Debug Server (linux64/osx/win64)
v12.5.0.3202
Debug Server Flash (linux64/osx/win64)
v12.5.0.3202
Eclipse (linux64/osx/win64)
v4.23.0.0
Theia-ide (linux64/osx/win64)
V1.40
IDE GUI Composer (linux64/osx/win64)
v3.3.0
InstallBuilder (linux64/osx/win64)
v21.9.0
JRE (linux64/osx/win64)
v17.0.2
MSPM0 Support (linux64/osx/win64)
v1.02.00.05
MSVC 2017 Redistributable (x64) (win64)
v14.34.31938
Node.js (linux64/osx/win64)
V18.16.0
Shared Device Support (linux64/win64)
v1.1.7
Segger J Link
V7.88.0.c
Sys Config (linux64/osx/win64)
v1.18.0.3246
TI Cloud Agent (linux64/osx/win64)
V0.5.4507
TI Emulators (linux64/osx/win64)
v12.6.0.00002
TIREX4 Desktop (linux64/osx/win64)
v4.15.0.202310191339
Windows
10,Visual SourceSafe, Visual Basic, and Visual C++ are all trademarks and/or
registered trademarks of Microsoft Corporation.
MSPM0, GUI Composer, Code Composer Studio, XDS110 are trademarks of Texas
Instruments.
© Copyright 2023