4.8. Leveraging DMAC instructions¶
Dual Multiply and Accumulate (DMAC) instructions perform multiply-accumulate operations on two adjacent signed integers (16-bit) simultaneously, optionally shifting the products. A multiply-accumulate operation multiplies two numbers and adds that product to an accumulator.
C source |
Assembly output with DMAC |
|---|---|
long dmac(int* array1, int* array2, int M)
{
// Assert to the compiler that both arrays are 32bit aligned
_nassert((long)array1 % 2 == 0);
_nassert((long)array2 % 2 == 0);
// Assert to the compiler that M is even and > 0
_nassert((M > 0) && (M % 2 == 0));
int j;
long sum = 0;
for (j=0; j < M; j++)
sum += (long)array1[j] * array2[j];
return sum;
}
|
||dmac||:
ASR AL,1
MOVL XAR7,XAR5
ADDB AL,#-1
MOVZ AR5,AL
MOV P,#0
MOVB ACC,#0
RPT AR5
|| DMAC ACC:P,*XAR4++,*XAR7++
ADDL ACC,P
LRETR
|
Table 4.8 illustrates an approach to generating the DMAC instruction from C source. Refer to the TMS320C28x Optimizing C/C++ Compiler User’s Guide, Section 3.15, “Compiler Support for Generating DMAC Instructions” for details.