6.12. CDD ADC Module Migration

Migration Approach: Follow sequential migration for clear understanding of changes at each version. Each migration is organized by individual changes with description, old vs new comparison, and migration actions.

6.12.1. v05.00.00 (i.e release v26.00.01) from v04.00.00 (i.e release v26.00.00) Migration

6.12.1.1. Summary

Version v05.00.00 introduces the following changes to the CDD ADC module:

  1. ASysCtl configuration parameters moved to ResourceAllocator: Temperature sensor, analog reference voltage, and internal test node parameters have been removed from the ADC plugin and are now configured centrally in the ResourceAllocator ASysCtl container

  2. Cdd_Adc_SetInternalTestNode() replaced by Mcu_ASysCtl_SelectInternalTestNode(): The internal test node runtime API has moved from the ADC module to the MCU module

6.12.1.2. Change 1: ASysCtl configuration parameters moved to ResourceAllocator

6.12.1.2.1. Description

Configuration parameters that control analog system control (ASysCtl) hardware — temperature sensor enable, analog reference voltage selection, and internal test node selection — have been removed from the ADC plugin and the generated Cdd_Adc_HwUnitCfgType struct, and are now configured centrally in the ResourceAllocator plugin under ResourceAllocatorGeneral → ASysCtl. All ASysCtl register writes are now performed by Mcu_Init() from the generated Mcu_ASysCtlConfigType structure.

This affects two layers:

  • EB Tresos configuration: parameters removed from CddAdcConfigSet and CddAdcHwUnit containers

  • Generated C code: struct fields voltref, analogrefsel, and analogrefvoltsel removed from Cdd_Adc_HwUnitCfgType; macros CDD_ADC_TEMPERATURE_SENSOR_ENABLE and CDD_ADC_LOCK_TEMPERATURE_SENSOR removed from Cdd_Adc_Cfg.h

6.12.1.2.2. Old vs New

EB Tresos configuration parameters:

Old Parameter [ADC plugin]

Old location

New Parameter [ResourceAllocator Plugin]

New location

CddAdcEnableTemperatureSensor

CddAdcConfigSet

TemperatureSensorEnable

ASysCtl/TemperatureSensor

CddAdcInternalTestInput

CddAdcConfigSet

InternalTestNodeSelect

ASysCtl/InternalTestNode

CddAdcHwUnitAnalogRefABVoltageMode

CddAdcHwUnit

AnalogRefABMode

ASysCtl/AnalogReference

CddAdcHwUnitAnalogRefABVoltage

CddAdcHwUnit

AnalogRefABVoltage

ASysCtl/AnalogReference

CddAdcHwUnitAnalogRefCDEVoltageMode

CddAdcHwUnit

AnalogRefCDEMode

ASysCtl/AnalogReference

CddAdcHwUnitAnalogRefCDEVoltage

CddAdcHwUnit

AnalogRefCDEVoltage

ASysCtl/AnalogReference

Note

CddAdcLockTemperatureSensor has been removed and is not replaced by a configuration parameter. Temperature sensor locking is now a runtime operation performed via Mcu_ASysCtl_CommitLock() in the MCU module.

ASysCtl container in ResourceAllocator

Fig. 6.46 New ASysCtl container under ResourceAllocatorGeneral showing TemperatureSensor, AnalogReference, and InternalTestNode sub-containers

6.12.1.2.3. Migration Actions

  1. Note your existing ADC ASysCtl settings: Before migrating, record the values of CddAdcEnableTemperatureSensor, CddAdcInternalTestInput, and the four CddAdcHwUnitAnalogRef* parameters from your ADC plugin

  2. Open ResourceAllocator in EB Tresos: Navigate to ResourceAllocatorGeneral → ASysCtl

  3. Add an ASysCtl instance if one does not already exist

  4. Configure TemperatureSensor: Set TemperatureSensorEnable to match your previous CddAdcEnableTemperatureSensor value

  5. Configure AnalogReference: Set AnalogRefABMode and AnalogRefABVoltage to match the previous CddAdcHwUnitAnalogRefABVoltageMode and CddAdcHwUnitAnalogRefABVoltage values; repeat for AnalogRefCDEMode and AnalogRefCDEVoltage

  6. Configure InternalTestNode: Set InternalTestNodeSelect to match your previous CddAdcInternalTestInput value, using the new MCU_ASYSCTL_TEST_NODE_* enum literals in place of the old CDD_ADC_TEST_NODE_* literals

  7. Regenerate the project: Regenerate the MCU plugin output (Mcu_Cfg.c and Mcu_Cfg.h) so that the new Mcu_ASysCtlConfigType struct and Mcu_ASysCtlTestNodeType enum are available before building


6.12.1.3. Change 2: Cdd_Adc_SetInternalTestNode() replaced by Mcu_ASysCtl_SelectInternalTestNode()

6.12.1.3.1. Description

The runtime API for selecting the internal analog test node has moved from the ADC module to the MCU module. Cdd_Adc_SetInternalTestNode() has been removed and replaced by Mcu_ASysCtl_SelectInternalTestNode(). The enum type used for the test node selection has also changed from Cdd_Adc_InternalTestNodeType (generated in Cdd_Adc_Cfg.h) to Mcu_ASysCtlTestNodeType (generated in Mcu_Cfg.h), and the enum literal prefix has changed from CDD_ADC_TEST_NODE_ to MCU_ASYSCTL_TEST_NODE_.

6.12.1.3.2. Old vs New

Aspect

v04.00.00 (v26.00.00)

v05.00.00 (v26.00.01)

API

Cdd_Adc_SetInternalTestNode(TestNode)

Mcu_ASysCtl_SelectInternalTestNode(TestNode)

Header

Cdd_Adc.h

Mcu.h

Enum type

Cdd_Adc_InternalTestNodeType

Mcu_ASysCtlTestNodeType

Enum prefix

CDD_ADC_TEST_NODE_*

MCU_ASYSCTL_TEST_NODE_*

6.12.1.3.3. Migration Actions

  1. Find all calls to Cdd_Adc_SetInternalTestNode() in your application code

  2. Replace each call with Mcu_ASysCtl_SelectInternalTestNode(), keeping the same argument value

  3. Update enum literals: Replace CDD_ADC_TEST_NODE_* literals with the corresponding MCU_ASYSCTL_TEST_NODE_* literals (the names after the prefix are identical, e.g. CDD_ADC_TEST_NODE_VDDCORE → MCU_ASYSCTL_TEST_NODE_VDDCORE)

  4. Update includes: Ensure Mcu.h is included in any file that calls Mcu_ASysCtl_SelectInternalTestNode(); Cdd_Adc.h no longer exposes this API


6.12.2. v04.00.00 (i.e release v26.00.00) from v03.00.01 (i.e release v01.04.01) Migration

6.12.2.1. Summary

Version v04.00.00 introduces API enhancements for temperature conversion:

  1. Voltref Parameter Added to Temperature APIs: Voltref parameter added to Cdd_Adc_GetTemperatureC() and Cdd_Adc_GetTemperatureK() APIs for accurate temperature calculations with different voltage references

6.12.2.2. Change 1: Voltref Parameter Added to Temperature APIs

6.12.2.2.1. Description

The Cdd_Adc_GetTemperatureC() and Cdd_Adc_GetTemperatureK() APIs did not support temperature calculation for different voltage references when using external reference mode, limiting their usability in systems with non-standard voltage references. When ADC is configured with external voltage reference mode using a non-standard voltage (e.g., 3.0V), calling these APIs to convert temperature sensor readings produces incorrect temperature calculations because the API cannot account for the actual external voltage reference value. This results in inaccurate temperature readings that can affect temperature-dependent control algorithms and safety mechanisms. To address this limitation, a new Voltref parameter (float32) has been added to both APIs, enabling accurate temperature calculation by accepting the actual voltage reference value being used (internal values such as 2.5F for 2.5V or 3.3F for 3.3V, or the actual external voltage reference value).

6.12.2.2.2. Old vs New API Signature

Old (v03.00.01):

Cdd_Adc_GetTemperatureC(VAR(Cdd_Adc_HwUnitInstanceType, AUTOMATIC) HwUnit,VAR(Cdd_Adc_ValueGroupType, AUTOMATIC) TempResult)
Cdd_Adc_GetTemperatureK(VAR(Cdd_Adc_HwUnitInstanceType, AUTOMATIC) HwUnit,VAR(Cdd_Adc_ValueGroupType, AUTOMATIC) TempResult)

New (v04.00.00):

Cdd_Adc_GetTemperatureC(VAR(Cdd_Adc_HwUnitInstanceType, AUTOMATIC) HwUnit,VAR(Cdd_Adc_ValueGroupType, AUTOMATIC) TempResult, float32 Voltref)
Cdd_Adc_GetTemperatureK(VAR(Cdd_Adc_HwUnitInstanceType, AUTOMATIC) HwUnit,VAR(Cdd_Adc_ValueGroupType, AUTOMATIC) TempResult, float32 Voltref)

6.12.2.2.3. Migration Actions

  1. Identify Temperature API Usage: Search your codebase for all calls to Cdd_Adc_GetTemperatureC() and Cdd_Adc_GetTemperatureK()

  2. Determine Voltage Reference: Identify the voltage reference configuration for your ADC:

    • Internal 2.5V reference: Use 2.5F

    • Internal 3.3V reference: Use 3.3F

    • External reference: Use the actual external voltage reference value (e.g., 3.0F for 3.0V)

  3. Update API Calls: Add the Voltref parameter to all temperature API calls:

    Example Migration:

    // Old code (v03.00.01)
    float32 tempC = Cdd_Adc_GetTemperatureC(HwUnit,AdcResult);
    float32 tempK = Cdd_Adc_GetTemperatureK(HwUnit,AdcResult);
    
    // New code (v04.00.00) - Internal 2.5V reference
    float32 tempC = Cdd_Adc_GetTemperatureC(HwUnit,AdcResult, 2.5F);
    float32 tempK = Cdd_Adc_GetTemperatureK(HwUnit,AdcResult, 2.5F);
    
    // New code (v04.00.00) - External 3.0V reference
    float32 tempC = Cdd_Adc_GetTemperatureC(HwUnit,AdcResult, 3.0F);
    float32 tempK = Cdd_Adc_GetTemperatureK(HwUnit,AdcResult, 3.0F);
    
  4. Verify Voltage Reference Value: Ensure the Voltref parameter exactly matches the actual voltage reference being used in your hardware configuration. Incorrect values will result in inaccurate temperature calculations.

  5. Test Temperature Readings: After migration, verify temperature readings against known reference temperatures to confirm accuracy with the new voltage reference parameter.

6.12.3. v03.00.00 (i.e release v01.04.00) from v02.00.01 (i.e release v01.03.00) Migration

6.12.3.1. Summary

Version v03.00.00 introduces Resource Allocator as a mandatory architectural foundation and SDK-based DMA integration. This represents a fundamental shift from direct parameter configuration to centralized resource management:

  1. Resource Allocator Introduction and Hardware Unit Configuration Updates: Resource Allocator becomes mandatory with CddAdcHwUnit configurations updated to reference Resource Allocator instances

  2. SDK-Based DMA Integration: Optional DMA integration for efficient ADC result transfers

  3. Symbolic Name Uniqueness Requirements: Enhanced validation requires unique symbolic names across configurations

PREREQUISITE: Complete Resource Allocator Setup before proceeding.

6.12.3.2. Change 1: Resource Allocator Introduction and Hardware Unit Configuration Updates

6.12.3.2.1. Description

Resource Allocator becomes a mandatory architectural foundation for the CDD ADC module, with CddAdcHwUnit configurations updated to reference Resource Allocator instances. This represents a fundamental shift from direct parameter configuration to centralized resource management, where CDD ADC instances are allocated through Resource Allocator and then referenced by hardware unit configurations.

6.12.3.2.2. Old vs New Configuration

Old (v02.00.01): Direct parameter selection was used without Resource Allocator dependency.

Old CDD ADC Config

Fig. 6.47 v02.00.01: Direct ADC hardware unit parameter selection

New (v03.00.00): CDD ADC hardware unit configurations now reference instances allocated through Resource Allocator.

Select CDD ADC Instance

Fig. 6.48 v03.00.00: Set CddAdcHwInstanceRef to point to the corresponding Cdd_AdcAllocatedInstance in Resource Allocator

6.12.3.2.3. Migration Actions

  1. Setup Resource Allocator: Follow Resource Allocator Setup

  2. Navigate to Context: Navigate to ResourceAllocatorGeneral → Context → Cdd_Adc and add CDD ADC allocator:

Add CDD ADC Allocator

Fig. 6.49 Navigate to Context and add CDD ADC allocator

  1. Add CDD ADC Instance: Add Cdd_AdcAllocatedInstance entries for each ADC instance your application requires:

Add CDD ADC Instance

Fig. 6.50 Add Cdd_AdcAllocatedInstance entries for each ADC instance your application requires

  1. Configure ADC Instance: Configure the InstanceName, Frame, and BaseAddr for each allocated instance:

Configure CDD ADC Instance

Fig. 6.51 Configure the InstanceName, Frame, and BaseAddr for each allocated instance

  1. Configure Safety Checker Instance (Optional): If your application requires safety-critical ADC monitoring, configure CddAdcSafetyCheckerInstance:

Configure CDD ADC Safety Checker Instance

Fig. 6.52 Configure CddAdcSafetyCheckerInstance for safety-critical applications (e.g., ADCSAFETYCHECK1)

  1. Configure Checker Interrupt Event Instance (Optional): If your application requires interrupt-based safety monitoring, configure CddAdcCheckerInterruptEvtInstance:

Configure CDD ADC Checker Interrupt Event Instance

Fig. 6.53 Configure CddAdcCheckerInterruptEvtInstance for interrupt-based safety monitoring (e.g., ADCSAFETYCHECKINIEVT1)

  1. Complete Configuration: Finalize CDD ADC instance allocation:

Final CDD ADC Configuration

Fig. 6.54 Complete CDD ADC instance allocation

  1. Navigate to CddAdcHwUnit: Navigate to Cdd → CddAdcHwUnit and update configurations to reference the CDD ADC instances allocated in Resource Allocator

  2. Open Hardware Unit Configuration: Access the CddAdcHwUnit configuration that needs to be updated

  3. Set Instance Reference: Set CddAdcHwInstanceRef to point to the corresponding Cdd_AdcAllocatedInstance in Resource Allocator

  4. Verify Automatic Derivation: Confirm that the CddAdcHwInstance parameter is now automatically derived from the Resource Allocator reference

6.12.3.3. Change 2: SDK-Based DMA Integration (Optional)

6.12.3.3.1. Description

Version v03.00.00 introduces SDK-based DMA integration for efficient ADC result transfers without CPU intervention. This is an optional feature that can be enabled for improved performance in applications that require high-speed ADC data transfer.

6.12.3.3.2. Old vs New DMA Configuration

Old (v02.00.01): No DMA integration available for ADC result transfers.

New (v03.00.00): Optional SDK-based DMA integration with CddAdcEnableDma parameter.

Add DMA Configuration

Fig. 6.55 Add CddAdcGroup configuration for DMA

Configure DMA Parameters

Fig. 6.56 Configure CddAdcEnableDma parameter for ADC groups

6.12.3.3.3. Migration Actions

  1. Evaluate DMA Requirement: Determine if your application requires DMA for ADC result transfers for improved performance

  2. Enable DMA (Optional): If using DMA for ADC result transfers, enable CddAdcEnableDma in the group configuration

  3. Configure SDK DMA: Configure the DMA channel in the SDK/system configuration on the application side. Refer to ADC + DMA Integration Guide for detailed integration steps and DMA Transfer Example for implementation examples

  4. Ensure Memory Alignment: Ensure proper memory alignment for DMA buffers to prevent transfer issues

6.12.3.4. Change 3: Symbolic Name Uniqueness Requirements

6.12.3.4.1. Description

Version v03.00.00 introduces enhanced validation that requires symbolic names to be unique across configurations. When migrating from v02.00.00 to v03.00.00, EB Tresos will generate validation errors if symbolic names are not unique. This is in accordance with [SWS_BSW_00200].

6.12.3.4.2. Old vs New Validation Requirements

Uniqueness Requirements:

Parameter

v02.00.01

v03.00.00

CddAdcGroup (container name)

No uniqueness constraint

Must be unique across all HW units

CddAdcPpbConfig (container name)

No uniqueness constraint

Must be unique across all HW units

CddAdcHwInstanceRef

No uniqueness constraint

Must be unique across all containers

CddAdcGlbSwTrigId

No uniqueness constraint

Must be unique across all containers

CddAdcCheckerInstanceRef

No uniqueness constraint

Must be unique across all containers

CddAdcCheckerIntEvtInstanceRef

No uniqueness constraint

Must be unique across all containers

6.12.3.4.3. Migration Actions

  1. Review Container Names: Check all CddAdcGroup and CddAdcPpbConfig container names for uniqueness across all HW units

  2. Review Instance References: Ensure CddAdcHwInstanceRef, CddAdcCheckerInstanceRef, and CddAdcCheckerIntEvtInstanceRef are unique across all containers

  3. Review Trigger IDs: Verify CddAdcGlbSwTrigId values are unique across all containers

  4. Resolve Conflicts: Update any duplicate symbolic names to ensure uniqueness and avoid validation errors during migration

  5. Validate Configuration: Run validation in EB Tresos to confirm all symbolic names are now unique

Note

The Resource Allocator module must be configured before the CDD ADC module to ensure correct instance availability. For more details on Resource Allocator configuration, see the Resource Allocator Module User Guide.

6.12.4. v02.00.00 (i.e release v01.02.00) from v01.00.00 (i.e release v01.01.00) Migration

6.12.4.1. Summary

Version v02.00.00 introduces schema compatibility updates to align with updated plugin structure and reference paths:

  1. AR-ELEMENT Name Change: Generated .xdm file AR-ELEMENT name requires updating for schema compatibility

  2. MODULE-CONFIGURATION Path Update: Generated .xdm file MODULE-CONFIGURATION definition path requires updating

  3. Reference Path Updates: Generated .xdm file reference paths require updating due to schema structure changes

Note

The CDD ADC v2.0.0 plugin contains updated schema definitions that are not backward compatible with v1.0.0 generated configurations. To use existing v1.0.0 configurations with the v2.0.0 plugin, the generated .xdm files (created by EB Tresos from your configuration) must be updated.

6.12.4.2. Change 1: AR-ELEMENT Name Change in Generated .xdm File

6.12.4.2.1. Description

When upgrading from v1.0.0 to v2.0.0, the generated .xdm file from EB Tresos contains AR-ELEMENT names that are not compatible with the new plugin schema. The AR-ELEMENT name needs to be updated in the generated .xdm file to ensure compatibility.

6.12.4.2.2. Old vs New AR-ELEMENT Configuration

Generated .xdm File AR-ELEMENT Name:

v01.00.00 Generated .xdm

v02.00.00 Required .xdm

<d:chc name="Cdd_Adc" type="AR-ELEMENT"

<d:chc name="Cdd" type="AR-ELEMENT"

6.12.4.2.3. Migration Actions

  1. Locate Generated .xdm File: Find your project’s generated .xdm file (created by EB Tresos from your configuration)

  2. Open File for Editing: Open the generated .xdm file in a text editor

  3. Find AR-ELEMENT Reference: Locate the line containing <d:chc name="Cdd_Adc" type="AR-ELEMENT"

  4. Update AR-ELEMENT Name: Change the AR-ELEMENT name from Cdd_Adc to Cdd

  5. Save File: Save the updated .xdm file

6.12.4.3. Change 2: MODULE-CONFIGURATION Path Update in Generated .xdm File

6.12.4.3.1. Description

The MODULE-CONFIGURATION definition path in the generated .xdm file needs to be updated to reflect the new schema structure. The path must include the additional Cdd component for proper module reference.

6.12.4.3.2. Old vs New MODULE-CONFIGURATION Path

Generated .xdm File MODULE-CONFIGURATION Path:

v01.00.00 Generated .xdm

v02.00.00 Required .xdm

<a:a name="DEF" value="ASPath:/TI_F29H85x/Cdd_Adc"/>

<a:a name="DEF" value="ASPath:/TI_F29H85x/Cdd_Adc/Cdd"/>

6.12.4.3.3. Migration Actions

  1. Continue Editing .xdm File: In the same generated .xdm file being edited

  2. Find MODULE-CONFIGURATION Path: Locate the line containing <a:a name="DEF" value="ASPath:/TI_F29H85x/Cdd_Adc"/>

  3. Update Definition Path: Change the MODULE-CONFIGURATION path from ASPath:/TI_F29H85x/Cdd_Adc to ASPath:/TI_F29H85x/Cdd_Adc/Cdd

  4. Verify Path Structure: Ensure the updated path includes the additional /Cdd component

  5. Save Changes: Save the updated .xdm file

6.12.4.4. Change 3: Reference Path Updates in Generated .xdm File

6.12.4.4.1. Description

Any REFERENCE type parameters in the generated .xdm file that refer to other CDD ADC parameters by their schema path must be updated due to the schema structure change. All internal reference paths need to be updated to reflect the new schema hierarchy.

6.12.4.4.2. Old vs New Reference Paths

Generated .xdm File Reference Path Example:

For CddAdcPpbChannel references expecting a channel reference:

v01.00.00 Generated .xdm Reference Path

v02.00.00 Required .xdm Reference Path

/Cdd_Adc/Cdd_Adc/CddAdcConfigSet/CddAdcHwUnit_0/CddAdcGroup_0/CddAdcChannel_0

/Cdd_Adc/Cdd/CddAdcConfigSet/CddAdcHwUnit_0/CddAdcGroup_0/CddAdcChannel_0

6.12.4.4.3. Migration Actions

  1. Continue Editing .xdm File: In the same generated .xdm file being edited

  2. Search for Reference Paths: Find all REFERENCE type parameters that contain /Cdd_Adc/Cdd_Adc/ in their paths

  3. Update Reference Paths: Change all occurrences of /Cdd_Adc/Cdd_Adc/ to /Cdd_Adc/Cdd/

  4. Verify All Updates: Ensure all reference paths now use the correct schema hierarchy

  5. Save Final Changes: Save the completely updated .xdm file

Generated .xdm File Structure Comparison:

Old (v01.00.00 Generated .xdm File):

<d:lst type="TOP-LEVEL-PACKAGES">
<d:ctr name="Cdd_Adc" type="AR-PACKAGE">
<d:lst type="ELEMENTS">
<d:chc name="Cdd_Adc" type="AR-ELEMENT" value="MODULE-CONFIGURATION">
<d:ctr type="MODULE-CONFIGURATION">
<a:a name="DEF" value="ASPath:/TI_F29H85x/Cdd_Adc"/>

New (v02.00.00 Compatible .xdm File):

<d:lst type="TOP-LEVEL-PACKAGES">
<d:ctr name="Cdd_Adc" type="AR-PACKAGE">
<d:lst type="ELEMENTS">
<d:chc name="Cdd" type="AR-ELEMENT" value="MODULE-CONFIGURATION">
<d:ctr type="MODULE-CONFIGURATION">
<a:a name="DEF" value="ASPath:/TI_F29H85x/Cdd_Adc/Cdd"/>

Note

Only the generated .xdm files (created by EB Tresos from your configuration) can be modified. The plugin .xdm files themselves cannot and should not be modified.