5.14. CDD I2C Module

5.14.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

API

Application Programming Interface

BSW

Basic Software

DET

Default Error Tracer

I2C

Inter Integrated Circuit

MCAL

Micro Controller Abstraction Layer

MCU

Micro Controller Unit

OS

Operating System

5.14.2. Introduction

The I2C driver is part of complex device drivers (CDD) which provides API for the inter-integrated circuit (I2C) module. The I2C driver provides an interface to communicate to the devices connected to the I2C bus. External components attached to this 2-wire serial bus can transmit/receive data to/from the device through the I2C module.

The following figure shows where the I2C is located in the AUTOSAR architecture.

I2C Architecture

Fig. 5.55 I2C Architecture

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile

Vendor ID

CDD_I2C_VENDOR_ID (44)(TEXAS INSTRUMENTS)

Module ID

CDD_I2C_MODULE_ID (255)

5.14.3. Functional Overview

The I2C module provides an interface between the MCU and devices compliant with the NXP Semiconductors Inter-IC bus (I2C bus) specification version 2.1, and connected by way of an I2C bus. External components attached to this 2-wire serial bus can transmit/receive 1- to 8-bit data to/from the device through the I2C module.

The I2C driver supports Controller Mode (Master) and Target Mode (Slave) operation.

5.14.3.1. Controller Mode (Master)

In Controller Mode, the I2C instance initiates and controls all data transfers on the bus. The expected flow for utilization of the driver in controller mode is:

  1. Interrupt registration (only required in case of interrupt mode)

  2. I2C driver initialization using Cdd_I2c_Init()

  3. Post initialization, buffer setup linking is done to point channels to their respective buffers using Cdd_I2c_SetupEB() or Cdd_I2c_SetupEBDynamic()

  4. For writing data to target devices, Cdd_I2c_AsyncTransmit() is used in both polling as well as interrupt mode

  5. For reception of data from I2C target devices, Cdd_I2c_AsyncTransmit() can be used in interrupt mode

  6. If polling mode is being used, use Cdd_I2c_MainFunction() to process any sequence in the queue and update the status of the queue to real time value

5.14.3.2. Target Mode (Slave)

In Target Mode, the I2C instance responds to requests from a controller device on the bus. Target Mode supports interrupt mode only. The expected flow for utilization of the driver in target mode is:

  1. I2C driver initialization using Cdd_I2c_Init() with the HW unit configured as Target Mode

  2. Submit initial TX buffer using Cdd_I2c_TargetSubmitTxBuffer() for controller read requests

  3. Submit initial RX buffer using Cdd_I2c_TargetSubmitRxBuffer() for controller write requests

  4. Start target mode operation using Cdd_I2c_TargetStart()

  5. Handle notifications via configured callbacks:

    • Cdd_I2c_TargetRxStartNotification: Called when controller initiates write operation

    • Cdd_I2c_TargetTxStartNotification: Called when controller initiates read operation

    • Cdd_I2c_TargetRxCompleteNotification: Called when RX buffer is full or STOP is detected

    • Cdd_I2c_TargetTxCompleteNotification: Called when TX buffer is empty or STOP is detected

    • Cdd_I2c_TargetErrorNotification: Called on errors (overflow, underflow, no buffer, NACK)

  6. In notification callbacks, submit new buffers as needed and process received/transmitted data

  7. Stop target mode operation using Cdd_I2c_TargetStop() when done

Note

Controller and Target modes are mutually exclusive per HW unit and are configured at initialization time. Target Mode supports interrupt mode only and cannot be configured in polling mode.

5.14.4. Hardware Features

On F29x platforms, there are 2 I2C instances I2CA and I2CB.

5.14.4.1. Hardware Features Supported

5.14.4.1.1. Common Features

Feature

Description

Polling Mode

Software polling for I2C events (at instance level)

Interrupt Mode

Hardware interrupt-driven operation (at instance level)

7-bit Addressing

Standard 7-bit I2C address scheme

10-bit Addressing

Extended 10-bit I2C address scheme

Configurable Own Address

Device’s own I2C address configuration (at instance level)

5.14.4.1.2. Controller Mode (Master) Features

Feature

Description

Configurable Baudrate

I2C bus speed configuration (at instance level)

Configurable Target Address

Address of target device to communicate with (at channel level)

Restart Mode

Stop or no-stop between channel transfers (at channel level)

Read/Write Operations

Separate read and write channel configurations (at channel level)

Multiple Channels per Sequence

Chain multiple transfers in a single sequence

Sequence Management

Queue and execute multiple sequences

5.14.4.1.3. Target Mode (Slave) Features

Feature

Description

Address Matching

Respond when own address is detected on bus

TX/RX Buffer Management

Dynamic buffer submission for data transfer

Start Notifications

Callbacks when controller initiates read/write

Completion Notifications

Callbacks when transfer completes or STOP detected

Error Notifications

Callbacks for overflow, underflow, NACK, no buffer

5.14.4.2. Hardware Features Not Supported by the Driver

  • DMA Mode

  • FIFO Mode

  • Multi Master Mode and Arbitration Loss scenarios are not tested

5.14.4.3. Software Supported Features

5.14.4.3.1. Common Features

  • Configurable Development Error Detection

  • Configurable Hardware Units

  • Configurable Data Length to Transfer

  • HW Unit Reset API for Bus Recovery

  • Configurable Controller/Target Mode per HW Unit

5.14.4.3.2. Controller Mode Features

  • Configurable Sequence Size

  • Configurable Channel Size

  • Configurable Channels

  • Configurable Sequences

  • Multiple Channels in a Sequence

  • Transfer Complete and Error Notification Callbacks

5.14.4.3.3. Target Mode Features

  • Start/Stop Control API

  • Dynamic TX/RX Buffer Submission

  • Start Notification Callbacks (TX and RX)

  • Complete Notification Callbacks (TX and RX)

  • Error Notification Callback

  • Event Notifications for Transfer Complete, STOP, Buffer Overflow/Underflow, and NACK conditions

5.14.5. Source Files

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Cdd_I2c
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_I2c_Hw.h : Contains data structures and Internal function declarations for HW access.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Utils.h : Contains internal function declarations for queue implementation.
┃ ┃ ┃ ┗ 📜Cdd_I2c.h : Contains the API declarations of the Cdd_I2c driver to be used by upper layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_I2c_Hw.c : Contains internal function definitions for HW access.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Irq.c : Contains the ISR implementation for both controller and target modes.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Priv.c : Contains internal function definitions that support the API.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Target.c : Contains target mode API implementation.
┃ ┃ ┃ ┣ 📜Cdd_I2c_Utils.c : Contains internal function definitions for queue implementation.
┃ ┃ ┃ ┗ 📜Cdd_I2c.c : Contains controller mode API implementation.
┃ ┃ ┗ 📜CMakeLists.txt

Description of generated files is provided below:

Plugin Files

Description

Cdd_I2c_Cfg.h

This file contains general container configuration parameters like DET error ON, Polling mode OFF, Sequence size, Queue size, Channel size etc.

Cdd_I2c_Cfg.c

Contains all channels Pre-Build Configuration parameters

The below diagram shows the files structure for the I2C driver.

I2C File Structure

Fig. 5.56 I2C File Structure

5.14.6. Module Requirements

5.14.6.1. Memory Mapping

The objects (e.g. variables, functions, constants) are declared by compiler independent definitions – the compiler abstraction definitions. Each compiler abstraction definition is assigned to a memory section. The following table contains the memory section names and the compiler abstraction definitions of the I2C and illustrates their assignment among each other.

Memory Mapping Sections

I2C_CODE

I2C_VAR_NO_INIT

I2C_VAR_INIT

I2C_CONST

I2C_CFG

I2C_APPL_CODE

I2C_APPL_DATA

CDD_I2C_START_SEC_CODE

x

CDD_I2C_STOP_SEC_CODE

x

CDD_I2C_START_SEC_ISR_CODE

x

CDD_I2C_STOP_SEC_ISR_CODE

x

CDD_I2C_START_SEC_CONFIG_DATA

x

CDD_I2C_STOP_SEC_CONFIG_DATA

x

CDD_I2C_START_SEC_CONFIG_CONST_32

x

CDD_I2C_STOP_SEC_CONFIG_CONST_32

x

CDD_I2C_START_SEC_VAR_NOINIT_UNSPECIFIED

x

CDD_I2C_STOP_SEC_VAR_NOINIT_UNSPECIFIED

x

CDD_I2C_START_SEC_VAR_INIT_UNSPECIFIED

x

CDD_I2C_STOP_SEC_VAR_INIT_UNSPECIFIED

x

Application buffers passed to I2C

x

Notification called from I2C

x

5.14.6.2. Scheduling

Schedule Function API

Description

Applicable Mode

Cdd_I2c_MainFunction

This function processes the I2C transmission in polling mode

Controller Mode only

Note

Cdd_I2c_MainFunction is applicable only for Controller Mode. Target Mode operates entirely in interrupt-driven mode and does not require a cyclic main function. All Target Mode operations are handled through interrupt callbacks.

5.14.6.3. Error Handling

5.14.6.3.1. Development Error Reporting

By default, development errors are reported to the DET using the service Det_ReportError(), if development error reporting is enabled (i.e. precompile parameter CDD_I2C_DEV_ERROR_DETECT==STD_ON). If another module is used for development error reporting, the function prototype for reporting the error can be configured by the integrator, but must have the same signature as the service Det_ReportError(). The reported I2C ID is 255

5.14.6.3.2. Development Error Codes

Type of Error

Related Error code

Value (Hex)

No errors

CDD_I2C_E_NO_ERROR

0x00

API service used without module initialization

CDD_I2C_E_UNINIT

0x01

Init service called twice without DeInit

CDD_I2C_E_ALREADY_INITIALIZED

0x02

Channel out of bounds, exceeds the maximum number of configured channels

CDD_I2C_E_PARAM_CHANNEL

0x04

Sequence out of bounds, exceeds the maximum number of configured sequences

CDD_I2C_E_PARAM_SEQUENCE

0x05

Length out of bounds – a zero length is not accepted. The total length is limited to 65535

CDD_I2C_E_PARAM_LENGTH

0x06

An invalid version info pointer has been passed (a NULL_PTR)

CDD_I2C_E_PARAM_VINFO_PTR

0x07

An invalid configuration has been passed (a non NULL_PTR)

CDD_I2C_E_PARAM_CONFIG

0x08

Two invalid transmission buffers have been passed (no NULL_PTR/ or both NULL_PTR)

CDD_I2C_E_PARAM_TRANS_BUFFER

0x09

Address out of bounds, exceeds the limit of the configured address range

CDD_I2C_E_PARAM_ADDRESS

0x0A

Buffer direction conflicts with channel direction set via EB

CDD_I2C_E_PARAM_DIRECTION

0x0B

API service called with invalid HW unit ID

CDD_I2C_E_PARAM_HWUNIT

0x16

API service called with sequence is busy

CDD_I2C_E_SEQ_BUSY

0x17

API service called with invalid mode - controller or target

CDD_I2C_E_PARAM_MODE

0x18

5.14.6.3.3. Runtime Error Codes

5.14.6.3.3.1. Controller Mode Runtime Errors

The following error codes are reported to the application via the Cdd_I2c_SequenceErrorNotification callback in controller mode:

Type of Error

Related Error code

Value (Hex)

NACK was received from target device

CDD_I2C_E_NACK_RECEIVED

0x01

Master lost arbitration (SDA stuck low or another master won arbitration)

CDD_I2C_E_ARBITRATION_FAILURE

0x02

SCL line is stuck low

CDD_I2C_E_BUS_FAILURE

0x03

Sequence was cancelled by user

CDD_I2C_E_CANCELLED

0x04

HW unit was reset (bus-off recovery)

CDD_I2C_E_HW_UNIT_RESET

0x08

5.14.6.3.3.2. Target Mode Runtime Errors

The following error codes are reported to the application via target mode notification callbacks (Cdd_I2c_TargetRxCompleteNotification, Cdd_I2c_TargetTxCompleteNotification, or Cdd_I2c_TargetErrorNotification):

Type of Error

Related Error code

Value (Hex)

Target received NACK from controller

CDD_I2C_E_NACK_RECEIVED

0x01

RX buffer overflow occurred

CDD_I2C_E_RX_OVERFLOW

0x05

TX buffer underflow occurred

CDD_I2C_E_TX_UNDERFLOW

0x06

No buffer was submitted

CDD_I2C_E_NO_BUFFER

0x07

5.14.7. Used Resources

5.14.7.1. Interrupt Handling

Interrupt routines are provided by the CDD I2C driver is Cdd_I2c_Isr_Handler(). Basically, the ISR’s are in the file Cdd_I2c_Irq.c. User might edit it for adapting for the suitable OS. Interrupt handler shall be provided for each instance of the CDD I2C driver. The corresponding CDD I2C Interrupt numbers are:

Hardware Unit

Interrupt Name

Interrupt handler

I2CA

I2CA_INT

Cdd_I2c_I2CA_ISR

I2CB

I2CB_INT

Cdd_I2c_I2CB_ISR

Note

Same Interrupt Category needs to be configured in both I2C and OS Modules.

5.14.7.2. Instance Support

CPU instances

supported

CPU 1

YES

CPU 2

NO

CPU 3

NO

5.14.8. Integration Description

5.14.8.1. Dependent Modules

5.14.8.1.1. DET

The module I2C depends on the DET (by default) in order to report development errors. Detection and reporting of development errors can be enabled or disabled by the switch “Enable Development Error Detection” on the “General” container within the module I2C. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.

5.14.8.1.2. MCU

The module MCU powers up the microcontroller’s peripherals at startup time and initializes clock source. Since the peripherals are also containing the registers for I/O functionality they have to be activated if it is intended to use them.

5.14.8.1.3. PORT

The module PORT enables the I2C lines at startup time. To operate the I2C properly, the PORT driver has to be configured. The PORT driver sets the Pins to the required values for the I2C to operate. The Pins used are SDA (serial data line) and SCL (serial clock). An open drain configuration is recommended. Some I2C drivers require the PORT for switching from I2C functionality to DIO functionality – to use the “clock free” procedure - and back.

5.14.8.1.4. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that CDD I2C module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.

For CDD_I2C Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

CDD_I2C Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

CDD_I2C_EXCLUSIVE_AREA_0

Cdd_I2c_SetupEB()
Cdd_I2c_SetupEBDynamic()
Cdd_I2c_AsyncTransmit()
Cdd_I2c_Cancel()
Cdd_I2c_MainFunction()

To protect against multiple access for shared resources

OS_RESOURCE : If the I2C APIs are only called from pre-emptible task context, its recommended to use this mechanism as it takes care of resource access protection and task priority management.
None: If I2C APIs are only called from non pre-emptible task context or during init, its recommended to use this mechanism as multiple access protection to shared resource is not needed.

5.14.8.2. Multi-core and Resource Allocator

The I2C module uses the Resource Allocator to allocate I2C peripheral instances to CPU cores and configure their memory-mapped base addresses. Each allocation is placed inside a Context that maps to a CPU core (e.g. CPU1). The CurrentContext parameter in the Resource Allocator selects which Context is active for MCAL execution. See the Resource Allocator Module User Guide for details on configuring device-specific settings.

5.14.8.2.1. Resource Allocator Usage Example

To allocate I2CA to CPU1 using FRAME0:

  1. In the Resource Allocator configuration, create a new I2c instance allocation under the CPU1 Context

  2. Set InstanceName to I2CA

  3. Set Frame to FRAME0

  4. Set BaseAddr to I2CA_BASE_FRAME(0U)

Resource Allocator Configuration:
├── Context (Core: CPU1)
│   └── I2cInstanceAllocation
│       ├── InstanceName: I2CA
│       ├── Frame: FRAME0
│       └── BaseAddr: I2CA_BASE_FRAME(0U)

5.14.9. Configuration

5.14.9.1. Configuration Parameters

5.14.9.1.1. CddI2cGeneral

General configuration settings for Complex device driver

5.14.9.1.1.1. CddI2cDevErrorDetect

Item

Name

CddI2cDevErrorDetect

Description

I2c Dev Error ON/OFF.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

5.14.9.1.1.2. CddI2cVersionInfoApi

Item

Name

CddI2cVersionInfoApi

Description

Pre-processor switch to enable/disable the get version info API.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

5.14.9.1.1.3. CddI2cCancelApi

Item

Name

CddI2cCancelApi

Description

Pre-processor switch to enable/disable the cancel API.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.14.9.1.1.4. CddI2cStatusApi

Item

Name

CddI2cStatusApi

Description

Pre-processor switch to enable/disable the get status API.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.14.9.1.1.5. CddI2cMainFunctionPeriod

Item

Name

CddI2cMainFunctionPeriod

Description

This parameter describes the period for cyclic call to Cdd_I2c_MainFunction. Unit is seconds.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0.01

Max-value

INF

Min-value

0.0

5.14.9.1.2. CddI2cHwConfig

This container contains the HW unit initialization parameters

5.14.9.1.2.1. CddI2cHwUnitMode

Item

Name

CddI2cHwUnitMode

Description

Selects the operation mode of the I2C HW unit (Controller or Target).

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_I2C_MODE_CONTROLLER

Range

CDD_I2C_MODE_CONTROLLER
CDD_I2C_MODE_TARGET

5.14.9.1.2.2. CddI2cHwUseInterrupts

Item

Name

CddI2cHwUseInterrupts

Description

Switches to activate or deactivate interrupt controlled job processing for this HW unit. Always enabled in Target mode.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.14.9.1.2.3. CddI2cHwBaudrate

Item

Name

CddI2cHwBaudrate

Description

Channel Bit Rate (Range = 10kbps - 400kbps). Value needs to be provided in bits per second.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

400000

Max-value

400000

Min-value

10000

5.14.9.1.2.4. CddI2cHwUnitFrequency

Item

Name

CddI2cHwUnitFrequency

Description

Frequency which the HW unit will utilize(Range = 7 MHz - 12 MHz), please note that this differs from the bus frequency used for communication

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

10000000

Max-value

12000000

Min-value

7000000

5.14.9.1.2.5. CddI2cHwAddressScheme

Item

Name

CddI2cHwAddressScheme

Description

Specifies whether the HW unit uses 7-bit or 10-bit addressing.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_I2C_ADDRESS_7_BIT

Range

CDD_I2C_ADDRESS_7_BIT
CDD_I2C_ADDRESS_10_BIT

5.14.9.1.2.6. CddI2cHwOwnAddress

Item

Name

CddI2cHwOwnAddress

Description

Own address - used in both 7 and 10-bit address mode.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

127

Max-value

1023

Min-value

0

5.14.9.1.2.7. CddI2cHwIrqType

Item

Name

CddI2cHwIrqType

Description

This parameters defines the category of the interrupt.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ISR_CAT1_RTINT

Range

ISR_CAT1_INT
ISR_CAT1_RTINT
ISR_CAT2_INT

5.14.9.1.2.8. CddI2cHwUnitRef

Item

Name

CddI2cHwUnitRef

Description

Reference to I2c HW unit to use.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.14.9.1.2.9. CddI2cHwFunctionalClock

Item

Name

CddI2cHwFunctionalClock

Description

Reference to a container of the type McuClockReferencePoint, to select an input clock.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.14.9.1.2.10. CddI2cTargetCallbacks

Container for target mode callback notifications. Only visible when HW unit is configured in Target mode.

5.14.9.1.2.11. CddI2cTargetTxStartNotification

Item

Name

CddI2cTargetTxStartNotification

Description

Function pointer to callback function called when target TX start condition is detected.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.2.12. CddI2cTargetRxStartNotification

Item

Name

CddI2cTargetRxStartNotification

Description

Function pointer to callback function called when target RX start condition is detected.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.2.13. CddI2cTargetTxCompleteNotification

Item

Name

CddI2cTargetTxCompleteNotification

Description

Function pointer to callback function called when target TX is complete (stop condition or buffer fully transferred).

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.2.14. CddI2cTargetRxCompleteNotification

Item

Name

CddI2cTargetRxCompleteNotification

Description

Function pointer to callback function called when target RX is complete (stop condition or buffer full).

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.2.15. CddI2cTargetErrorNotification

Item

Name

CddI2cTargetErrorNotification

Description

Function pointer to callback function called when a target bus error occurs.

Multiplicity-Configuration-Class

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.3. CddI2cChConfig

This container contains the Channel configurations

5.14.9.1.3.1. CddI2cChDirection

Item

Name

CddI2cChDirection

Description

Selection of Channel direction.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

WRITE

Range

WRITE
READ

5.14.9.1.3.2. CddI2cChTargetAddress

Item

Name

CddI2cChTargetAddress

Description

Set target address for channel

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

1023

Min-value

0

5.14.9.1.3.3. CddI2cChTargetAddressScheme

Item

Name

CddI2cChTargetAddressScheme

Description

Specifies whether channel is 7 bit or 10 bit.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ADDRESS_7_BIT

Range

ADDRESS_7_BIT
ADDRESS_10_BIT

5.14.9.1.4. CddI2cSeqConfig

This container contains the Sequence configurations

5.14.9.1.4.1. CddI2cSeqCompleteNotify

Item

Name

CddI2cSeqCompleteNotify

Description

Function pointer to callback function sequence complete notify

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.4.2. CddI2cSeqErrorNotify

Item

Name

CddI2cSeqErrorNotify

Description

Function pointer to callback function sequence complete notify

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.14.9.1.4.3. CddI2cSeqRestartModeType

Item

Name

CddI2cSeqRestartModeType

Description

I2c transfer mode.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

RESTART_MODE_STOP

Range

RESTART_MODE_STOP
RESTART_MODE_NOSTOP

5.14.9.1.4.4. CddI2cSeqHwUnitAssignment

Item

Name

CddI2cSeqHwUnitAssignment

Description

I2c HW unit reference to use. Only HW units configured in Controller mode are allowed.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.14.9.1.4.5. CddI2cSeqChList

References to I2c channels and their order within the Sequence.

5.14.9.1.4.6. CddI2cSeqChAssignment

Item

Name

CddI2cSeqChAssignment

Description

A Sequence reference to a I2c channel.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.14.10. Examples

The example applications demonstrates use of I2C module, the list below identifies key steps performed in the example.

5.14.10.1. Cdd_I2c_Interrupt and Cdd_I2c_Poll

5.14.10.1.1. Overview

  • I2c Example (Interrupt and Polled Mode)

    • Initialize clock using Mcu_Init()

    • Initializes pins as I2C SDA and SCL using Port_Init()

    • Get I2C version using Cdd_I2c_GetVersionInfo()

    • Initialize I2c module using Cdd_I2c_Init()

    • Set up channels using Cdd_I2c_SetupEBDynamic()

    • Write data to target device

    • Receive and process data

    • De-initialize I2c module using Cdd_I2c_DeInit()

5.14.10.1.2. Setup Required to Run Example

  • Connect the hardware and power up

  • Connect the uart and set up the baudrate to check the log on serial console

  • Note: I2C examples are supported only in F29x LP board

5.14.10.1.3. How to Run Examples

  • Open CCS and import Cdd_I2c_Interrupt or Cdd_I2c_Poll Example

  • Build project and start debug project

5.14.10.1.4. Sample Log

5.14.10.1.5. Sample Log of Cdd_I2c_Interrupt

Cdd_I2c_Interrupt: Example Application - STARTS ...
 
 Cdd I2c MCAL Version Info
 -------------------------
 Vendor ID           : 44
 Module ID           : 255
 SW Major Version    : 1
 SW Minor Version    : 4
 SW Patch Version    : 0
 
PMIC (0x60) offset 0x01: 0xAE!!
PMIC (0x60) offset 0x02: 0x04!!
PMIC (0x60) offset 0x03: 0x02!!
PMIC (0x60) offset 0x04: 0x00!!
Cdd_I2c_Interrupt: Example Application - ENDS (Passed)!!!
Cdd_I2c_Interrupt: All tests have passed

5.14.10.1.6. Sample Log of Cdd_I2c_Poll

Cdd_I2c_Poll: Example Application - STARTS ...
 
 Cdd I2c MCAL Version Info
 -------------------------
 Vendor ID           : 44
 Module ID           : 255
 SW Major Version    : 1
 SW Minor Version    : 4
 SW Patch Version    : 0
 
PMIC (0x60) offset 0x01: 0xAE!!
PMIC (0x60) offset 0x02: 0x04!!
PMIC (0x60) offset 0x03: 0x02!!
PMIC (0x60) offset 0x04: 0x00!!
Cdd_I2c_Poll: Example Application - ENDS (Passed)!!!
Cdd_I2c_Poll: All tests have passed

5.14.10.2. Cdd_I2c_Target_Loopback

5.14.10.2.1. Overview

This example demonstrates the I2C Target Mode (Slave) functionality with an external loopback configuration. The example uses two I2C instances on the same device:

  • I2CA configured as Target (slave) at address 0x48

  • I2CB configured as Controller (master)

  • I2CA and I2CB are externally connected via wires

Test Flow:

  1. Controller (I2CB) writes data to Target (I2CA), target receives and verifies

  2. Controller (I2CB) reads data from Target (I2CA), controller verifies read data

5.14.10.2.2. Setup Required to Run Example

  • Install Code Composer Studio (CCS) latest version

  • Install compiler as recommended

  • Connect the hardware and power up

  • Connect the UART and set up the baudrate to check the log on serial console

  • IMPORTANT: External wiring connections required on F29H85x LaunchPad:

    • Connect I2CA_SCL (J1 Pin 9) to I2CB_SCL (J5 Pin 49) using a jumper wire

    • Connect I2CA_SDA (J1 Pin 10) to I2CB_SDA (J5 Pin 50) using a jumper wire

Note

This example requires external wiring between I2CA and I2CB on the LaunchPad board. Without these connections, the example will not function properly.

5.14.10.2.3. How to Run Example

  • Open CCS and import Cdd_I2c_Target_Loopback Example from the examples directory

  • Ensure external wiring connections are in place as described above

  • Build project and start debug

  • Run the application

  • Observe the UART console output for test results

5.14.10.2.4. Sample Log

Cdd_I2c_Target_Loopback: Example Application - STARTS ...

 Cdd I2c MCAL Version Info
 -------------------------
 Vendor ID           : 44
 Module ID           : 255
 SW Major Version    : 1
 SW Minor Version    : 2
 SW Patch Version    : 0

Controller WR -> Target RX:
  [0] WR: 0x00  RX: 0x00
  [1] WR: 0x01  RX: 0x01
  [2] WR: 0x02  RX: 0x02
  [3] WR: 0x03  RX: 0x03
  [4] WR: 0x04  RX: 0x04
  [5] WR: 0x05  RX: 0x05
  [6] WR: 0x06  RX: 0x06
  [7] WR: 0x07  RX: 0x07
Target TX -> Controller RD:
  [0] TX: 0x10  RD: 0x10
  [1] TX: 0x11  RD: 0x11
  [2] TX: 0x12  RD: 0x12
  [3] TX: 0x13  RD: 0x13
  [4] TX: 0x14  RD: 0x14
  [5] TX: 0x15  RD: 0x15
  [6] TX: 0x16  RD: 0x16
  [7] TX: 0x17  RD: 0x17
Cdd_I2c_Target_Loopback: Example Application - ENDS (Passed)!!!
Cdd_I2c_Target_Loopback: All tests have passed

5.14.10.2.5. Expected Results

When the example runs successfully:

  1. Version information is displayed showing I2C MCAL driver version

  2. Controller write test: 8 bytes written by controller match the 8 bytes received by target

  3. Controller read test: 8 bytes read by controller match the 8 bytes transmitted by target

  4. Final message shows “ENDS (Passed)!!!” and “All tests have passed”

If the example fails, check:

  • External wiring connections are correct

  • Both I2CA and I2CB pins are properly configured in Port driver

  • Target address 0x48 matches in both controller channel configuration and target HW unit configuration