6.15. CDD I2C Module Migration

Migration Approach: Follow sequential migration for clear understanding of changes at each version. Each migration is organized by individual changes with description, old vs new comparison, and migration actions.

6.15.1. v01.03.00 (i.e release v26.00.00) from v01.01.00 (i.e release v01.04.01) Migration

6.15.1.1. Summary

Version v01.03.00 introduces I2C target (slave) mode support and restructures the interrupt/polling configuration from a global setting to per-HW-unit control:

  1. Per-HW-Unit Interrupt Configuration: The global CddI2cUseInterrupts flag is replaced by a per-HW-unit CddI2cHwUseInterrupts parameter, allowing each I2C instance to be independently configured for polling or interrupt mode.

  2. Cdd_I2c_PollingModeProcessing() Removed: Polling is now integrated into Cdd_I2c_MainFunction(); the standalone polling processing API is removed.


6.15.1.2. Change 1: Per-HW-Unit Interrupt/Polling Configuration

6.15.1.2.1. Description

Previously, interrupt or polling mode was selected globally for all I2C HW units through a single CddI2cUseInterrupts boolean in the CddI2cGeneral container. In v01.02.00, this global flag is removed. Each HW unit now has its own CddI2cHwUseInterrupts parameter inside its CddI2cHwConfig entry.

Additionally, the generated macros are updated: two separate macros (CDD_I2C_POLLING_MODE and CDD_I2C_INTERRUPT_MODE) are now generated based on whether any HW unit is in polling or interrupt mode respectively.

6.15.1.2.2. Old vs New Configuration

Parameter

v01.01.00

v01.02.00

Location

CddI2cGeneral/CddI2cUseInterrupts (global)

CddI2cHwConfig/<unit>/CddI2cHwUseInterrupts (per HW unit)

Scope

All HW units share one setting

Each HW unit configured independently

Generated Macro Changes:

Macro

v01.01.00

v01.02.00

CDD_I2C_POLLING_MODE

STD_ON if CddI2cUseInterrupts = false

STD_ON if any HW unit has CddI2cHwUseInterrupts = false

CDD_I2C_INTERRUPT_MODE

Not generated

STD_ON if any HW unit has interrupts or Target mode enabled

CDD_I2C_CONTROLLER_ACTIVE

Not generated

STD_ON if any HW unit is in controller mode

CDD_I2C_TARGET_ACTIVE

Not generated

STD_ON if any HW unit is in target mode

6.15.1.2.3. Migration Actions

  1. Open your I2C configuration in EB Tresos.

  2. Navigate to CddI2cGeneral and note the current value of CddI2cUseInterrupts (true = interrupt mode, false = polling mode).

  3. Remove CddI2cUseInterrupts — this parameter no longer exists.

  4. Navigate to each CddI2cHwConfig entry for your configured HW units.

  5. Set CddI2cHwUseInterrupts on each HW unit to match your previous global setting:

    • If old CddI2cUseInterrupts = true → set CddI2cHwUseInterrupts = true on each unit

    • If old CddI2cUseInterrupts = false → leave CddI2cHwUseInterrupts = false (default) on each unit

  6. Update application code: Replace any #if (STD_ON == CDD_I2C_POLLING_MODE) guards with the new equivalent. Logic is the same but note that CDD_I2C_INTERRUPT_MODE is now also available.

  7. Regenerate configuration.

CddI2cGeneral old global interrupt setting

Fig. 6.62 v01.01.00: CddI2cGeneral showing global CddI2cUseInterrupts parameter

CddI2cHwConfig new per-unit interrupt setting

Fig. 6.63 v01.02.00: CddI2cHwConfig showing per-unit CddI2cHwUseInterrupts parameter


6.15.1.3. Change 2: Cdd_I2c_PollingModeProcessing() Removed

6.15.1.3.1. Description

The Cdd_I2c_PollingModeProcessing() API has been removed. In v01.01.00, this function was used to process pending I2C transfers when interrupts were disabled. In v01.02.00, polling processing is handled internally by Cdd_I2c_MainFunction() (available when CDD_I2C_CONTROLLER_ACTIVE == STD_ON).

The service ID previously assigned to this function (CDD_I2C_SID_POLLING_MODE_PROCESSING = 0x0A) has been reassigned to Cdd_I2c_GetStatus().

6.15.1.3.2. Old vs New

v01.01.00

v01.02.00

Cdd_I2c_PollingModeProcessing() — explicit polling processing API

Removed — use Cdd_I2c_MainFunction() for controller polling

CDD_I2C_SID_POLLING_MODE_PROCESSING (0x0AU)

Removed

CDD_I2C_SID_GET_STATUS (0x0BU)

CDD_I2C_SID_GET_STATUS (0x0AU) (renumbered)

6.15.1.3.3. Migration Actions

  1. Search your application code for all calls to Cdd_I2c_PollingModeProcessing().

  2. Replace each call with Cdd_I2c_MainFunction() — this now handles both periodic timeout checking and polling-mode transfer processing for controller mode.

  3. Remove any #if (STD_ON == CDD_I2C_POLLING_MODE) guards previously wrapping Cdd_I2c_PollingModeProcessing() calls — Cdd_I2c_MainFunction() is available whenever CDD_I2C_CONTROLLER_ACTIVE == STD_ON.

  4. Verify no code references CDD_I2C_SID_POLLING_MODE_PROCESSING numerically — if so, update to the new service ID assignments.