6.17. CDD PWM Module Migration

Migration Approach: Follow sequential migration for clear understanding of changes at each version. Each migration is organized by individual changes with description, old vs new comparison, and migration actions.

6.17.1. v03.00.00 (i.e release v01.04.00) from v02.00.00 (i.e release v01.03.00) Migration

6.17.1.1. Summary

Version v03.00.00 introduces Resource Allocator as a mandatory architectural foundation, fixes PWM channel symbolic name generation, and adds HRPWM calibration instance configuration support. This represents a fundamental shift from direct parameter configuration to centralized resource management:

  1. Resource Allocator Introduction and PWM Instance Configuration Updates: Resource Allocator becomes mandatory with CDD PWM configurations updated to reference Resource Allocator instances

  2. HRPWM Configuration Support: Optional HRPWM calibration instance configuration support added

  3. Symbolic Name Uniqueness Requirements: Enhanced validation requires unique symbolic names across configurations

PREREQUISITE: Complete Resource Allocator Setup before proceeding.

6.17.1.2. Change 1: Resource Allocator Introduction and PWM Instance Configuration Updates

6.17.1.2.1. Description

Resource Allocator becomes a mandatory architectural foundation for the CDD PWM module, with CDD PWM configurations updated to reference Resource Allocator instances. This represents a fundamental shift from direct parameter configuration to centralized resource management, where CDD PWM instances are allocated through Resource Allocator and then referenced by PWM unit configurations.

6.17.1.2.2. Old vs New Configuration

Old (v02.00.00): Direct parameter selection was used without Resource Allocator dependency.

Old CDD PWM Config

Fig. 6.71 v02.00.00: Direct PWM instance parameter selection

New (v03.00.00): CDD PWM configurations now reference instances allocated through Resource Allocator.

Select CDD PWM Instance

Fig. 6.72 v03.00.00: Set CddPwmInstanceRef to point to the corresponding Cdd_PwmAllocatedInstance in Resource Allocator

6.17.1.2.3. Migration Actions

  1. Setup Resource Allocator: Follow Resource Allocator Setup

  2. Navigate to Context: Navigate to ResourceAllocatorGeneral → Context → Cdd_Pwm and add CDD PWM allocator:

Add CDD PWM Allocator

Fig. 6.73 Navigate to Context and add CDD PWM allocator

  1. Add CDD PWM Instance: Add Cdd_PwmAllocatedInstance entries for each PWM instance your application requires:

Add CDD PWM Instance

Fig. 6.74 Add Cdd_PwmAllocatedInstance entries for each PWM instance your application requires

  1. Configure PWM Instance: Configure the InstanceName, Frame, and BaseAddr for each allocated instance:

Configure CDD PWM Instance

Fig. 6.75 Configure the InstanceName, Frame, and BaseAddr for each allocated instance

  1. Complete Configuration: Finalize CDD PWM instance allocation

  2. Navigate to CddPwmUnit: Navigate to Cdd → CddPwmUnit and update configurations to reference the CDD PWM instances allocated in Resource Allocator

  3. Open PWM Unit Configuration: Access the CddPwmUnit configuration that needs to be updated

  4. Set Instance Reference: Set CddPwmInstanceRef to point to the corresponding Cdd_PwmAllocatedInstance in Resource Allocator

  5. Verify Automatic Derivation: Confirm that the CddPwmBaseAddress parameter is now automatically derived from the Resource Allocator reference

6.17.1.3. Change 2: HRPWM Configuration Support

6.17.1.3.1. Description

Version v03.00.00 adds optional HRPWM (High-Resolution PWM) calibration instance configuration support for advanced PWM applications. This feature allows configuration of HRPWM calibration instances through the Resource Allocator and referencing them in CDD PWM configuration.

6.17.1.3.2. Old vs New HRPWM Configuration

Old (v02.00.00): Limited HRPWM configuration options without calibration instance support.

New (v03.00.00): Optional HRPWM calibration instance configuration through CddPwmHrpwmCalibrationConfig container in advanced mode.

6.17.1.3.3. Migration Actions

  1. Evaluate HRPWM Requirements: Determine if your application requires HRPWM (High-Resolution PWM) features

  2. Configure HrCal in Resource Allocator: If using HRPWM features, configure HrCal allocation in Resource Allocator first:

    • Navigate to ResourceAllocatorGeneral → Context → Cdd_Pwm → CddPwmHrpwmCalInstance

    • Add CddPwmHrpwmCalInstance allocator entries for each calibration instance required

    • Configure the InstanceName and calibration parameters for each allocated CddPwmHrpwmCalInstance instance

Configure HrCal in Resource Allocator

Fig. 6.76 Configure HrCal allocation in Resource Allocator for HRPWM calibration support

  1. Enable Advanced Mode: Enable advanced mode in the CDD PWM configuration to access HRPWM features. Refer to Advanced Mode for detailed information on advanced features and APIs

  2. Configure HRPWM Calibration: Configure HRPWM calibration instances through the CddPwmHrpwmCalibrationConfig container and reference the CddPwmHrpwmCalInstance instances from Resource Allocator:

Configure HRPWM

Fig. 6.77 Configure HRPWM calibration instances and reference HrCal instances from Resource Allocator

  1. Verify Calibration Settings: Ensure proper calibration settings for high-resolution PWM operation and that HrCal instances are properly referenced

6.17.1.4. Change 3: Symbolic Name Uniqueness Requirements

6.17.1.4.1. Description

Version v03.00.00 introduces enhanced validation that requires symbolic names to be unique across configurations. When migrating from v02.00.00 to v03.00.00, EB Tresos will generate validation errors if symbolic names are not unique.

6.17.1.4.2. Old vs New Validation Requirements

Uniqueness Requirements:

Parameter

v02.00.00

v03.00.00

CddPwmOutputChannel (container name)

No uniqueness constraint

Must be unique across all HW units

CddPwmXlinkInstanceRef

No uniqueness constraint

Must be unique across all containers

CddPwmHrpwmCalInstanceRef

No uniqueness constraint

Must be unique across all containers

6.17.1.4.3. Migration Actions

  1. Review Container Names: Check all CddPwmOutputChannel container names for uniqueness across all HW units

  2. Review Instance References: Ensure CddPwmXlinkInstanceRef and CddPwmHrpwmCalInstanceRef are unique across all containers

  3. Resolve Conflicts: Update any duplicate symbolic names to ensure uniqueness and avoid validation errors during migration

  4. Validate Configuration: Run validation in EB Tresos to confirm all symbolic names are now unique

  5. Regenerate Configuration: Generate configuration files to get the corrected symbolic names in Cfg.h

Note

The Resource Allocator module must be configured before the CDD PWM module to ensure correct instance availability. For more details on Resource Allocator configuration, see the Resource Allocator Module User Guide.

6.17.2. v02.00.00 (i.e release v01.03.00) from v01.00.00 (i.e release v01.02.00) Migration

6.17.2.1. Summary

Version v02.00.00 introduces parameter name updates, new advanced features, and enhanced functionality while maintaining backward compatibility for basic PWM operations:

  1. Parameter Renaming: Existing parameters renamed for clarity and consistency as initialization/default values

  2. Advanced Mode Features: Introduction of Advanced Mode with Trip Zone protection, Xlink synchronization, and enhanced emulation support

6.17.2.2. Change 1: Parameter Renaming

6.17.2.2.1. Description

Version v02.00.00 renames existing parameters to better reflect their purpose as initialization/default values and improves naming consistency across the module. This change clarifies that these parameters represent initial configuration values written during PWM initialization.

6.17.2.2.2. Old vs New Parameter Names

Parameter Name Mapping:

v01.00.00

v02.00.00

CddPwmPeriod

CddPwmDefaultPeriod

CddPwmDutyCycle

CddPwmDefaultDutyCycle

CddPwmDutyCycleInPercentage

CddPwmDefaultDutyCycleInPercentage

CddPwmNotification

CddPwmInterruptNotification

Parameter Details:

  • CddPwmDefaultPeriod: Period value for initialization, written to TBPRD register

  • CddPwmDefaultDutyCycle: Duty cycle value for initialization

  • CddPwmDefaultDutyCycleInPercentage: Duty cycle in percentage (0-100%)

  • CddPwmInterruptNotification: PWM interrupt callback function

6.17.2.2.3. Migration Actions

  1. Update Parameter Names: Update the following parameter names in your PWM configuration:

    • Rename CddPwmPeriodCddPwmDefaultPeriod

    • Rename CddPwmDutyCycleCddPwmDefaultDutyCycle

    • Rename CddPwmDutyCycleInPercentageCddPwmDefaultDutyCycleInPercentage

    • Rename CddPwmNotificationCddPwmInterruptNotification

  2. Verify Configuration Values: Ensure all renamed parameters retain their intended configuration values

  3. Update Documentation: Update any project documentation that references the old parameter names

6.17.2.3. Change 2: Advanced Mode Features

6.17.2.3.1. Description

Version v02.00.00 introduces Advanced Mode with Trip Zone protection and Xlink synchronization features, along with enhanced emulation mode support. These features provide fault protection capabilities and PWM synchronization for advanced applications.

6.17.2.3.2. Old vs New Feature Configuration

New Parameters Added:

Parameter

v01.00.00

v02.00.00

CddPwmEmulationMode

Not available

Controls PWM behavior during debug/emulation

CddPwmAdvancedMode

Not available

Enable for Trip Zone protection and Xlink synchronization features

CddPwmTripZoneInterruptEnable

Not available

Enable trip zone interrupt for fault protection

CddPwmTripZoneInterruptCategory

Not available

Trip zone interrupt category (CAT1/CAT2)

CddPwmTripZoneNotification

Not available

Callback function for trip zone events

New Containers Added:

Container

Description

CddPwmXlinkConfig

Configure PWM cross-linking for frame synchronization

CddPwmLinkHwUnit

Link multiple PWM hardware units together

6.17.2.3.3. Migration Actions

  1. Configure Emulation Mode: Set CddPwmEmulationMode as required for your debug setup

  2. Enable Advanced Mode (Optional): If you need Trip Zone or Xlink synchronization features, enable CddPwmAdvancedMode. Refer to Advanced Mode for detailed information on Trip Zone protection, Xlink synchronization, and other advanced features

  3. Configure Trip Zone Protection (Optional): If fault protection is required, configure the Trip Zone parameters:

    • Enable CddPwmTripZoneInterruptEnable for trip zone interrupts

    • Set CddPwmTripZoneInterruptCategory (CAT1/CAT2) as appropriate

    • Configure CddPwmTripZoneNotification callback function for trip zone events

  4. Configure Xlink Synchronization (Optional): If PWM synchronization is needed, configure the Xlink containers:

    • Add and configure CddPwmXlinkConfig for cross-linking setup

    • Add and configure CddPwmLinkHwUnit to link multiple PWM hardware units

  5. Maintain Backward Compatibility: For applications not requiring Advanced Mode features, leave parameters in default configuration to ensure backward compatibility

Important

For users migrating from v1.0.0 to v2.0.0 who do not require Advanced Mode features, the default configurations ensure backward compatibility and will not affect your current working setup.