5.3. GPT
5.3.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Type for GPT Predef Timers. |
|
enum |
GPT channel mode macro. |
|
enum |
GPT Simulation enabled/disabled. |
|
enum |
GPT Simulation Behaviour Hard/Soft stop upon GPT simulation enabled. |
|
enum |
GPT Operation Mode. |
|
enum |
GPT channel notification enable/disable status. This indicates if the notification of GPT channel is enabled or disabled. |
|
enum |
GPT channel state. GPT will be in one of this state during its lifetime. |
|
typedef uint8 |
Numeric ID of a GPT channel. |
|
typedef uint32 |
Base address of a GPT channel. |
|
typedef uint32 |
Type for reading and setting the timer values(in number of ticks). |
|
typedef uint16 |
Prescale value for General purpose timer channels. |
|
typedef void(*)(void) |
Notification callback function pointer. |
5.3.1.1. enum Gpt_PredefTimerType
Enumerator |
Value |
Description |
|---|---|---|
GPT_PREDEF_TIMER_1US_16BIT |
0U |
GPT Predef Timer with tick duration 1µs and range 16bit. |
GPT_PREDEF_TIMER_1US_24BIT |
1U |
GPT Predef Timer with tick duration 1µs and range 24bit. |
GPT_PREDEF_TIMER_1US_32BIT |
2U |
GPT Predef Timer with tick duration 1µs and range 32bit. |
GPT_PREDEF_TIMER_100US_32BIT |
3U |
GPT Predef Timer with tick duration 100µs and range 32bit. |
Brief: Type for GPT Predef Timers.
5.3.1.2. enum Gpt_ChannelModeType
Enumerator |
Value |
Description |
|---|---|---|
GPT_CH_MODE_CONTINUOUS |
Timer will continue to running with the specified time period when target time reached. |
|
GPT_CH_MODE_ONESHOT |
Timer will stop after running once when target time reached. |
Brief: GPT channel mode macro.
5.3.1.3. enum Gpt_SimStatusType
Enumerator |
Value |
Description |
|---|---|---|
GPT_SIM_DISABLE |
Timer is free-running. |
|
GPT_SIM_ENABLE |
Timer is not free-running. Gpt_SimMode decides mode of operation. |
Brief: GPT Simulation enabled/disabled.
5.3.1.4. enum Gpt_SimModeType
Enumerator |
Value |
Description |
|---|---|---|
GPT_SIM_STOP_TIMER_AT_NEXT_COUNTER_DEC |
Timer stops at next decrement (HARD STOP) |
|
GPT_SIM_STOP_TIMER_AT_NEXT_TIMER_ELAPSE |
Timer stops at the next timer elapsed (SOFT STOP) |
Brief: GPT Simulation Behaviour Hard/Soft stop upon GPT simulation enabled.
5.3.1.5. enum Gpt_ModeType
Enumerator |
Value |
Description |
|---|---|---|
GPT_MODE_NORMAL |
0x0U |
Normal Mode. |
GPT_MODE_SLEEP |
0x1U |
Sleep Mode. |
Brief: GPT Operation Mode.
5.3.1.6. enum Gpt_NotificationStateType
Enumerator |
Value |
Description |
|---|---|---|
GPT_NOTIF_ENABLED |
GPT notification is enabled. |
|
GPT_NOTIF_DISABLED |
GPT notification is disabled. |
Brief: GPT channel notification enable/disable status. This indicates if the notification of GPT channel is enabled or disabled.
5.3.1.7. enum Gpt_ChannelStateType
Enumerator |
Value |
Description |
|---|---|---|
GPT_CH_UNINITIALIZED |
GPT channel is uninitialized. |
|
GPT_CH_INITIALIZED |
GPT channel is initialized. |
|
GPT_CH_RUNNING |
GPT channel is running. |
|
GPT_CH_STOPPED |
GPT channel is stopped. |
|
GPT_CH_EXPIRED |
GPT channel is expired. |
Brief: GPT channel state. GPT will be in one of this state during its lifetime.
5.3.2. Structures
Name |
Brief |
|---|---|
Configuration per channel. |
|
global configuration of the driver. |
|
GPT driver object structure. |
5.3.3. Defines
Name |
Brief |
|---|---|
GPT_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
GPT_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
GPT_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
GPT_AR_RELEASE_MAJOR_VERSION |
AUTOSAR major version specification implemented by GPT Driver. |
GPT_AR_RELEASE_MINOR_VERSION |
AUTOSAR minor version specification implemented by GPT Driver. |
GPT_AR_RELEASE_PATCH_VERSION |
AUTOSAR patch version specification implemented by GPT Driver. |
GPT_VENDOR_ID |
Texas Instruments Vendor ID. |
GPT_MODULE_ID |
GPT Driver Module ID. |
GPT_E_UNINIT |
API service called without module initialization. |
GPT_E_BUSY |
API service called when timer channel is still busy (running). |
GPT_E_MODE |
API service called when driver is in wrong mode. |
GPT_E_ALREADY_INITIALIZED |
API service for initialization called when already initialized. |
GPT_E_INIT_FAILED |
API error return code: Init function failed. |
GPT_E_PARAM_CHANNEL |
API parameter checking: invalid channel. |
GPT_E_PARAM_VALUE |
API parameter checking: invalid value. |
GPT_E_PARAM_POINTER |
API parameter checking: invalid pointer. |
GPT_E_PARAM_PREDEF_TIMER |
API parameter checking: invalid pointer. |
GPT_E_PARAM_MODE |
API parameter checking: invalid mode. |
GPT_SID_GET_VERSION_INFO |
Gpt_GetVersionInfo(). |
GPT_SID_INIT |
Gpt_Init(). |
GPT_SID_DEINIT |
Gpt_DeInit(). |
GPT_SID_GET_TIME_ELAPSED |
Gpt_GetTimeElapsed(). |
GPT_SID_GET_TIME_REMAINING |
Gpt_GetTimeRemaining(). |
GPT_SID_START_TIMER |
Gpt_StartTimer(). |
GPT_SID_STOP_TIMER |
Gpt_StopTimer(). |
GPT_SID_ENABLE_NOTIFY |
Gpt_EnableNotification(). |
GPT_SID_DISABLE_NOTIFY |
Gpt_DisableNotification(). |
GPT_SID_SET_MODE |
Gpt_SetMode(). |
GPT_SID_DISABLE_WAKEUP |
Gpt_DisableWakeup(). |
GPT_SID_ENABLE_WAKEUP |
Gpt_EnableWakeup(). |
GPT_SID_CHECK_WAKEUP |
Gpt_CheckWakeup(). |
GPT_SID_GET_TIME_PREDEF |
Gpt_GetPredefTimerValue(). |
GPT_MAX_32BIT_VAL |
Max. 32bit value. |
5.3.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Gpt_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr) |
Gpt_GetVersionInfo : Returns the Gpt Version Info. |
void |
Gpt_Init(const Gpt_ConfigType * ConfigPtr) |
Gpt_Init : Initializes the Gpt module. |
void |
Gpt_DeInit(void ) |
Gpt_DeInit : De-initializes the GPT module. |
Gpt_GetTimeElapsed(Gpt_ChannelType Channel) |
Gpt_GetTimeElapsed : Returns the time elapsed for a given channel. |
|
Gpt_GetTimeRemaining(Gpt_ChannelType Channel) |
Gpt_GetTimeRemaining : Returns the time remaining for a given channel. |
|
void |
Gpt_StartTimer(Gpt_ChannelType Channel, Gpt_ValueType Value) |
Gpt_StartTimer : Starts a timer channel. |
void |
Gpt_StopTimer(Gpt_ChannelType Channel) |
Gpt_StopTimer : Stops a timer channel. |
void |
Gpt_SetMode(Gpt_ModeType Mode) |
Gpt_SetMode : Sets the operation mode of the GPT. |
void |
Gpt_DisableWakeup(Gpt_ChannelType Channel) |
Gpt_DisableWakeup : Disables the wakeup interrupt of a channel (relevant in sleep mode). |
void |
Gpt_EnableWakeup(Gpt_ChannelType Channel) |
Gpt_EnableWakeup : Enables the wakeup interrupt of a channel (relevant in sleep mode). |
void |
Gpt_CheckWakeup(EcuM_WakeupSourceType WakeupSource) |
Gpt_CheckWakeup : Checks if a wakeup capable GPT channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid GPT channel wakeup event. |
void |
Gpt_SetDriverObjPtr(Gpt_DriverObjType * Set_DrvObj) |
Set the Gpt driver object into global pointer. |
void |
Gpt_DeInitPriv(const Gpt_ChannelConfigType * ChannelObj) |
Deinitializes the timer hardware to reset state. |
void |
Gpt_InitPriv(const Gpt_ChannelConfigType * ChannelObj) |
Initialize the timer instance. |
uint32 |
Gpt_GetCurCountPriv(const Gpt_ChannelConfigType * ChannelObj) |
Get the current timer count. |
uint32 |
Gpt_GetPrdCountPriv(const Gpt_ChannelConfigType * ChannelObj) |
Get the timer period count. |
void |
Gpt_StartTimerPriv(const Gpt_ChannelConfigType * ChannelObj, uint32 count) |
Start the timer. |
void |
Gpt_StopTimerPriv(const Gpt_ChannelConfigType * ChannelObj) |
Stop the timer. |
void |
Gpt_ClrOvfFlagPriv(const Gpt_ChannelConfigType * ChannelObj) |
Clear the Timer Overflow flag. |
void |
Gpt_EnableIntPriv(const Gpt_ChannelConfigType * ChannelObj) |
Enable the timer interrupt. |
void |
Gpt_DisableIntPriv(const Gpt_ChannelConfigType * ChannelObj) |
Disable the timer interrupt. |
void |
Gpt_GetChIdxPriv(const Gpt_DriverObjType * GptDrvObj, Gpt_ChannelType Channel, uint32 * ChannelIndex) |
Get the array index of a channel from configuration array/vector. |
Std_ReturnType |
Gpt_GetPredefTimerValue(Gpt_PredefTimerType PredefTimer, uint32 * TimeValuePtr) |
Gpt_GetPredefTimerValue : Delivers the current value of the desired GPT Predef Timer. |
void |
Gpt_IsrNotifyFunction(Gpt_ChannelType Channel) |
Gpt_IsrNotifyFunction: Invoked by the respective timer channel ISR. |
5.3.4.1. function Gpt_GetVersionInfo
void Gpt_GetVersionInfo(
Std_VersionInfoType * VersionInfoPtr
)
Brief: Gpt_GetVersionInfo : Returns the Gpt Version Info.
This service returns the version information of this module.
Parameters:
VersionInfoPtr
VersionInfoPtr Pointer to where to store the version information of this module.
Returns:
None
Return: None
Precondition: VersionInfoPtr should not be NULL
Postcondition: None
5.3.4.2. function Gpt_Init
void Gpt_Init(
const Gpt_ConfigType * ConfigPtr
)
Brief: Gpt_Init : Initializes the Gpt module.
This service initializes all the configured Gpt channels. This will set the state of the each channel to “Initialized”.
Parameters:
ConfigPtr
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.3. function Gpt_DeInit
void Gpt_DeInit(
void
)
Brief: Gpt_DeInit : De-initializes the GPT module.
This service deinitializes the Gpt driver to the power on reset state. The Gpt driver state is changed to “Uninitialized” state”. All the configuration registers are cleared to stop the timer channels. API will disable all interrupts.
Returns:
None
Return: None
Precondition: Gpt_Init should be called first before calling this service.
Postcondition: None
5.3.4.4. function Gpt_GetTimeElapsed
Gpt_ValueType Gpt_GetTimeElapsed(
Gpt_ChannelType Channel
)
Brief: Gpt_GetTimeElapsed : Returns the time elapsed for a given channel.
This service will return the time elapsed for the referenced channel. The user can configure the channel in two modes, One-shot and Continuous mode. In one shot mode, if the timer is in stopped state, the function will return time value at the moment of stopping. If the timer is expired, the function will return the target time configured for the channel. If the timer has not expired/stopped in one shot mode, it will return the value of time elapsed, relative to the time of starting. In Continuous Mode - The elapsed time value will be the value relative to last occurrence of start/restart, that is for current iteration only.
Parameters:
Channel Numeric identifier of the GPT channel.
Returns:
Value of the type Gpt_ValueType
Return: Returns the time already elapsed.
Precondition: Gpt Driver must be initialized.
Postcondition: None
5.3.4.5. function Gpt_GetTimeRemaining
Gpt_ValueType Gpt_GetTimeRemaining(
Gpt_ChannelType Channel
)
Brief: Gpt_GetTimeRemaining : Returns the time remaining for a given channel.
Gpt_GetTimeRemaining will return the timer value remaining until the target time will be reached next time. The remaining time is the absolute difference of the target time and time already elapsed. In one shot mode, if the timer is in stopped state, the function will return remaining time value at the moment of stopping. If the timer is expired, the function will return 0. In continuous mode, the return value will be the time remaining in the current iteration only.
Parameters:
Channel Numeric identifier of the GPT channel.
Returns:
Value of the type Gpt_ValueType
Return: Returns the time remaining until the target time is reached.
Precondition: Gpt Driver must be initialized.
Postcondition: None
5.3.4.6. function Gpt_StartTimer
void Gpt_StartTimer(
Gpt_ChannelType Channel,
Gpt_ValueType Value
)
Brief: Gpt_StartTimer : Starts a timer channel.
Gpt_StartTimer will start the selected timer channel with defined target time. If the timer channel is enabled for interrupt notification, then interrupt notification will be triggered after expiration of the selected timer channel. In one shot mode, if the timer is expired then the channel will be stopped in interrupt subroutine. The selected channel will be moved to “Running” state after calling this function.
Parameters:
Channel Numeric identifier of the GPT channel.
Value Target time in number of ticks.
Returns:
None
Return: None
Precondition: Gpt Driver must be initialized.
Postcondition: Postconditions
5.3.4.7. function Gpt_StopTimer
void Gpt_StopTimer(
Gpt_ChannelType Channel
)
Brief: Gpt_StopTimer : Stops a timer channel.
Gpt_StopTimer will stop the selected timer channel.This will clear all the registers corresponding to the selected channel. The state of the timer channel will be changed to “Stopped”.If the channel is in state “Initialized”,”Expired”,”Stopped” before calling this function,the function will be left without any action.
Parameters:
Channel Numeric identifier of the GPT channel.
Returns:
None
Return: None
Precondition: Gpt Driver must be initialized.
Postcondition: None
5.3.4.8. function Gpt_SetMode
void Gpt_SetMode(
Gpt_ModeType Mode
)
Brief: Gpt_SetMode : Sets the operation mode of the GPT.
5.3.4.9. function Gpt_DisableWakeup
void Gpt_DisableWakeup(
Gpt_ChannelType Channel
)
Brief: Gpt_DisableWakeup : Disables the wakeup interrupt of a channel (relevant in sleep mode).
5.3.4.10. function Gpt_EnableWakeup
void Gpt_EnableWakeup(
Gpt_ChannelType Channel
)
Brief: Gpt_EnableWakeup : Enables the wakeup interrupt of a channel (relevant in sleep mode).
5.3.4.11. function Gpt_CheckWakeup
void Gpt_CheckWakeup(
EcuM_WakeupSourceType WakeupSource
)
Brief: Gpt_CheckWakeup : Checks if a wakeup capable GPT channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid GPT channel wakeup event.
5.3.4.12. function Gpt_SetDriverObjPtr
void Gpt_SetDriverObjPtr(
Gpt_DriverObjType * Set_DrvObj
)
Brief: Set the Gpt driver object into global pointer.
This function Set the Gpt driver object into global pointer which can be used in ISR notification API.
Parameters:
Gpt_DrvObj Gpt_DrvObj is the Gpt driver object defined in Gpt.c
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.13. function Gpt_DeInitPriv
void Gpt_DeInitPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Deinitializes the timer hardware to reset state.
This function deintializes the timer module to its reset state. All the registers are set to their initial values by calling the static inline APIs.
Parameters:
ChannelObj ChannelObj contains the channel configuration
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.14. function Gpt_InitPriv
void Gpt_InitPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Initialize the timer instance.
This function initializes the CPU timer using the configuration parameters.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.15. function Gpt_GetCurCountPriv
uint32 Gpt_GetCurCountPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Get the current timer count.
This function queries the current (instantaneous) timer count of the TIM reg.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
Value of Type uint32
Return: This function returns the current (instantaneous) timer count.
Precondition: None
Postcondition: None
5.3.4.16. function Gpt_GetPrdCountPriv
uint32 Gpt_GetPrdCountPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Get the timer period count.
This function queries the period count from the PRD reg. that is programmed.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
Value of Type uint32
Return: Returns the period count of the PRD regsiter.
Precondition: None
Postcondition: None
5.3.4.17. function Gpt_StartTimerPriv
void Gpt_StartTimerPriv(
const Gpt_ChannelConfigType * ChannelObj,
uint32 count
)
Brief: Start the timer.
This function starts the timer with the tick count argument.
Parameters:
ChannelObj is the structure containing timer configuration.
count is timer tick count.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.18. function Gpt_StopTimerPriv
void Gpt_StopTimerPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Stop the timer.
This function stops the running timer.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.19. function Gpt_ClrOvfFlagPriv
void Gpt_ClrOvfFlagPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Clear the Timer Overflow flag.
This function clears the timer overflow flag, which is set on timer expiry
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.20. function Gpt_EnableIntPriv
void Gpt_EnableIntPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Enable the timer interrupt.
This function enables the timer interrupt.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.21. function Gpt_DisableIntPriv
void Gpt_DisableIntPriv(
const Gpt_ChannelConfigType * ChannelObj
)
Brief: Disable the timer interrupt.
This function disables the timer interrupt.
Parameters:
ChannelObj is the structure containing timer configuration.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.22. function Gpt_GetChIdxPriv
void Gpt_GetChIdxPriv(
const Gpt_DriverObjType * GptDrvObj,
Gpt_ChannelType Channel,
uint32 * ChannelIndex
)
Brief: Get the array index of a channel from configuration array/vector.
This function populates the ‘ChannelIndex’ pointer with the array index of the ‘Channel’ present in configuration array
Parameters:
GptDrvObj is a structure containing multiple timer configurations.
Channel Numeric identifier of the GPT channel.
ChannelIndex Pointer to populate the index of channel present in config
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.3.4.23. function Gpt_GetPredefTimerValue
Std_ReturnType Gpt_GetPredefTimerValue(
Gpt_PredefTimerType PredefTimer,
uint32 * TimeValuePtr
)
Brief: Gpt_GetPredefTimerValue : Delivers the current value of the desired GPT Predef Timer.
5.3.4.24. function Gpt_IsrNotifyFunction
void Gpt_IsrNotifyFunction(
Gpt_ChannelType Channel
)
Brief: Gpt_IsrNotifyFunction: Invoked by the respective timer channel ISR.
This Interrupt notification call function is called when interrupt notification is enabled for the channel in Gpt_StartTimer. Once the timer channel is expired/reached zero, interrupt is triggered which calls the Gpt_IsrNotifyFunction call back function inside the timer Isr.
Parameters:
Channel Numeric identifier of the GPT channel.
Returns:
None
Return: None
Precondition: None
Postcondition: None