4.10. CDD SENT Module
4.10.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
SENT |
Single Edge Nibble Transmission |
API |
Application Programming Interface |
BSW |
Basic Software |
ECU |
Electronic Control Unit |
DET |
Default Error Tracer |
HW |
Hardware |
SW |
Software |
I/O |
Input/Output |
MCAL |
Micro Controller Abstraction Layer |
RTE |
Runtime Environment |
CDD |
Complex Device Driver |
MTP |
Master Pulse Trigger |
GPIO |
General Purpose Input Output |
4.10.2. Introduction
SENT stands for Single Edge Nibble Transmission. The SENT protocol is unidirectional and uses single wire between two or more points to transmit signals from one or more sensors to a controller. This protocol can transmit high resolution data at a low cost to the system. The SENT module utilizes a Master Trigger Pulse Generator to control and receive data from one or more sensors, using a configurable pulse signal. The received data can be stored directly into memory or a FIFO and read by the CPU or RTDMA.
SENT driver is part of complex device drivers which receive the data from the sensors and send the RX indication, support both fast channel and slow channel.
Fig. 4.36 CDD_SENT MCAL AUTOSAR
This document details AUTOSAR BSW CDD_SENT module implementation
Supported AUTOSAR Release |
4.3.1 |
|---|---|
Supported Configuration Variants |
Pre-Compile |
Vendor ID |
CDD_SENT_VENDOR_ID (44) |
Module ID |
CDD_SENT_MODULE_ID (255) |
4.10.3. Functional Overview
F29X supports two modes of the SENT :
Standard SENT:
This supports only one sensor per the instance.
Sensors will be automatically sends the data, no triggering required from the ECU/coordinator.
MTP ( Master Trigger Pulse ):
This supports up to 4 sensors + broadcast.
Sensors sends the data only after master triggers the corresponding pulse of the sensor.
For triggering the pulse, there are 10 comparators which can be configured to different pulse widths.
4.10.4. Hardware Features
4.10.4.1. Hardware Features supported
The SENT module includes the following features:
Based on SAE J2716 (J2716 January 2010 and J2716 April 2016)
Supports 2007 and 2010 CRC checksum calculation
Fast channel receiver
Slow channel receiver
Configurable memory depth
5 SENT channels that can each be set to be triggered by one of 63 trigger sources
Nibble sorting to minimize CPU intervention
Timeout feature in SENT channel can be re-purposed for watchdog (only usable in continuous receive mode)
Time stamp captures for received data frames
Receiver and Interrupt Features
Fig. 4.37 Cdd_Sent Block Diagram
4.10.4.2. Not supported Features
Master Trigger Pulse Generator (MTPG)
FIFO
4.10.4.3. Non compliance
None
4.10.5. Source files
📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Can
┃ ┣ 📂Cdd_Sent
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Sent.h : Contains the API declarations of the Cdd_Sent driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Cdd_Sent_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┗ 📜Cdd_Sent_Reg_Access.h : Contains the MACROs for Cdd_Sent register access.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Sent.c : Contains the implementation of the API for Cdd_Sent driver.
┃ ┃ ┃ ┣ 📜Cdd_Sent_Irq.c : Contains the implementation for Cdd_Sent interrupts handlers.
┃ ┃ ┃ ┗ 📜Cdd_Sent_Priv.c : Contains Functions that support the API for Cdd_Sent driver
┃ ┃ ┗ 📜CMakeLists.txt
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂hw_include
┃ ┣ 📂Mcal_Lib
┃ ┣ 📂Mcu
┃ ┗ 📂Port
┣ 📂examples
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json
Fig. 4.38 Cdd_Sent Header File Structure
4.10.6. Module requirements
4.10.6.1. Memory Mapping
Will be added in later release
4.10.6.2. Scheduling
None
4.10.6.3. Error handling
4.10.6.3.1. Development Error Reporting
Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.
4.10.6.4. Error codes
Type of Error |
Related Error code |
Value (Hex) |
|---|---|---|
API called with a NULL_PTR |
CDD_SENT_E_PARAM_POINTER |
0x20U |
API service invoked with invalid channel |
CDD_SENT_E_PARAM_CHANNEL |
0x21U |
API service for initialization called when already initialized |
CDD_SENT_E_ALREADY_INITIALIZED |
0x22U |
API invoked without performing module initialization |
CDD_SENT_E_UNINIT |
0x23U |
4.10.7. Used resources
4.10.7.1. Interrupt Handling
Cdd_Sent driver provides ISR. The interrupt vector lines to be used is configurable in Cdd_Sent driver. The ISR functionality is implemented in the file Cdd_Sent_Irq.c.
Cdd_Sent Instance |
Interrupt handler |
Interrupt Line |
|---|---|---|
Cdd_Sent 1 |
Cdd_Sent_1_ISR, |
Line 0 |
Cdd_Sent 2 |
Cdd_Sent_2_ISR |
Line 0 |
Cdd_Sent 3 |
Cdd_Sent_3_ISR |
Line 0 |
Cdd_Sent 4 |
Cdd_Sent_4_ISR |
Line 0 |
Cdd_Sent 5 |
Cdd_Sent_5_ISR |
Line 0 |
Cdd_Sent 6 |
Cdd_Sent_6_ISR |
Line 0 |
Note
Same Interrupt Category needs to be configured in both Cdd_Sent and OS Modules.
4.10.7.2. Instance support
CPU instances |
supported |
|---|---|
CPU 1 |
YES |
CPU 2 |
NO |
CPU 3 |
NO |
4.10.7.3. Hardware-Software Mapping
Below image shows Cdd_Sent driver Hardware-Software mapping. For more information related to HW/SW mapping, refer the F29x Reference Manual.
Fig. 4.39 Cdd_Sent HW/SW Mapping
4.10.8. Integration description
4.10.8.1. Dependent modules
This implementation depends on the DET in order to report development errors. The detection of development errors is configurable (ON / OFF), The switch CDD_SENT_CFG_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.
4.10.8.1.1. MCU
MCU Module is required to initialize all the clock to be used by different peripherals.
4.10.8.1.2. Port
The Port module configures the port pins used for the SENT driver as input. Hence, the Port driver has to be initialized prior to the use of SENT functions. Otherwise Cdd_Sent driver functions will exhibit undefined behavior.
4.10.8.1.3. OS
The Cdd_Sent driver uses interrupts and therefore there is a dependency on the OS, which configures the interrupt sources.
4.10.8.2. Multi-core and Resource allocator
Not Supported
4.10.9. Configuration
The Cdd_Sent Driver implementation supports one configuration variant Pre-Compile config. The driver expects generated Cdd_Sent_Cfg.h to be present as input file. The associated Cdd_Sent driver configuration generated source files are Cdd_Sent_Cfg.c
The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.
4.10.9.1. CddSentController
4.10.9.1.1. CddSentInstance
SWS Item |
|
|---|---|
Name |
CddSentInstance |
Parent Container |
CddSentController |
Description |
Selects CddSent HW unit Instance. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
SENT1 |
Default value |
SENT1 |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.2. CddSentBaseAddress
SWS Item |
|
|---|---|
Name |
CddSentBaseAddress |
Parent Container |
CddSentController |
Description |
Specifies the CddSent HW unit base address. |
Multiplicity |
1 |
Type |
INTEGER |
Range |
0 .. 4294967295 |
Default value |
– |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.3. CddSentHWUnitId
SWS Item |
|
|---|---|
Name |
CddSentHWUnitId |
Parent Container |
CddSentController |
Description |
This parameter provides the HW unit ID which is unique in a given CddSent Driver. The value for this parameter starts with 0 and continue without any gaps. |
Multiplicity |
1 |
Type |
INTEGER (Symbolic Name generated for this parameter) |
Range |
0 .. 5 |
Default value |
– |
Post-Build Variant Value |
true |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: ECU |
4.10.9.1.4. CddSentClockTick
SWS Item |
|
|---|---|
Name |
CddSentClockTick |
Parent Container |
CddSentController |
Description |
This parameter is for setting the clock tick for the CddSent in Use. |
Multiplicity |
1 |
Type |
INTEGER |
Range |
0 .. 600 |
Default value |
– |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: ECU |
4.10.9.1.5. CddSentInterruptType
SWS Item |
|
|---|---|
Name |
CddSentInteruptType |
Parent Container |
CddSentController |
Description |
Defines the interrupt type. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
CDD_SENT_ISR_CAT1_RTINT |
Default value |
CDD_SENT_ISR_CAT2 |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.6. CddSentCRCType
SWS Item |
|
|---|---|
Name |
CddSentCRCType |
Parent Container |
CddSentController |
Description |
CddSent CRC type selection. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
CDD_SENT_CRC_LEGACY_2007 |
Default value |
CDD_SENT_CRC_RECOMENDED_2010 |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.7. CddSentCRCWidth
SWS Item |
|
|---|---|
Name |
CddSentCRCWidth |
Parent Container |
CddSentController |
Description |
CddSent CRC Width selection. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
CDD_SENT_CRC_4_BIT |
Default value |
CDD_SENT_CRC_4_BIT |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.8. CddSentCRCWithStatus
SWS Item |
|
|---|---|
Name |
CddSentCRCWithStatus |
Parent Container |
CddSentController |
Description |
Enable/Disable CRC with status. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
CDD_SENT_CRC_WITH_STATUS |
Default value |
CDD_SENT_CRC_WITH_STATUS |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.9. CddSentDataNibblesCount
SWS Item |
|
|---|---|
Name |
CddSentDataNibblesCount |
Parent Container |
CddSentController |
Description |
Number of data nibbles expected. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
CDD_SENT_1_DATA_NIBBLES |
Default value |
CDD_SENT_6_DATA_NIBBLES |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.10. CddSentPausePulse
SWS Item |
|
|---|---|
Name |
CddSentPausePulse |
Parent Container |
CddSentController |
Description |
Enable/Disable Pause pulse. |
Multiplicity |
1 |
Type |
BOOLEAN |
Default value |
true |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.11. CddSentEnableTimeStamp
SWS Item |
|
|---|---|
Name |
CddSentEnableTimeStamp |
Parent Container |
CddSentController |
Description |
Enable/disable Time stamping. |
Multiplicity |
1 |
Type |
BOOLEAN |
Default value |
false |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.12. CddSentSyncTimeout
SWS Item |
|
|---|---|
Name |
CddSentSyncTimeout |
Parent Container |
CddSentController |
Description |
This parameter is for setting Timeout for receiving the synchronization pulse. |
Multiplicity |
1 |
Type |
INTEGER |
Range |
0 .. 255 |
Default value |
0 |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: ECU |
4.10.9.1.13. CddSentAcceptErrorData
SWS Item |
|
|---|---|
Name |
CddSentAcceptErrorData |
Parent Container |
CddSentController |
Description |
Accept error data or not. |
Multiplicity |
1 |
Type |
BOOLEAN |
Default value |
false |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.1.14. CddSentCpuClockRef
SWS Item |
|
|---|---|
Name |
CddSentCpuClockRef |
Parent Container |
CddSentController |
Description |
Reference to the CPU clock configuration, which is set in the MCU driver configuration. |
Multiplicity |
1 |
Type |
REFERENCE |
Default value |
– |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.2. CddSentChannelObject
4.10.9.2.1. CddSentChannelType
SWS Item |
|
|---|---|
Name |
CddSentChannelType |
Parent Container |
CddSentChannelObject |
Description |
Selection of channel types. |
Multiplicity |
1 |
Type |
ENUMERATION |
Range |
FAST_CHANNEL |
Default value |
FAST_CHANNEL |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.3. CddSentGeneral
4.10.9.3.1. CddSentDevErrorDetect
SWS Item |
|
|---|---|
Name |
CddSentDevErrorDetect |
Parent Container |
CddSentGeneral |
Description |
Switches the development error detection and notification on or off. |
Multiplicity |
1 |
Type |
BOOLEAN |
Default value |
false |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.3.2. CddSentVersionInfoApi
SWS Item |
|
|---|---|
Name |
CddSentVersionInfoApi |
Parent Container |
CddSentGeneral |
Description |
Adds / removes the service CddSent_ GetVersionInfo() from the code. |
Multiplicity |
1 |
Type |
BOOLEAN |
Default value |
false |
Post-Build Variant Value |
false |
Value Configuration Class |
|
Pre-compile time |
All Variants |
Link time |
– |
Post-build time |
– |
Scope / Dependency |
scope: local |
4.10.9.4. Steps To Configure Cdd_Sent Module
Open EB Tresos configurator tool, load Cdd_Sent module. Select the Precompile Config Variant.
Configure the required parameters.
Save the configuration and generate the configuration.
4.10.10. Examples
The example application demonstrates use of Cdd_Sent module, the list below identifies key steps performed in the example.
4.10.10.1. Cdd_Sent_standard
4.10.10.1.1. Overview Of Cdd_Sent_standard
Cdd_Sent_standard
EcuM_Init()
Initializes clock to 200 MHz using Mcu_Init()
Initializes pins as GPIO Outputs and GPIO Inputs using Port_Init()
Initializes Cdd_Sent driver using Cdd_Sent_Init()
Verification of Cdd_Sent standard mode feature functionality
4.10.10.1.2. Setup required to run Cdd_Sent_standard
Install Code Composer Studio(CCS) latest version
Install latest C29 compiler
Connect the hardware, sensors and power up
Connect the uart set up to check the log on serial console
Below image shows the hardware connections that needs to be done to run the example.
Fig. 4.40 Cdd_Sent HW Setup
4.10.10.1.3. How to run Cdd_Sent_standard
Open CCS and import Cdd_Sent_standard Example
Build project and start debug project
4.10.10.1.4. Sample Log of Cdd_Sent_standard
Cdd_Sent Driver Sample Application - Starts!!!
Cdd_Sent MCAL Version Info
---------------------
Vendor ID : 44
Module ID : 255
SW Major Version : 1
SW Minor Version : 0
SW Patch Version : 0
Timestamp received from Fast channel : 21589807
Data received from Fast channel : 3427036
Timestamp received from Fast channel : 21602800
Data received from Fast channel : 3427196
Timestamp received from Fast channel : 21615830
Data received from Fast channel : 3423260
Timestamp received from Fast channel : 21628961
Data received from Fast channel : 3427516
Timestamp received from Fast channel : 21642046
Data received from Fast channel : 3423580
Cdd_Sent_Standard: Sample Application - Completes successfully !!!
4.10.10.2. File Structure
📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┣ 📂examples
┃ ┣ 📂AppUtils
┃ ┣ 📂Can
┃ ┣ 📂Cdd_Sent
┃ ┃ ┗ 📂Cdd_Sent_standard
┃ ┃ ┃ ┣ 📂CCS
┃ ┃ ┃ ┃ ┗ 📜Cdd_Sent_Standard.projectspec
┃ ┃ ┃ ┣ 📂Cdd_Sent_Standard_Config
┃ ┃ ┃ ┃ ┣ 📂config
┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Sent.xdm : Generated EB Tresos config file in .xdm format
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Os.xdm
┃ ┃ ┃ ┃ ┃ ┗ 📜Port.xdm
┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Sent_Cfg.h : Contains the generated pre-compiler configuration header.*
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.h
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_Cfg.h
┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Sent_Cfg.c : Contains the Pre-compile build configuration parameters.
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_PBcfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.c
┃ ┃ ┃ ┃ ┃ ┗ 📜Port_PBcfg.c
┃ ┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜Cdd_Sent_Standard.c : Example application for Cdd_Sent.
┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┣ 📂DeviceSupport
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json