The F29 SDK differs from C2000Ware in that it is device-specific , with separate installers for each F29 device family (e.g., F29H85x-SDK, F29P58x-SDK). Below is a comparison of the components available in C2000Ware versus the F29 SDK, highlighting the key differences:
| Component | C2000Ware | F29_SDK | Comments |
|---|---|---|---|
| Driverlib | Y | Y | For more details on F28-F29 Driverlib compatibility, refer to Driverlib Migration Guide. |
| Bitfields headers | Y | Y | Bitfields definitions available for all peripherals. Compatible with F28 for reused IPs. |
| Bitfields common code and examples | Y | N | Bitfields based init code (common functions) are not available in F29. Driverlib function may be used instead. Driverlib + Bitfields examples are available. |
| Bootrom source files and binaries | Y | N | Bootrom status and tables are available in global struct instances in F29 driverlib (bootrom.h). The full bootrom source code and binaries are not released. |
| DCL | Y | Y | Part of RTLibs, compatible with F28. Application code using #include "DCL.h" or #include "DCLF32.h" should update to #include "dcl.h". For backward compatibility, dcl.h includes dcl_c28_compatibility.h with F28-F29 API mapping. For more details, refer to RTLib Migration Guide. |
| DSP (FPU) | Y | Y | Part of RTLibs, generally compatible with F28. For more details, refer to RTLib Migration Guide. |
| DSP(Fixed Point) | Y | N | Not currently supported in F29. Recommended to use FPU library for better performance. |
| VCU/VCRC Lib | Y | NA | CRC compute functions available as part of RTLibs/FastMath. Compatible with F28. For more details, refer to RTLib Migration Guide. |
| IQMath | Y | Y | Part of RTLibs, compatible with F28. For more details, refer to RTLib Migration Guide. |
| FastRTS | Y | NA | Not applicable to F29, C29 contains TMU. RTlibs/FastMath with optimal implementations of some RTS functions. |
| FastIntDiv | Y | NA | Not applicable to F29, C29 contains native support for fast integer division. |
| CLAMath | Y | NA | Not applicable to F29. Equivalent mapping functions currently not supported in RTLib. |
| Flash API | Y | Y | Not compatible with F28. For more details, refer to Flash API User Guide |
| SFO | Y | Y | Compatible with F28. |
| SDL | Y | Y | Not compatible with F28. Details will be added later. |
| Ethercat Stack | Y | Y | Compatible with F28. |
| FreeRTOS | Y | Y | Application layer is compatible with F28. Port layer updated for C29 CPU. |
| Sysconfig - Peripheral Config | Y | Y | Configuration is compatible for reused IPs. |
| Sysconfig - Clocktree | Y | Y | F29 devices does not have LSPCLK. All other configurations are compatible with F28. |
| Sysconfig - Linker cmd tool | Y | N | Replaced with Memory Configuration tool which is used to allocate memories across cores and generate linker cmd file. |
| Sysconfig - FreeRTOS config | Y | Y | Compatible with F28. User should take care of updating the stack sizes as needed. |
| Sysconfig - Board view | Y | N | Currently not supported. This will be added in future SDK release. |
| Sysconfig - Libraries | Y | N | Currently not supported. This will be added in future SDK release. |
| Board Schematics | Y | N | Board schematics and other docs available in the product page. Eg: F29H85x-SOM |