The ERAD IP in the F29 devices is an enhanced version of the IP present in F28 devices. Some of the key differences include :
Base address macros available in F28 devices :
In F29 devices, a single macro ERAD_BASE is provided. All the driverlib functions which expects the submodule base address as parameter has been updated to take in an enum as parameter instead. Refer to the Driverlib API mapping table for more details.
| F28 Macro/Enum | F28 Macro/Enum |
|---|---|
| ERAD_INST_BUSCOMP1-8 | ERAD_INST_BUSCOMP0-7 |
| ERAD_INST_COUNTER1-4 | ERAD_INST_COUNTER0-3 |
| ERAD_INST_CRC1-8 | - |
| ERAD_BUSCOMP_BUS_VPC | ERAD_BUSCOMP_BUS_VPC_I_ALIGNED / VPC_W_ALIGNED |
| ERAD_BUSCOMP_BUS_DRAB | ERAD_BUSCOMP_BUS_DRAB_W |
| ERAD_EVENT_HWBP1-8 | ERAD_EVENT_EBC0-7 |
| ERAD_EVENT_COUNTER1_EVENT-COUNTER4_EVENT | ERAD_EVENT_COUNTER0_EVENT-COUNTER3_EVENT |
| ERAD_EVENT_PIE_INT1-12 | ERAD_EVENT_PIPE_INT/RTINT/NMI |
| ERAD_EVENT_TIMER0_TINT0-ERAD_EVENT_TIMER2_TINT2 | ERAD_EVENT_CPU1/2/3_TIMER0/1/2_INT |
| ERAD_EVENT_DMACH1INT-ERAD_EVENT_DMACH6INT | ERAD_EVENT_RTDMA1/2_CH1INT-ERAD_EVENT_RTDMA1/2_CH10INT |
| ERAD_EVENT_INPUTXBAR0-15 | ERAD_EVENT_INPUTXBAR1-32 |
| ERAD_AND_MASK1-4 | ERAD_AND_MASK0-3 |
| ERAD_OR_MASK1-4 | ERAD_OR_MASK0-3 |
| ERAD_CRC_QUAL_xx | - |
| ERAD_PCTRACE_WINDOWED_QUAL_HWBP1..8 | ERAD_PCTRACE_WINDOWED_QUAL_EBC0..7 |
| ERAD_PCTRACE_WINDOWED_QUAL_HWBP_OR1..4 | ERAD_PCTRACE_WINDOWED_QUAL_OR_MASK0..3 |
| ERAD_PCTRACE_WINDOWED_QUAL_HWBP_AND1..4 | ERAD_PCTRACE_WINDOWED_QUAL_AND_MASK..3 |
| F28 Function | F29 Function | Comments |
|---|---|---|
| ERAD_setOwnership | ERAD_setOwnership | Compatible. Configures ownership for all submodules to specified owner. Separate functions available for configuring individual ownerships. |
| ERAD_getOwnership | - | Not available. Separate functions available for each submodule |
| ERAD_resetCounter | - | Not available |
| ERAD_getHaltStatus | - | Not available |
| ERAD_getBusCompStatus | ERAD_getBusCompStatus | Parameter is an enum instead of base address |
| ERAD_clearBusCompEvent | ERAD_clearBusCompEvent | Parameter is an enum instead of base address |
| ERAD_getCounterStatus | ERAD_getCounterStatus | Parameter is an enum instead of base address |
| ERAD_configBusComp | ERAD_configBusComp | Parameter is an enum instead of base address |
| ERAD_configCounterInCountingMode | ERAD_configCounterInCountingMode | Parameter is an enum instead of base address |
| ERAD_configCounterInStartStopMode | ERAD_configCounterInStartStopMode | Parameter is an enum instead of base address |
| ERAD_configCounterInCumulativeMode | ERAD_configCounterInCumulativeMode | Parameter is an enum instead of base address |
| ERAD_configMask | ERAD_configMask | Additional parameter to configure nmi |
| ERAD_enableCounterResetInput | ERAD_enableCounterResetInput | Parameter is an enum instead of base address |
| ERAD_disableCounterResetInput | ERAD_disableCounterResetInput | Parameter is an enum instead of base address |
| ERAD_clearCounterEvent | ERAD_clearCounterEvent | Parameter is an enum instead of base address |
| ERAD_clearCounterOverflow | ERAD_clearCounterOverflow | Parameter is an enum instead of base address |
| ERAD_getCurrentCount | ERAD_getCurrentCount | Parameter is an enum instead of base address |
| ERAD_setCurrentCount | ERAD_setCurrentCount | Parameter is an enum instead of base address |
| ERAD_getMaxCount | ERAD_getMaxCount | Parameter is an enum instead of base address |
| ERAD_setMaxCount | ERAD_setMaxCount | Parameter is an enum instead of base address |
| ERAD_setCounterInputConditioning | ERAD_setCounterInputConditioning | Parameter is an enum instead of base address |
C29 ERAD module does not support the CRC feature. Hence all the crc related functions are not available.
New functions added in F29 ERAD driverlb :