DCSM Module¶
The DCSM driver accesses the DCSM COMMON registers. In order to configure the Dual Code Security Module, the user must program the Linkpointer in DCSM OTP as well as the security configuration registers of the Zone Select Blocks in DCSM OTP. The DCSM driver provides functions which secure and unsecure each zone and return the ownership, security status, EXEONLY status of specific RAM modules or Flash sectors. Included are two functions which can claim and release the Flash pump to operate on a specific zone.
-
group
dcsm_api Defines
-
DCSM_O_Z1_CSMPSWD00x08U¶ Z1 CSMPSWD0 offset.
-
DCSM_O_Z1_CSMPSWD10x0AU¶ Z1 CSMPSWD1 offset.
-
DCSM_O_Z1_CSMPSWD20x0CU¶ Z1 CSMPSWD2 offset.
-
DCSM_O_Z1_CSMPSWD30x0EU¶ Z1 CSMPSWD3 offset.
-
DCSM_O_Z2_CSMPSWD00x08U¶ Z2 CSMPSWD0 offset.
-
DCSM_O_Z2_CSMPSWD10x0AU¶ Z2 CSMPSWD1 offset.
-
DCSM_O_Z2_CSMPSWD20x0CU¶ Z2 CSMPSWD2 offset.
-
DCSM_O_Z2_CSMPSWD30x0EU¶ Z2 CSMPSWD3 offset.
-
FLSEM_KEY0xA5U¶ Zone semaphore key.
-
DCSM_ALLZERO0x08U¶ CSM Passwords all zeros.
-
DCSM_ALLONE0x10U¶ CSM Passwords all ones.
-
DCSM_UNSECURE0x20U¶ Zone is secure/unsecure.
-
DCSM_ARMED0x40U¶ CSM is armed.
Enums
-
enum
DCSM_MemoryStatus¶ Values to distinguish the status of RAM or FLASH sectors. These values describe which zone the memory location belongs too. These values can be returned from DCSM_getRAMZone(), DCSM_getFlashSectorZone().
Values:
-
enumerator
DCSM_MEMORY_INACCESSIBLE¶ Inaccessible.
-
enumerator
DCSM_MEMORY_ZONE1¶ Zone 1.
-
enumerator
DCSM_MEMORY_ZONE2¶ Zone 2.
-
enumerator
DCSM_MEMORY_FULL_ACCESS¶ Full access.
-
enumerator
-
enum
DCSM_SemaphoreZone¶ Values to pass to DCSM_claimZoneSemaphore(). These values are used to describe the zone that can write to Flash Wrapper registers.
Values:
-
enumerator
DCSM_FLSEM_ZONE1= 0x01U¶ Flash semaphore Zone 1.
-
enumerator
DCSM_FLSEM_ZONE2= 0x02U¶ Flash semaphore Zone 2.
-
enumerator
-
enum
DCSM_SecurityStatus¶ Values to distinguish the security status of the zones. These values can be returned from DCSM_getZone1CSMSecurityStatus(), DCSM_getZone2CSMSecurityStatus().
Values:
-
enumerator
DCSM_STATUS_SECURE¶ Secure.
-
enumerator
DCSM_STATUS_UNSECURE¶ Unsecure.
-
enumerator
DCSM_STATUS_LOCKED¶ Locked.
-
enumerator
-
enum
DCSM_EXEOnlyStatus¶ Values to decribe the EXEONLY Status. These values are returned from to DCSM_getZone1RAMEXEStatus(), DCSM_getZone2RAMEXEStatus(), DCSM_getZone1FlashEXEStatus(), DCSM_getZone2FlashEXEStatus().
Values:
-
enumerator
DCSM_PROTECTED¶ Protected.
-
enumerator
DCSM_UNPROTECTED¶ Unprotected.
-
enumerator
DCSM_INCORRECT_ZONE¶ Incorrect Zone.
-
enumerator
-
enum
DCSM_RAMModule¶ Values to distinguish RAM Module. These values can be passed to DCSM_getZone1RAMEXEStatus() DCSM_getZone2RAMEXEStatus(), DCSM_getRAMZone().
Values:
-
enumerator
DCSM_RAMLS0¶ RAMLS0.
-
enumerator
DCSM_RAMLS1¶ RAMLS1.
-
enumerator
DCSM_RAMLS2¶ RAMLS2.
-
enumerator
DCSM_RAMLS3¶ RAMLS3.
-
enumerator
DCSM_RAMLS4¶ RAMLS4.
-
enumerator
DCSM_RAMLS5¶ RAMLS5.
-
enumerator
DCSM_RAMD0¶ RAMD0.
-
enumerator
DCSM_RAMD1¶ RAMD1.
-
enumerator
DCSM_CLA= 14U¶ Offset of CLA field in in RAMSTAT divided by two.
-
enumerator
-
enum
DCSM_Sector¶ Values to distinguish Flash Sector. These values can be passed to DCSM_getZone1FlashEXEStatus() DCSM_getZone2FlashEXEStatus(), DCSM_getFlashSectorZone().
Values:
-
enumerator
DCSM_SECTOR_A¶ Sector A.
-
enumerator
DCSM_SECTOR_B¶ Sector B.
-
enumerator
DCSM_SECTOR_C¶ Sector C.
-
enumerator
DCSM_SECTOR_D¶ Sector D.
-
enumerator
DCSM_SECTOR_E¶ Sector E.
-
enumerator
DCSM_SECTOR_F¶ Sector F.
-
enumerator
DCSM_SECTOR_G¶ Sector G.
-
enumerator
DCSM_SECTOR_H¶ Sector H.
-
enumerator
DCSM_SECTOR_I¶ Sector I.
-
enumerator
DCSM_SECTOR_J¶ Sector J.
-
enumerator
DCSM_SECTOR_K¶ Sector K.
-
enumerator
DCSM_SECTOR_L¶ Sector L.
-
enumerator
DCSM_SECTOR_M¶ Sector M.
-
enumerator
DCSM_SECTOR_N¶ Sector N.
-
enumerator
Functions
-
void
DCSM_secureZone1(void)¶ Secures zone 1 by setting the FORCESEC bit of Z1_CR register
This function resets the state of the zone. If the zone is unlocked, it will lock(secure) the zone and also reset all the bits in the Control Register.
- Return
None.
-
void
DCSM_secureZone2(void)¶ Secures zone 2 by setting the FORCESEC bit of Z2_CR register
This function resets the state of the zone. If the zone is unlocked, it will lock(secure) the zone and also reset all the bits in the Control Register.
- Return
None.
-
DCSM_SecurityStatus
DCSM_getZone1CSMSecurityStatus(void)¶ Returns the CSM security status of zone 1
This function returns the security status of zone 1 CSM
- Return
Returns security status as an enumerated type DCSM_SecurityStatus.
-
DCSM_SecurityStatus
DCSM_getZone2CSMSecurityStatus(void)¶ Returns the CSM security status of zone 2
This function returns the security status of zone 2 CSM
- Return
Returns security status as an enumerated type DCSM_SecurityStatus.
-
uint16_t
DCSM_getZone1ControlStatus(void)¶ Returns the Control Status of zone 1
This function returns the Control Status of zone 1 CSM
- Return
Returns the contents of the Control Register which can be used with provided defines.
-
uint16_t
DCSM_getZone2ControlStatus(void)¶ Returns the Control Status of zone 2
This function returns the Control Status of zone 2 CSM
- Return
Returns the contents of the Control Register which can be used with the provided defines.
-
DCSM_MemoryStatus
DCSM_getRAMZone(DCSM_RAMModule module)¶ Returns the security zone a RAM section belongs to
This function returns the security zone a RAM section belongs to.
- Parameters
module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :DCSM_RAMLS0
DCSM_RAMLS1
DCSM_RAMLS2
DCSM_RAMLS3
DCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMD0
DCSM_RAMD1
- Return
Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible, DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure).
-
DCSM_MemoryStatus
DCSM_getFlashSectorZone(DCSM_Sector sector)¶ Returns the security zone a flash sector belongs to
This function returns the security zone a flash sector belongs to.
- Parameters
sector: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible , DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure)..
-
uint32_t
DCSM_getZone1LinkPointerError(void)¶ Read Zone 1 Link Pointer Error
A non-zero value indicates an error on the bit position that is set to 1.
- Return
Returns the value of the Zone 1 Link Pointer error.
-
uint32_t
DCSM_getZone2LinkPointerError(void)¶ Read Zone 2 Link Pointer Error
A non-zero value indicates an error on the bit position that is set to 1.
- Return
Returns the value of the Zone 2 Link Pointer error.
-
void
DCSM_unlockZone1CSM(const DCSM_CSMPasswordKey *const psCMDKey)¶ Unlocks Zone 1 CSM.
This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers
- Parameters
psCMDKey: is a pointer to the DCSM_CSMPasswordKey struct that has the CSM password for zone 1.
- Return
None.
- Note
This function should not be called in an actual application, should only be used for once to program the OTP memory. Ensure flash data cache is disabled before calling this function(Flash_disableCache).
-
void
DCSM_unlockZone2CSM(const DCSM_CSMPasswordKey *const psCMDKey)¶ Unlocks Zone 2 CSM.
This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers
- Parameters
psCMDKey: is a pointer to the CSMPSWDKEY that has the CSM password for zone 2.
- Return
None.
- Note
This function should not be called in an actual application, should only be used for once to program the OTP memory. Ensure flash data cache is disabled before calling this function(Flash_disableCache).
-
DCSM_EXEOnlyStatus
DCSM_getZone1FlashEXEStatus(DCSM_Sector sector)¶ Returns the EXE-ONLY status of zone 1 for a flash sector
This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.
- Parameters
sector: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone1RAMEXEStatus(DCSM_RAMModule module)¶ Returns the EXE-ONLY status of zone 1 for a RAM module
This function takes in a valid module value and returns the status of EXE ONLY security protection for that module. DCSM_CLA is an invalid module value. There is no EXE-ONLY available for DCSM_CLA.
- Parameters
module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :DCSM_RAMLS0
DCSM_RAMLS1
DCSM_RAMLS2
DCSM_RAMLS3
DCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMD0
DCSM_RAMD1
- Return
Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone2FlashEXEStatus(DCSM_Sector sector)¶ Returns the EXE-ONLY status of zone 2 for a flash sector
This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.
- Parameters
sector: is the flash sector value. Use DCSM_Sector type.
- Return
Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.
-
DCSM_EXEOnlyStatus
DCSM_getZone2RAMEXEStatus(DCSM_RAMModule module)¶ Returns the EXE-ONLY status of zone 2 for a RAM module
This function takes in a valid module value and returns the status of EXE ONLY security protection for that module. DCSM_CLA is an invalid module value. There is no EXE-ONLY available for DCSM_CLA.
- Parameters
module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :DCSM_RAMLS0
DCSM_RAMLS1
DCSM_RAMLS2
DCSM_RAMLS3
DCSM_RAMLS4
DCSM_RAMLS5
DCSM_RAMD0
DCSM_RAMD1
- Return
Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.
-
bool
DCSM_claimZoneSemaphore(DCSM_SemaphoreZone zone)¶ Claims the zone semaphore which allows access to the Flash Wrapper register for that zone.
- Return
Returns true for a successful semaphore capture, false if it was unable to capture the semaphore.
- Parameters
zone: is the zone which is trying to claim the semaphore which allows access to the Flash Wrapper registers.
-
bool
DCSM_releaseZoneSemaphore(void)¶ Releases the zone semaphore.
- Return
Returns true if it was successful in releasing the zone semaphore and false if it was unsuccessful in releasing the zone semaphore.
- Note
If the calling function is not in the right zone to be able to access this register, it will return a false.
-
struct
DCSM_CSMPasswordKey¶ - #include <dcsm.h>
Data structures to hold password keys.
-
The code for this module is contained in driverlib/dcsm.c, with driverlib/dcsm.h containing the API declarations for use by applications.