|
|
|
This is 5.04.00.00 of C2000Ware. This HTML will provide a list of the version and paths for the devices and software libraries in C2000ware directory.
| Library | Version | Location |
|---|---|---|
| HRCAP Calibration | 1.11.00.00 | /libraries/calibration/hrcap |
| IQmath | 1.69.00.00 | /libraries/math/IQmath/c28 |
| Fixed Point DSP | 1.28.00.00 | /libraries/dsp/FixedPoint/c28 |
| SGEN | 1.02.00.00 | /libraries/dsp/SGEN/c28 |
| VCU | 2.28.00.00 | /libraries/dsp/VCU/c28 |
| PMBus | 1.10.00.00 | /libraries/communications/PMBus/c28 |
| Digital Controller Library | 3.05.00.00 | /libraries/control/DCL/c28 |
| Feature Extract Library | 1.00.00.00 | /libraries/ai/feature_extract/c28 |
| Target Host Communictation Protocol Library | 1.00.00.00 | /libraries/ai/target_host_comm_protocol/c28 |
| FPU | 2.11.00.00 | /libraries/dsp/FPU/c28 |
| FPU Fast RTS | 2.09.00.00 | /libraries/math/FPUfastRTS/c28 |
| LWIP | 2.1.2 | /libraries/communications/Ethernet/third_party/lwip |
| PTPD | 2.2.1 | /libraries/communications/Ethernet/third_party/ptpd |
| CLAmath | 4.05.00.00 | /libraries/math/CLAmath/c28 |
| FASTINTDIV | 1.06.00.00 | /libraries/math/FASTINTDIV/c28 |
| SFO Library | 8.00.00.00 | /libraries/calibration/hrpwm/ |
| F28p65x USB Library | 5.04.00.00 | /libraries/communications/usb/f28p65x |
| F28p55x USB Library | 5.04.00.00 | /libraries/communications/usb/f28p55x |
| F2838x USB Library | 5.04.00.00 | /libraries/communications/usb/f2838x |
| F2806x USB Library | 4.00.00.00 | /libraries/communications/usb/f2806x |
| F2807x USB Library | 5.04.00.00 | /libraries/communications/usb/f2807x |
| F2837xD USB Library | 5.04.00.00 | /libraries/communications/usb/f2837xd |
| F2837xS USB Library | 5.04.00.00 | /libraries/communications/usb/f2837xs |
| F28002x Flash API | 1.57.00.00 | /libraries/flash_api/f28002x/ |
| F2838x C28x Flash API | 1.60.00.00 | /libraries/flash_api/f2838x/c28x/ |
| F2838x CM Flash API | 1.60.00.00 | /libraries/flash_api/f2838x/cm/ |
| F2837xD Flash API | 1.54.00.00 | /libraries/flash_api/f2837xd |
| F2807x Flash API | 1.54.00.00 | /libraries/flash_api/f2807x |
| F2837xS Flash API | 1.55.00.00 | /libraries/flash_api/f2837xs |
| F28003x Flash API | 1.58.10.00 | /libraries/flash_api/f28003x |
| F280033_34 Flash API | 1.58.11.00 | /libraries/flash_api/f28003x | F28004x Flash API | 1.56.01.00 | /libraries/flash_api/f28004x |
| F2802x Flash API | 2.01.00.00 | /libraries/flash_api/f2802x |
| F2803x Flash API | 1.00.00.00 | /libraries/flash_api/f2803x |
| F2805x Flash API | 1.00.00.00 | /libraries/flash_api/f2805x |
| F2806x Flash API | 1.00.00.00 | /libraries/flash_api/f2806x |
| F2823x Flash API | 2.10.00.00 | /libraries/flash_api/f2823x |
| F2833x Flash API | 2.10.00.00 | /libraries/flash_api/f2833x |
| F2838x Ethercat | 2.02.00.00 | /libraries/communications/Ethercat/f2838x |
| F2838x EtherCAT Slave Demo Installer | 2.02.00.00 | libraries/communications/Ethercat/f2838x/ethercat_slave_ssc_and_demo_setup.exe |
| F28P65x Ethercat | 1.00.00.00 | /libraries/communications/Ethercat/f28p65x |
| F28P65x EtherCAT Slave Demo Installer | 1.01.00.00 | libraries/communications/Ethercat/f28p65x/ethercat_slave_ssc_and_demo_setup.exe |
| FatFS | R0.13a | libraries/fatfs |
| SDL | 5.00.00.00 | /libraries/diagnostic |
| Crypto AES | 2.00.00.00 | /libraries/security/crypto/c28/aes | Crypto SHA | 2.00.00.00 | /libraries/security/crypto/c28/sha | Crypto RSA | 1.00.00.00 | /libraries/security/crypto/c28/rsa | F280013x Flash API | 2.00.10.00 | /libraries/flash_api/f280013x |
| F280015x Flash API | 2.00.10.00 | /libraries/flash_api/f280015x |
| F28P65x Flash API | 3.00.02.00 | /libraries/flash_api/f28p65x |
| F28P55x Flash API | 4.00.00.00 | /libraries/flash_api/f28p55x |
| FreeRTOS Demo | 1.0.0 | kernel/FreeRTOS/Demo |
| FreeRTOS Kernel | 10.4.2 | kernel/FreeRTOS/Source |
| FreeRTOS Heap | 10.4.2 | kernel/FreeRTOS/Source/portable/MemMang |
| Device | Version | Location |
|---|---|---|
| f2807x | 3.19.00.00 | /device_support/f2807x |
| f2807x | 5.04.00.00 | /driverlib/f2807x |
| f2837xd | 3.19.00.00 | /device_support/f2837xd |
| f2837xd | 5.04.00.00 | /driverlib/f2837xd |
| f2837xs | 3.19.00.00 | /device_support/f2837xs |
| f2837xs | 5.04.00.00 | /driverlib/f2837xs |
| f2802x | 3.06.00.00 | /device_support/f2802x |
| f2802x0 | 3.05.00.00 | /device_support/f2802x0 |
| f2803x | 2.06.00.00 | /device_support/f2803x |
| f2805x | 2.05.00.00 | /device_support/f2805x |
| f2806x | 2.07.00.00 | /device_support/f2806x |
| f2823x | 2.06.00.00 | /device_support/f2823x |
| f2833x | 2.05.00.00 | /device_support/f2833x |
| f28002x | 5.04.00.00 | /device_support/f28002x |
| f28002x | 5.04.00.00 | /driverlib/f28002x |
| f28003x | 5.04.00.00 | /device_support/f28003x |
| f28003x | 5.04.00.00 | /driverlib/f28003x |
| f28004x | 5.04.00.00 | /device_support/f28004x |
| f28004x | 5.04.00.00 | /driverlib/f28004x |
| f2838x | 5.04.00.00 | /device_support/f2838x |
| f2838x | 5.04.00.00 | /driverlib/f2838x |
| f280013x | 5.04.00.00 | /device_support/f280013x |
| f280013x | 5.04.00.00 | /driverlib/f280013x |
| f280015x | 5.04.00.00 | /device_support/f280015x |
| f280015x | 5.04.00.00 | /driverlib/f280015x |
| f28p65x | 5.04.00.00 | /device_support/f28p65x |
| f28p65x | 5.04.00.00 | /driverlib/f28p65x |
| f28p55x | 5.04.00.00 | /device_support/f28p55x |
| f28p55x | 5.04.00.00 | /driverlib/f28p55x |
Note:The minimum version of Code Composer Studio required is CCSv12.8, SysConfig version is 1.21 and compiler version is 22.6.1.LTS
Note 1: "device_cal" function address is different for different revisions of the F28P55x device. If the revision ID (value at address 0x5D00C) is "1" then define the REV_ID as a predefined symbol in the projectspec (Add "--define=REV_ID=1" in the compiler flags, which correspond to REV0). For REVID as REVA, the value will be 2, which is the default value in the package.
Note 2: I2C config name change in SysConfig : "OwnTargetAddress" has been renamed to "OwnAddress". Any .syscfg file which uses the older name has to be updated to use this new name (i2cx.ownTargetAddress to i2cx.OwnAddress)
Note 3: The TINIE naming is to be updated to NPU in driverlib functionalities/macros for F28P55x device for previous SDKs.
Note:The minimum version of Code Composer Studio required is CCSv12.7 and compiler version is 22.6.1.LTS
Note:The minimum version of Code Composer Studio required is CCSv12.4 and compiler version is 22.6.0.LTS
Note:The minimum version of Code Composer Studio required is CCSv12.4 and compiler version is 22.6.0.LTS