Macros | Functions
hmac.c File Reference

The file implements the register level functions for HMAC/HASH module using SHA/MD5 algorithms. No validations are performed on input parameters. The caller of the APIs need to ensure the input parameters are valid. More...

#include <stdint.h>
#include <string.h>
#include <ti/drivers/osal/MemoryP.h>
#include <ti/drivers/crypto/include/crypto_internal.h>
#include <ti/common/hw_types.h>

Macros

#define P_EIP57T_INTERRUPT_MASK   (0x00000007U)
 

Functions

void HMAC_init (DTHERegs *dtheBaseAddress, SHARegs *hmacBaseAddress)
 
void HMAC_setConfig (SHARegs *hmacBaseAddress, uint32_t cryptoMode, uint8_t useAlgoConstant, uint8_t closeHash, uint8_t useHMACKey, uint8_t HMACOuterHash)
 
uint32_t HMAC_isReady (const SHARegs *hmacBaseAddress, uint32_t flag)
 
void HMAC_setDataLength (SHARegs *hmacBaseAddress, uint32_t dataLength)
 
void HMAC_writeData (SHARegs *hmacBaseAddress, const uint8_t *ptrData)
 
uint32_t HMAC_getDigestSize (uint32_t config)
 
void HMAC_readResult (SHARegs *hmacBaseAddress, uint8_t *ptrData)
 
void HMAC_writeResult (SHARegs *hmacBaseAddress, uint8_t *ptrData)
 
uint32_t HMAC_readDigestCount (SHARegs *hmacBaseAddress)
 
void HMAC_writeDigestCount (SHARegs *hmacBaseAddress, uint32_t digestCount)
 
void HMAC_setHMACKey (SHARegs *hmacBaseAddress, const uint8_t *ptrKey)
 
void HMAC_setHMACPPKey (SHARegs *hmacBaseAddress, const uint8_t *ptrKey)
 
void HMAC_enableInterrupt (DTHERegs *dtheBaseAddress, SHARegs *hmacBaseAddress, uint32_t intFlags)
 
void HMAC_disableInterrupt (DTHERegs *dtheBaseAddress, SHARegs *hmacBaseAddress, uint32_t intFlags)
 
void HMAC_clearInterrupt (DTHERegs *dtheBaseAddress, uint32_t intFlags)
 
uint32_t HMAC_getInterruptStatus (DTHERegs *dtheBaseAddress, SHARegs *hmacBaseAddress, uint8_t masked)
 

Detailed Description

The file implements the register level functions for HMAC/HASH module using SHA/MD5 algorithms. No validations are performed on input parameters. The caller of the APIs need to ensure the input parameters are valid.

NOTE: (C) Copyright 2017 Texas Instruments, Inc.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Macro Definition Documentation

#define P_EIP57T_INTERRUPT_MASK   (0x00000007U)

Interrupt masks


Copyright 2018, Texas Instruments Incorporated