PKTUTL 2.0.0.0 Release Notes
June 9, 2010
Introduction, Documentation, What's New, Upgrade and Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.
Introduction
Contains packet utility modules shared across the components.
back to top
Documentation
The following documentation is available:
Release notes from previous releases are also available in the relnotes_archive directory.
back to top
What's New
- Created new pktutl component and added pkt module which was formerly a part of the util component
- Added the crclib module.
back to top
Upgrade and Compatibility Information
This ti.mas.pktutl version is source compatible with the last released version.
Please note that the package compatibility keys are independent of XDC product release numbers.
Package compatibility keys are intended to:
- Enable tooling to identify incompatibilities between components, and
- Convey a level of compatibility between different releases to set end user expectations.
Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:
- M = Major - A difference in M indicates a break in compatibility. The package consumer is required to re-write its source code in order to use the package.
- S = Source - A difference in S indicates source compatibility. The package consumer’s source code doesn't require change, but does require a recompile.
- R = Radix - A difference in R indicates an introduction of new features, but compatibility with previous interfaces is not broken. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.
- P = Patch - A difference in P indicates that only bugs have been fixed in the latest package and no new features have been introduced. If libraries are provided by the package, an application must re-link with the new libraries, but is not required to recompile its source.
back to top
Host Support
This release supports the following hosts:
back to top
Dependencies
This release requires the following other software components and tools versions to successfully function
- XDC Tools version 3.15.0.33
- RTSC Packaging Standard version 1.00.00
- C6x Code Generation Tools version 6.0.15.
- C55 Code Generation Tools version 4.0.1.
- C54 Code Generation Tools version 4.10.
- ARM Montavista Pro 4.0.1
- ARM Montavista Pro 5.0
- WINCE Windows CE Embedded 6.0 with Platform builder R2
back to top
Device Support
This release supports the following device families:
- C64P, C64
- C55
- C54
- ARM
- Native development host (Windows)
back to top
Validation Information
This release is yet to be built and validated against using the following components:
back to top
Known Issues
back to top
Version Information
This product's version follows a version format, M.m.x.p, where M is a single digit Major number, m is single digit minor number, x is single digit vertical numbner and p is a single digit patch number
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
back to top
Technical Support
Contact local TI Field Application Engineer for technical support.
back to top
Copyright 2010, Texas Instruments Incorporated