#!/bin/bash
#
#  ======== genefs ========
#  Generate a C source code file for the NDK EFS (Embedded Filesystem) from
#  a directory of files.
#
#  In addition to converting all regular files into C char strings, files with
#  a .cgi suffix are treated specially. On the target device, a CGI "script"
#  is actually mapped to a C function. So, this script takes the base name of
#  a file ending with .cgi and generates a CGI entry with a function name
#  matching the basename:
#
#  demo/sampleData.cgi ->
#        efs_createfile("demo/sampleData.cgi", 0, (UINT8 *)sampleData);
#
#  Obviously, there must be an actual C function with that name in the
#  application code or the linker will fail.
#
#  The actual contents of the .cgi file are ignored. This makes it possible
#  to serve the directory structure via a host webserver during development,
#  and then just run genefs when ready to use on the target.
#

if test $# != 2
then
    echo "Usage: $0 input-directory output-file"
    exit 1
fi    

in=$1
out=$2

if ! test -d $in
then
    echo "$0: input $in is not a directory"
    exit 2
fi

rm -f $out
if ! touch $out || ! test -f $out 
then
    echo "$0: cannot write to output file $out"
    exit 3
fi    

tmp=efs$$.c

# change a /-delimited pathname to use _ separators for use as C identifier
function mapname
{
    base=${1//\//_}
    echo ${base//./_}
}

echo '#include <netmain.h>' > $tmp
echo '#include <_stack.h>' >> $tmp
echo "" >> $tmp

echo "void initEfsData()" > $out
echo "{" >> $out

for file in $(find $in -type f)
do
    suffix=${file##*.}
    base=${file##$in/}

    if [ $suffix = "cgi" ]
    then
	f=$(basename $file)
	id=${f%%.*}
	echo "    "extern int $id\(SOCKET s, int length\)\; >> $out
        echo "    "efs_createfile\(\"$base\", 0, \(UINT8 \*\)$id\)\; >> $out
    else
	id=$(mapname $base)
	#echo $id

	./binsrc $file tmp$$.c $id
	cat tmp$$.c >> $tmp
	echo "" >> $tmp
	rm tmp$$.c

	echo "    "efs_createfile\(\"$base\", ${id}_SIZE, $id\)\; >> $out
    fi
done

echo "}" >> $out

cat $tmp $out > tmp$$
mv tmp$$ $out
rm $tmp