Network Developers Kit API  3.61.01.01
Data Fields
_ci_route Struct Reference

#include <netcfg.h>

Collaboration diagram for _ci_route:
Collaboration graph

Data Fields

uint32_t IPDestAddr
 
uint32_t IPDestMask
 
uint32_t IPGateAddr
 
void * hRoute
 

Field Documentation

§ IPDestAddr

uint32_t _ci_route::IPDestAddr

§ IPDestMask

uint32_t _ci_route::IPDestMask

§ IPGateAddr

uint32_t _ci_route::IPGateAddr

§ hRoute

void* _ci_route::hRoute

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale